:FUNCtion:PARameters:USER:LSTatus:REASon?

Query Syntax

:FUNCtionN:PARameters:USER:LSTatus:REASon?

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Description

Returns the reason for a failed load of a configuration file.

Use the :FUNCtion:PARameters:USER:CFILe command to configure the function.

Parent Command