:GRAPh:DHERtz:X:AUToscale
Command Syntax
:GRAPh:DHERtzN:X:AUToscale
Where N specifies one of four {1:4} waveform content windows.
Description
Automatically scales the X-axis of the specified Degrees (Hz) waveform content window. Use the :GRAPh:DHERtz:X:CENTer, :GRAPh:DHERtz:X:SPAN, :GRAPh:DHERtz:X:STARt, and :GRAPh:DHERtz:X:STOP sibling commands to individually set these values.