:GRAPh:DHERtz:Y:OFFSet

Command Syntax

:GRAPh:DHERtzN:Y:OFFSet <degrees>

<degrees> is a double.

Where N specifies one of four {1:4} waveform content windows.

Query Syntax

:GRAPh:DHERtzN:Y:OFFSet?

Description

Sets the vertical offset of the specified Degrees (Hz) content window in degrees (°) at the Y-axis's center graticule. Use the :GRAPh:DHERtz:Y:AUToscale sibling command to automatically set the offset and scale settings. Use the :GRAPh:DHERtz:AUToscale parent command to automatically scale both the waveform in both X and Y axis.