:GRAPh:DHERtz:Y:SCALe

Command Syntax

:GRAPh:DHERtzN:Y:SCALe <scale>

<scale> is a double.

Where N specifies one of four {1:4} waveform content windows.

Query Syntax

:GRAPh:DHERtzN:Y:SCALe?

Description

Sets the vertical scale of the specified Degrees (Hz) content window in degrees-per-division. The vertical expansion and contraction is referenced to the center graticule (:GRAPh:DHERtz:Y:OFFSet sibling command) of the display. Use the :GRAPh:DHERtz:Y:AUToscale sibling command to automatically set the offset and scale settings. Use the :GRAPh:DHERtz:AUToscale parent command to automatically scale both the waveform in both X and Y axis.