:GRAPh:DHERtz:X:CENTer
Command Syntax
:GRAPh:DHERtzN:X:CENTer <frequency>
<frequency> is a double.
Where N specifies one of four {1:4} waveform content windows.
Query Syntax
:GRAPh:DHERtzN:X:CENTer?
Description
For the specified Degrees (Hz) waveform content window, sets the graph's X- axis center frequency in Hertz. Use the :GRAPh:DHERtz:X:AUToscale sibling command to automatically set the center, span, start, and stop settings. Use the :GRAPh:DHERtz:AUToscale parent command to automatically scale both the waveform in both X and Y axis.