:GRAPh:DHERtz:X:SPAN

Command Syntax

:GRAPh:DHERtzN:X:SPAN <frequency>

<frequency> is a double.

Where N specifies one of four {1:4} waveform content windows.

Query Syntax

:GRAPh:DHERtzN:X:SPAN?

Description

For the specified Degrees (Hz) waveform content window, sets the graph's X- axis frequency span in Hertz. Use the :GRAPh:DHERtz:X:AUToscale sibling command to automatically set the center, span, start, and stop settings. Use the :GRAPh:DHERtz:AUToscale parent command to automatically scale both the waveform in both X and Y axis.