:INSTrument:CONNection:CMEThod?
Query Syntax
:INSTrument:CONNectionN:CMEThod?
Where N identifies a specific instrument by connection number and must be selected from {1:8}. For example, :CONNection2.
Query Response
{USB | NONE}
Description
Use this query to determine if an oscilloscope is connected to Infiniium. As the only connection method for an oscilloscope is via USB, the value returned can be USB or NONE.