:LTESt:LLINe:SIMage:FNAMe:AUPDate
Command Syntax
:LTESt:LLINeN:SIMage:FNAMe:AUPDate
Where N identifies one of 64 {1:64} possible limit lines. For example, :LLINe23.
Description
Increments a file name's autonumber for the next screen image save. Use the :LTESt:LLINe:SIMage:STATe command to enable and disable screen-capture reporting. To enable or disable limit-line limit tests, use the :LTESt:LLINe:TEST{N}:STATe command. The autonumber format is explained in :LTESt:LLINe:SIMage:FNAMe.
Example Command Sequence
:ACQuire:SINGle :LTESt:LLINe:SIMage:FNAMe "my_file_1.png" :LTESt:LLINe:SIMage:STATe ON // Enable screen capture reporting :LTESt:LLINe:TEST:STATe ON // Turn limit test on :ACQuire:RUN;*OPC? # my_file_1.png … … :ACQuire:CDISplay :LTESt:LLINe:SIMage:FNAMe:AUPDate :ACQuire:RUN;*OPC? # my_file_2.png