:LTESt:LLINe:SIMage:FNAMe:USTandard

Command Syntax

:LTESt:LLINeN:SIMage:FNAMe:USTandard

Where N identifies one of 64 {1:64} possible limit lines. For example, :LLINe23.

Description

Resets the file name for the screen image file from using a custom name to using the standard name in the following form:

Screen_<date><autonumber>.<extension>

For example, Screen_2017-04-08_1.jpg. Refer to :LTESt:LLINe:SIMage:FNAMe to learn about standard and custom names.