:LTESt:LLINe:SIMage:MONochrome

Command Syntax

:LTESt:LLINe:SIMage:MONochrome {ON | OFF}

Query Syntax

:LTESt:LLINe:SIMage:MONochrome?

Description

Upon completion of limit testing for a limit line test, a screen image can be saved to a graphics file. Use this command to turn monochrome screen capture on and off. When on, a black and white image will be captured and saved into a file specified by the :LTESt:LLINe:SIMage:FNAMe command. Selecting monochrome automatically inverts the graticule area's background color.

Use the :LTESt:LLINe:SIMage:STATe command to enable and disable screen-capture reporting. To enable or disable limit testing for a limit line test, use the :LTESt:LLINe:TEST{N}:STATe command.