:LTESt:LLINe:SIMage:IMETadata
Command Syntax
:LTESt:LLINe:SIMage:IMETadata {ON | OFF}
Query Syntax
:LTESt:LLINe:SIMage:IMETadata?
Description
Turns on and off the inclusion of metadata when saving a screen image file as the result of the completion of limit testing for a limit line test. Saving metadata only applies to screen captures that are saved as jpg or tiff files. To view or edit the metadata placed in your screen image file, you can right click on the file in Window's File Explorer and from the shortcut menu select Properties. In the Properties dialog box, click the Details tab as shown in this picture. To edit the metadata fields for your image, click on the Value entree shown on the dialog box. The following table lists the metadata fields that Infiniium populates. The query form of the command returns the current setting.
| Metadata Field | Value Examples |
|---|---|
| Subject | Screen Capture |
| Comments | ?????A (S/N USXXXXXXXX) Modules: Connection 1 Module(86108B LBW,232,300,400,JSA) (MYXXXXXXXX) |
| Date taken | 7/10/2015 4:32 PM |
| Program name | Infiniium |
| Camera maker | Keysight Technologies |
| Camera model | Infiniium |
| Name | ScreenCapture.jpg |