:LTESt:LLINe:SIMage:SINClude

Command Syntax

:LTESt:LLINe:SIMage:SINClude {ALL | CHANnel{N} | FUNCtion{1:64} | WMEMory{1:8} | CGMemroy{1:8}}

{N} identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:LTESt:LLINe:SIMage:SINClude?

Description

Upon completion of limit testing for a limit line test, a screen image can be saved to a graphics file. If multiple waveforms are displayed, use this command to select that all or only one waveform be included in the saved image file. By default, all waveforms visible on the display are saved in the screen capture. However, when you select one waveform, all other waveform's will be hidden except for their ground markers ( ), which are shown on the screen's right side. Including these markers serves as a reminder that other waveforms were present on the display.

This command is disabled, if the :LTESt:LLINe:SIMage:WINDow command is set to the DISPlay argument. In this case, all waveforms are included in the screen image.

Use the :LTESt:LLINe:SIMage:STATe command to enable and disable screen-capture reporting. To enable or disable limit testing for a limit line test, use the :LTESt:LLINe:TEST{N}:STATe command.