:MEASure:JITTer:NOISe:DMAXimized
Command Syntax
:MEASure:JITTerN:NOISe:DMAXimized {ON | OFF | 1 | 0}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:NOISe:DMAXimized?
Query Response
{1 | 0}
Description
When Noise graphs are displayed in a grid (see :MEASure:JITTer:NOISe:GSIZe), this command lets you maximize the most recently selected graph (see :MEASure:JITTer:NOISe:MGRaph) to occupy the space of all the grids (ON) or return to the display of graphs in a grid (OFF).