:MTESt:MARGin:AUTO:HITS

Command Syntax

:MTEStN:MARGin:AUTO:HITS <hits>

<hits> is an integer.

Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.

Query Syntax

:MTEStN:MARGin:AUTO:HITS?

Description

Automatically sets the margin size based on a target hit count. The margin is sized so that:

Automatic margin sizing can also be based on a hit ratio as determined by the :MTESt:MARGin:AUTO:METHod command.

Example Command Sequence

:MTESt3:MARGin:METHod AUTO
:MTESt3:MARGin:AUTO:METHod HITS
:MTESt3:MARGin:AUTO:HITS 10
:MTESt3:MARGin:STATe ON
:MTESt3:LOAD:FNAMe "009.95328 - 10GbE_9_953_May02.mskx"
:MTESt3:LOAD