:MTESt:MARGin:STATe
Command Syntax
:MTEStN:MARGin:STATe {ON | OFF | 1 | 0}
Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.
Query Syntax
:MTEStN:MARGin:STATe?
Query Response
{1 | 0}
Description
Turns the compliance margins for a mask on or off. Use the :MTESt:MARGin:METHod command to select automatic or manual determination of margin size.