:MTESt:MARGin:AUTO:METHod
Command Syntax
:MTEStN:MARGin:AUTO:METHod {HITS | HRATio}
Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.
Query Syntax
:MTEStN:MARGin:AUTO:METHod?
Description
Selects that automatic configuration of the margin size is to be based on a target hit count (HITS) or target hit ratio (HRATio). Automatic mask margin configuration must first be enabled using the :MTESt:MARGin:METHod command.
Example Command Sequence
:MTESt2:MARGin:METHod AUTO :MTESt2:MARGin:AUTO:METHod HITS :MTESt2:MARGin:AUTO:HITS 10 :MTESt2:MARGin:STATe ON :MTESt2:LOAD:FNAMe "009.95328 - 10GbE_9_953_May02.mskx" :MTESt2:LOAD