:SYSTem:MPButton:SIMage:BFName

Command Syntax

:SYSTem:MPButton:SIMage:BFName "<filename>"

"<filename>" is a string of the file name with optional path. The string can include path substitution strings.

Query Syntax

:SYSTem:MPButton:SIMage:BFName?

Description

Enters the base filename for saving screen images using the Multi-Purpose button. The default filename is QuickScreenSave.jpg.

To specify the type of image file saved, append one of the following file name extensions .bmp, .gif, .jpg, .png, or .tif.

Each image file that is saved uses a variation of your base filename. The name of the saved file is in the form of:

<base filename>_<year>-<month>-<day>_<index>.<extension>

For example, suppose that you enter a base filename of EyeDiagram.png and you save your first screen image file on April 19th, 2015. The name of the file will be EyeDiagram_2015-4-19_1.png.

After entering the base filename, configure the Multi-Purpose button to save a screen images using the :SYSTem:MPButton:FUNCtion command.

Example Command Sequence

:SYSTem:MPButton:SIMage:BFName "ProtoWaveform.png"  //  Assign a base filename
:SYSTem:MPButton:SIMage:INVert ON
:SYSTem:MPButton:FUNCtion SSCReen  //  Assign saving a screen image to Multi-Purpose button