:SYSTem:MPButton:QSPBack:FNAMe
Command Syntax
:SYSTem:MPButton:QSPBack:FNAMe "<path substitution string>\subfolder\filename"
Where:
- "<path substitution string> is a string that expands into a specific file path. For example, %USER_DATA_DIR%.
- "subfolder" is an optional path folder. For example, %USER_DATA_DIR%\SCPI Scripts.
- "filename" is a string without the filename extension.
Query Syntax
:SYSTem:MPButton:QSPBack:FNAMe?
Description
When the Multi-Purpose button is configured to run a single SCPI script (.scpi) regardless of instrument mode, this command identifies the path and name of the script. To select to use a single script, use the command. To configure the Multi-Purpose button to run a SCPI script file, use the :SYSTem:MPButton:FUNCtion command.
Default User Folder
The default folder for storing script files is in %USER_DATA_DIR%\SCPI Scripts as shown in this picture. It is good practice to include a path substitution string with the filename. For example, %USER_DATA_DIR%\SCPI Scripts\filename.
File names must include a path when using the child :FNAMe command. The :FNAMe command is not affected by a Default Setup or Factory Default.
Specifying a path using a path substitution string in the filename ensures that the file will be saved in (or loaded from) the standard user-data folder. Failure to use a path substitution string may result either in a file created in an parent folder or a file error.
Example Command Sequence
:SYSTem:MPButton:QSPBack:FNAMe "%USER_DATA_DIR%\SCPI Scripts\MyScript.scpi" // Assign running a script to Multi-Purpose button