:SYSTem:MPButton:SIMage:INVert

Command Syntax

:SYSTem:MPButton:SIMage:INVert {ON | OFF}

Query Syntax

:SYSTem:MPButton:SIMage:INVert?

Description

Turns on and off the inversion of the graticule area's background color. The entire application window is saved with a black graticule upon a white background. The waveform colors remain unchanged. Inversion is automatically turned on and cannot be turned off if the :SYSTem:MPButton:SIMage:MONochrome sibling command is enabled. To configure the Multi-Purpose button to save a screen image to a file, use the :SYSTem:MPButton:FUNCtion command.