:SYSTem:MPButton:SIMage:MONochrome

Command Syntax

:SYSTem:MPButton:SIMage:MONochrome {ON | OFF}

Query Syntax

:SYSTem:MPButton:SIMage:MONochrome?

Description

Turns monochrome screen capture on and off. When on, a black and white image will be saved. Selecting monochrome automatically inverts the graticule area's background color. When off, you can invert the graticule area's background color using the :SYSTem:MPButton:SIMage:INVert sibling command. To configure the Multi-Purpose button to save a screen image to a file, use the :SYSTem:MPButton:FUNCtion command.