:SYSTem:MPButton:DOCWizard:BFName

Command Syntax

:SYSTem:MPButton:DOCWizard:BFName "<filename>"

"<filename>" is a string of the file name including an optional path. The string can include path substitution strings.

Query Syntax

:SYSTem:MPButton:DOCWizard:BFName?

Description

When the Multi-Purpose button is configured to documentation wizard file, this command identifies the path and name of the saved file. The default file (including path) is:

  • %USER_DATA_DIR%\Documentation Results\DocumentationResults.zip

To configure the Multi-Purpose button to save a documentation wizard file, use the :SYSTem:MPButton:FUNCtion command.

Example Command Sequence

:SYSTem:MPButton:DOCWizard:BFName "%USER_DATA_DIR%\Documentation Results\DocWizard.zip"
:SYSTem:MPButton:FUNCtion SDWFile