:WMEMory:XSCale

Command Syntax

:WMEMory:XSCale <horizontal_scale>

<horizontal_scale> is a double.

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:XSCale?

Description

Sets the horizontal scale which is stored for the selected waveform memory. It may or may not be the same as Infiniium's current setting. Multiply the horizontal scale by 10 to obtain the horizontal range. The default value is 100 ps.

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.