:WMEMory:XPOSition

Command Syntax

:WMEMory:XPOSition <horizontal_position>

<horizontal_position> is a double.

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:XPOSition?

Description

Sets the horizontal time position which is stored in the waveform memory. The default value is 250 ps, the minimum is -50 ps, and the maximum is -50 ps. It may or may not be the same as Infiniium's current setting. The horizontal position is the time delay relative to the trigger event, which is referenced to the display's left edge or center (:WMEMory:XREFerence?). The horizontal reference and position of the original waveform was set with the :TIMebase:REFerence and :TIMebase:POSition commands.

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.