:WMEMory:XSCale:FINE

Command Syntax

:WMEMoryN:XSCale:FINE {{OFF | 0} | {ON | 1}}

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:XSCale:FINE?

Query Response

{0 | 1}

Description

Enables or disables fine adjustment of the horizontal scale.

When OFF (coarse adjustment), the horizontal scale is adjusted in a 1-2-5 sequence.

When ON (fine adjustment), the horizontal scale is adjusted in smaller, evenly spaced increments.