:WMEMory:XRIGht?
Query Syntax
:WMEMoryN:XRIGht?
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Description
Queries the time value stored in waveform memory for the waveform's right edge. This is the value that existed when the source waveform was saved into memory or, if the data was loaded into memory from a waveform file (:DISK:WAVeform:SAVE), it is the value that existed when the file was created. It may or may not be the same as Infiniium's current setting.