:WMEMory:YOFFset

Command Syntax

:WMEMoryN:YOFFset <amplitude>

<amplitude> is a double.

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:YOFFset?

Description

Sets the vertical offset which is stored for the selected waveform memory. It may or may not be the same as Infiniium's current setting. The default value is 0V.

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.