Quick Start
This topic shows the configurations that can be used for controlling Infiniium 2026.
From a remote computer, you can control Infiniium 2026 running on an oscilloscope or running offline on a PC. Because the oscilloscope is also a PC, you can also run programs on the oscilloscope or on the PC running Infiniium 2026 offline.
For example scripts for different configurations, see:
To determine Infiniium 2026's current configuration
The following table lists the queries that you can send to learn about the current configuration of Infiniium 2026.
| Query | Configurations | Description | |
|---|---|---|---|
| Offline | Oscilloscope | ||
*IDN?
|
D9300A
|
XR804KA
|
These responses are substrings of the returned identification string. For example,Keysight Technologies,D9300A,2UA5383S5F,A.26.60.000 |
:INSTrument:CONNection1:SELection?
|
VFCHannel
|
XR8
|
Indicates that a virtual 4-channel oscilloscope or real oscilloscope hardware is assigned to connection 1. |
:INSTrument:CONNection1:STATe?
|
CONN
|
CONN
|
Indicates a communication connection has been established with a virtual instrument or oscilloscope hardware. |