Starting a Program

Always start your programs with the commands shown in the following listing. Use the *RST (Reset) common command to initialize Infiniium to a preset state. The :SYSTem:AUToscale command is very useful on unknown waveforms as it automatically sets up the channel vertical scale, time base, and trigger level. A typical instrument setup configures the vertical range and offset voltage, the horizontal range, delay time, delay reference, trigger mode, trigger level, and slope. Notice that the :SYSTem:DEFault and :SYSTem:AUToscale commands should be followed by an *OPC (Operation Complete) common query.

Example programs are provided that show how to setup basic communications. Example are provided for C#.NET, Labview, MATLAB, and Python. Look in the installation folder: \Keysight\Infiniium\Demo\Example Programs

The following command snippet demonstrate starting lines of code for starting and ending your programs.

Starting a Program

Infiniium.write('*RST')  # Initialize the instrument
Infiniium.write('*CLS')  # Clear status and error registers
Infiniium.query(':SYSTem:DEFault;*OPC?')
Infiniium.query(':SYSTem:AUToscale;*OPC?')
…
…
#  Your code here
…
…
Infiniium.write(':SYSTem:GTLocal')
Infiniium.close()