Calculating Compensation Coefficients and Turning ON/OFF Compensation
Preventing Operational Errors When Measuring Data for Calculating
Saving or Recalling Compensated State (Retrieving or Writing Compensation)
Other topics about Preparing for Accurate Measurement
You can either use the E4982A's predefined compensation kit values or directly enter other compensation kit values. To choose how the compensation kit values are defined, use the following command:
If you opt to enter the values, you need to specify how the compensation kit itself is defined and then enter the definitions.
To define the OPEN and SHORT standards, use the commands listed in the following table:
|
|
Impedance value |
Rdc value |
|
OPEN |
||
|
SHORT |
To measure the data for calculating the compensation coefficients, use the following command:
The command shown above measures the data for calculating the compensation coefficients for both impedance and Rdc measurements. If you want to obtain the data for either impedance or Rdc measurement alone, use one of the following commands instead:
To define the OPEN and SHORT compensation standards using the commands described so far, follow these steps:
Connect the OPEN standard and then issue the :CORR2:COLL command, which designates “STAN1” as the parameter. If the trigger source is not Internal trigger, you must trigger the instrument after issuing the command. This applies to step 2 as well.
Connect the SHORT standard and then issue the :CORR2:COLL command, which designates “STAN2” as the parameter.
Issue the :CORR2:COLL:SAVE command.
Connect the OPEN standard for impedance measurement and then issue the :CORR2:COLL or :CORR2:COLL:RF command, which designates “STAN1” as the parameter. If the trigger source is not Internal trigger, you must trigger the instrument after issuing the command. This applies to steps 2 through 4 as well.
Connect the SHORT standard for impedance measurement and then issue the :CORR2:COLL or :CORR2:COLL:RF command, which designates “STAN2” as the parameter.
Connect the OPEN standard for Rdc measurement and then issue the :CORR2:COLL:DC command, which designates “STAN1” as the parameter.
Connect the SHORT standard for Rdc measurement and then issue the :CORR2:COLL:DC command, which designates “STAN2” as the parameter.
Issue the :CORR2:COLL:SAVE command.
After measuring the data for calculating the compensation coefficients, issue the following commands to calculate the compensation coefficients and turn on the compensation function:
|
Measured data |
GPIB command |
Status of compensation function after calculation |
|
|
OPEN and SHORT |
ON |
ON |
|
|
ON |
Unchanged |
||
|
Unchanged |
ON |
||
|
OPEN only |
ON |
OFF |
|
|
ON |
OFF |
||
|
Not supported |
|||
|
SHORT only |
OFF |
ON |
|
|
Not supported |
|||
|
OFF |
ON |
||
*1. Issue the command, which designates "ON" (or '1") as the parameter.
When the OPEN compensation function is currently ON, you can issue the :CORR2:COLL:OPEN command by specifying “OFF” (or “0”) as the parameter to turn OFF the OPEN compensation function.
Similarly, when the SHORT compensation function is currently ON, you can issue the :CORR2:COLL:SHOR command by specifying “OFF” (or “0”) as the parameter to turn OFF the SHORT compensation function.
To retrieve each standard’s measurement data for calculating the compensation coefficients for Rdc measurement, use the following command:
Since this command returns the Rdc measurement value (without compensation) for each of the OPEN and SHORT standards, you can check whether this value is normal to prevent operational errors (such as connecting the wrong standard) that may arise when measuring the data.
When you validate the Rdc measurement results returned by the command :DATA:RCMD{1-2}?, you should use the absolute value for the same reasons as shown in Preventing operational errors when measuring data for calculating calibration coefficients.
The measurement data of the OPEN and SHORT standards used for calculating the compensation coefficients for impedance measurement are stored in the calibration data array (see Compensation Data Arrays). You can retrieve this data with the following command:
This command returns RF measurement data without compensation, which require more complex handling than Rdc values.To detect operational errors that may have occurred while measuring the compensation data, it is best to use Rdc values instead.
You can retrieve the compensation coefficients and save them to a file. Later, you can retrieve the compensation coefficients from the file and load them into the E4982A to restore the compensated state at the time you saved the file.
The compensation coefficients for impedance measurement are stored in the compensation coefficient array (see Compensation Data Arrays). To read or write the compensation coefficient array, use the following command:
To read or write the compensation coefficients for Rdc measurement, use the following command: