The S963015B SSA-X Signal Source Analyzer advanced features is required to enable this application.
The transient measurement allows you to observe the frequency, phase and power transition over time. It has two measurement modes: Wide-Narrow band mode and Narrow-Narrow band mode.
Wide band mode is useful for observing overall transient behavior.
Narrow band mode is useful for observing the precise behavior at the
settling and/or at start of the transition.

A PLL DUT should be connected on either RF 1 Input or RF 2 Input in the two port hardware configuration. One channel can measure one port only. If you want to measure PLLs on both RF 1 and 2 inputs, at least two channels are required.

How to start Transient |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
Select a different Measurement Class for the currently active channel.