Only the Main and Layout Setup commands corresponding to the Swept IMD measurement class are documented here. All other commands are identical to the Setup commands for the Standard measurement class and can be accessed by clicking here or by clicking on the softtabs on the graphic below.
Click here to view links to Setup commands for all Measurement Classes.
| Main Tab Commands | ||
| Softkey | Sub-item | SCPI |
| IMD Setup... | Frequency | |
| Sweep Type | ||
| Sweep fc | SENSe:IMD:SWEep:TYPE | |
| Sweep DeltaF | SENSe:IMD:SWEep:TYPE | |
| Power Sweep | SENSe:IMD:SWEep:TYPE | |
| CW | SENSe:IMD:SWEep:TYPE | |
| Segment Sweep fc | SENSe:IMD:SWEep:TYPE | |
| Sweep Settings | ||
| Start fc | SENSe:IMD:FREQuency:FCENter:STARt | |
| Center fc | SENSe:IMD:FREQuency:FCENter:CENTer | |
| Fixed DeltaF | SENSe:IMD:FREQuency:DFRequency[:CW] | |
| Number Of Points | SENSe:SWEep:POINt | |
| Stop fc | SENSe:IMD:FREQuency:FCENter:STOP | |
| Span fc | SENSe:IMD:FREQuency:FCENter:SPAN | |
| Main Tone IFBW | SENSe:IMD:IFBWidth:MAIN | |
| IM Tone IFBW | SENSe:IMD:IFBWidth:IMTone | |
| Reduce IF BW at Low Frequencies | None | |
| Power | ||
| Power On (All Channels) | OUTPut[:STATe] | |
| DUT Input | ||
| Input Port | SENSe:IMD:PMAP | |
| Source Attenuator | SOURce:POWer:ATTenuation | |
| Receiver Attenuator | SENSe:POWer:ATTenuator | |
| DUT Output | ||
| Output Port | SENSe:IMD:PMAP | |
| Source Attenuator | SOURce:POWer:ATTenuation | |
| Receiver Attenuator | SENSe:POWer:ATTenuator | |
| Tone Powers | ||
| Coupled Tone Powers | SENSe:IMD:TPOWer:COUPle[:STATe] | |
| ALC On | SENSe:IMD:TPOWer:LEV | |
| Power Leveling | ||
| Set Input Power | SENSe:IMD:TPOWer:LEV | |
| Set Input Power, receiver leveling | SENSe:IMD:TPOWer:LEV | |
| Set Input Power, equal tones at output | SENSe:IMD:TPOWer:LEV | |
| Set Output Power, receiver leveling | SENSe:IMD:TPOWer:LEV | |
| Fixed | SENSe:IMD:TPOWer:F1
SENSe:IMD:TPOWer:F2 |
|
| Start | SENSe:IMD:TPOWer:F1:STARt
SENSe:IMD:TPOWer:F2:STARt |
|
| Stop | SENSe:IMD:TPOWer:F1:STOP
SENSe:IMD:TPOWer:F2:STOP |
|
| Step | None | |
| Path Configuration... | SENSe:PATH:CONFig:ELEMent[:STATe] | |
| Configure | ||
| Receiver Configuration | SENSe:IMD:RECeiver:CONFig:COMBiner:PATH SENSe:IMD:RECeiver:CONFig:REFerence COUNt |
|
| Add Source... | SENSe:ROLE:DEVice | |
| Meas Class... | CALCulate:MEASure:DEFine | |
| Quick Start... | S-Param | CALCulate:MEASure:PARameter |
| Balanced | CALCulate:MEASure:PARameter | |
| Other | CALCulate:MEASure:PARameter | |
| Layout Tab Commands | ||
| Softkey | Sub-item | SCPI |
| New Trace | DISPlay:WINDow:TRACe[:STATe] | |
| New Channel | None | |
| New Window | DISPlay:WINDow[:STATe] | |
| New Sheet | DISPlay:SHEet:STATe | |
| Delete | TrN | DISPlay:WINDow:TRACe:DELete |
| ChN | SYSTem:CHANnels:DELete | |
| WinN | DISPlay:WINDow[:STATe] | |
| Select | TrN | DISPlay:WINDow:TRACe:SELect |
| ChN | None | |
| WinN | DISPlay:WINDow:TRACe:SELect | |
Measure... |
CALCulate:MEASure:PARameter | |
| Meas Class... | CALCulate:MEASure:DEFine | |