Only the Main and Layout Setup commands corresponding to the Scalar Mixer/Converter + Phase measurement class are documented here. All other commands are identical to the Setup commands for the Standard measurement class and can be accessed by clicking here or by clicking on the softtabs on the graphic below.
Click here to view links to Setup commands for all Measurement Classes.
Main Tab Commands | ||
Softkey | Sub-item | SCPI |
SMC Setup... | Sweep | |
Sweep Type | ||
Linear Frequency | SENSe:SWEep:TYPE | |
CW Time | SENSe:SWEep:TYPE | |
Segment Sweep | SENSe:SWEep:TYPE | |
Power | SENSe:SWEep:TYPE | |
X-Axis Point Spacing | SENSe:SEGMent:X:SPACing | |
Reversed Port 2 Coupler | SENSe:MIXer:REVerse | |
Number of Points | SENSe:SWEep:POINts | |
IF Bandwidth | SENSe:BWIDth[:RESolution] | |
Phase Reference Point | ||
Enable Phase | SENSe:MIXer:PHASe | |
Normalize First Point | SENSe:MIXer:NORMalize | |
Normalize Middle Point | SENSe:MIXer:NORMalize | |
Normalize Last Point | SENSe:MIXer:NORMalize | |
Specify Normalized Point | SENSe:MIXer:NORMalize | |
Use Absolute Phase (requires internal source as LO) | SENSe:MIXer:PHASe:ABSolute[:STATe] | |
Power | ||
Power On (All Channels) | OUTPut[:STATe] | |
Port Powers Coupled | SOURce:POWer:COUPle | |
DUT Input Port | ||
Input Port | SENSe:MIXer:PMAP | |
Power Level | SOURce:POWer[:LEVel][:IMMediate][:AMPLitude] | |
Source Leveling Mode | SOURce:POWer:ALC[:MODE] | |
DUT Output Port | ||
Output Port | SENSe:MIXer:PMAP | |
Power Level | SOURce:POWer[:LEVel][:IMMediate][:AMPLitude] | |
Source Leveling Mode | SOURce:POWer:ALC[:MODE] | |
DUT Input Port Power Sweep | ||
Start Power | SOURce:POWer:PORT:STARt | |
Stop Power | SOURce:POWer:PORT:STOP | |
Points | None | |
Power Step | None | |
DUT Output Port Power Sweep | ||
Start Power | SOURce:POWer:PORT:STARt | |
Stop Power | SOURce:POWer:PORT:STOP | |
Mixer Frequency | ||
Input | SENSe:MIXer:CALCulate | |
LO1 | SENSe:MIXer:LO:FREQuency:FIXed | |
Input > LO | SENSe:MIXer:LO:FREQuency:ILTI | |
IF Start | SENSe:MIXer:IF:FREQuency:STARt | |
IF Stop | SENSe:MIXer:IF:FREQuency:STOP | |
Output | SENSe:MIXer:CALCulate | |
Mixer Power | ||
Power On (All Channels) | OUTPut[:STATe] | |
LO1 Power | SENSe:MIXer:LO:POWer | |
LO2 Power | SENSe:MIXer:LO:POWer | |
Source Attenuator | SOURce:POWer:ATTenuation | |
Receiver Attenuator | SENSe:POWer:ATTenuator | |
LO1 Swept Power | ||
Start | SENSe:MIXer:LO:FREQuency:STARt | |
Stop | SENSe:MIXer:LO:FREQuency:STOP | |
Step | None | |
LO2 Swept Power | ||
Start | SENSe:MIXer:LO:FREQuency:STARt | |
Stop | SENSe:MIXer:LO:FREQuency:STOP | |
Step | None | |
Mixer Setup | ||
Converter Stages | SENSe:MIXer:STAGe | |
Add Source... | SENSe:ROLE:DEVice | |
Enable Embedded LO
See Embedded LO Setup commands |
SENSe:MIXer:LO:FREQuency:MODE | |
Port Input/Output | SENSe:MIXer:PMAP | |
Input Numerator Frac.Mult | SENSe:MIXer:INPut:FREQuency:NUMerator | |
Input Denominator Frac.Mult | SENSe:MIXer:INPut:FREQuency:DENominator | |
LOx | SENSe:MIXer:LO:NAME | |
LO Numerator Frac. Mult. | SENSe:MIXer:LO:FREQuency:NUMerator | |
LO Denominator Frac.Mult | SENSe:MIXer:LO:FREQuency:DENominator | |
Save... | SENSe:MIXer:SAVE | |
Load... | SENSe:MIXer:LOAD | |
Meas Class... | CALCulate:MEASure:DEFine | |
Quick Start... | S-Param | CALCulate:MEASure:PARameter |
Balanced | CALCulate:MEASure:PARameter | |
Other | CALCulate:MEASure:PARameter | |
Layout Tab Commands | ||
Softkey | Sub-item | SCPI |
New Trace | DISPlay:WINDow:TRACe[:STATe] | |
New Channel | None | |
New Window | DISPlay:WINDow[:STATe] | |
New Sheet | DISPlay:SHEet:STATe | |
Delete | TrN | DISPlay:WINDow:TRACe:DELete |
ChN | SYSTem:CHANnels:DELete | |
WinN | DISPlay:WINDow[:STATe] | |
Select | TrN | DISPlay:WINDow:TRACe:SELect |
ChN | None | |
WinN | DISPlay:WINDow:TRACe:SELect | |
Measure... |
CALCulate:MEASure:PARameter | |
Meas Class... | CALCulate:MEASure:DEFine |