Handler
IO Tab

Enable Handler Control Enables and disables sending data out
the Handler
IO Connector. The enable is set independently per-channel
and for "Before Sweep" and "After Sweep".
Ports A,
B, C, D Sends
values to the respective Handler I/O port. Although ports C and
D are normally bidirectional, ONLY Output mode is allowed using
the Interface Control feature. It cannot read from these, or any
other, ports.
Enable Control-All Channels Enables and disables ALL
Interface Control communication. When cleared (default setting)
Interface Control is disabled and NO data is sent. To send data,
the individual interfaces must also be enabled.
Channel Pulldown This
allows user to set IO independently for each channel.
Before Sweep/After Sweep Pull down
Allows setting IO data independently for before or after
sweep. Default setting is Before sweep. Before sweep is used to
set up command before making a measurement. After Sweep is used
to return SSA to a safe state so that the next channel does not
have any problems.
Dwell Entry
Delay time between all commands sent and measurement start. Set
independently per channel and for forward and reverse sweep, not
set per IO type. This is used to allow all external devices to
settle before making a measurement.
For save or recall, refer to Instrument
State Save.
DIO1/ DIO2 Tabs
(Device Test I/O)

Digital 16-bit IO is composed of 2 independent sets of Digital
8-bit IO. See the Device Test IO in Rear
Panel I/O.
The DUT Control function
provides 2 different type of controls for user DUT. These are
“parallel IO control” and “MIPI RFFE control”. The analyzer
can provide 2 sets of 8-bit digital IO. A 8-bit digital IO has
up to 8-line parallel IOs, and up to 4 MIPI RFFE controllers,
and user can set mixed configuration of parallel IO and MIPI RFFE
with some limitations.
The DUT Control signal generation timing is basically same as
Control Lines control of External Testset, so the function design
is based on the External Testset control.
Enable DIO1/DIO2 Enables
and disables sending data out the 8-bit digital IO (Device
Test I/O).
IO Level Set voltage
level of "Power Output" pin of the 8-bit IO. The power
out pin is used as VIO of RFEE. This level determine the "HIGH"
logic level of all IO pins of the 8-bit IO. The value range is
0.9V to 3.5V with 0.05V resolution.
Type Eight IO
pins are consists of 4 group of 2-pins pair: (Pins No. 1 and 2),
(Pins No. 3 and 4), (Pins No. 5 and 6), (Pins No. 7 and 8). Each
group can be assigned with Parallel or RFFE by using the pull-down
box.
Name The name of assigned
signal.
State Control buttons
are displayed depending on Type
selection, either Parallel or RFFE.
When
Parallel is selected:
In or OUT
- Select the pin function from Input or Output.
Low or High
- For input pin, show the current state. For output pin, select
the level from Low or High
When
RFFE is selected:
Clicking
RFFE setup.. shows
the RFFE setup dialog box.
Warning: Users
can save or recall IO settings as a state file. So users need
to take care not to damage the DUT if they use state files.
Macro Tab

Enable Macro Enables
and disables sending commands out the GPIB or VISA interface.
SCPI Commands The
multi-line edit control accepts pairs of GPIB or VISA address
and SCPI command. The SCPI commands are sent to the GPIB or VISA
addresses before the first trace on the channel begins sweeping.
Macro File-
Path The single-line edit control accepts a file path to a macro.
The macro is executed before the first trace on the channel begins
sweeping. The firmware just waits for the end of the macro and
does not care errors occurring in the macro. The macro designer
is responsible for error handling if necessary.
Macro File- Parameters The
single-line edit control accepts parameters to execute macro.
App IO Tab
Note: See
:CONTrol:SIGNal:AIO:PIN:FUNCtion.

Enable Control-All Channels,
Before Sweep, Dwell These controls are disabled.
Function When
a white cell is clicked, a drop down list appears to show functions
assignable to the specified port. Refer to the command description
about “:CONTrol:SIGNal:AIO:PIN<pin>:FUNCtion
<func>” for the assignable functions. If “CHANNEL_CTRL”
is specified, different functions can be assigned per channel.
All Channels When a channel
is selected in the channel scope dropdown, the dialog switches
to channel mode as shown in the figure below. Functions can be
assigned to the ports for which “CHANNEL_CTRL” has been specified
in the global mode.

|