Performs Mixer setup and configuration.
|
SENSe:MIXer: IF:FREQ: | SIDeband | STARt | STOP INPut:FREQ: | FIXed | MODE | STARt | STOP | STARt | STOP LO:FREQ: | FIXed | ILTI | MODE | STARt | STOP | STARt | STOP OUTPut:FREQ: | FIXed | MODE | SIDeband | STARt | STOP | INPut | OUTPut ROLE | CATalog? | DEVice STAGe (number of LOs) |
Click on a keyword to view the command details.
See Also
Note: If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface.
|
Applicable Models: All (Write only) Applies the mixer setup settings and turns the channel ON. (Performs the same function as the Apply button on the mixer setup dialog box). |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
Examples |
SENS:MIX:APPL |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB (Read Write) Sets and returns the state of the avoid spurs feature. Learn more about avoid spurs. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<bool> |
Avoid spurs state. Choose from 0 - Avoid spurs OFF 1 - Avoid spurs ON |
|
Examples |
SENS:MIX:AVO sense2:mixer:avoidspurs 1 |
|
Query Syntax |
SENSe<ch>:MIXer:AVOidspurs? |
|
Return Type |
Boolean |
|
0 (OFF) |
|
|
Applicable Models: All (Write only) Calculates the Input, IF, or Output frequencies of the mixer setup and updates the channel settings. Note: The target mode must be swept. This command does not allow calculation of fixed values. |
|||||||||||||||||||
|
Parameters |
|
||||||||||||||||||
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
||||||||||||||||||
|
<char> |
Mixer port to be calculated. Choose from:
|
||||||||||||||||||
|
Examples |
SENS:MIX:CALC Output |
||||||||||||||||||
|
Query Syntax |
Not Applicable |
||||||||||||||||||
|
Not Applicable |
|||||||||||||||||||
|
Applicable Models: All (Write only) Cancels changes that have been made to the Converter setup and reverts to the previously-saved setup. Same as the Cancel button on the mixer setup dialog box. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
Examples |
SENS:MIX:DISC |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) When two LO stages are used, sets or returns whether to select the sum or difference for the IF1 product. (Input + or - LO1 = IF1)
|
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<char> |
Sideband value. Choose from LOW - Difference (-) HIGH - Sum (+) |
|
Examples |
SENS:MIX:IF:FREQ:SID LOW |
|
Query Syntax |
SENSe<ch>:MIXer:IF:FREQuency:SIDeband? |
|
Return Type |
Character |
|
LOW |
|
|
Applicable Models: All (Read-Write) Sets or returns the IF start frequency value of the mixer. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<num> |
IF Start Frequency value |
|
Examples |
SENS:MIX:IF:FREQ:STAR 1e9 |
|
Query Syntax |
SENSe<ch>:MIXer:IF:FREQuency:STARt? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the stop frequency value of the mixer IF frequency. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<num> |
IF Stop Frequency value |
|
Examples |
SENS:MIX:IF:FREQ:STOP 2e9 |
|
Query Syntax |
SENSe<ch>:MIXer:IF:FREQuency:STOP? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the denominator value of the Input Fractional Multiplier. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Input denominator value. |
|
Examples |
SENS:MIX:INP:FREQ:DEN 5 |
|
Query Syntax |
SENSe<ch>:MIXer:INPut:FREQuency:DENominator? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the fixed frequency of the input. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Input frequency. |
|
Examples |
SENSe:MIXer:INPut:FREQ:FIXed 1e9 |
|
Query Syntax |
SENSe<ch>:MIXer:INPut:FREQuency:FIXed? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the Input sweep mode. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<char> |
Input sweep mode. Choose either FIXED or SWEPT |
|
Examples |
SENS:MIX:INP:FREQ:MODE FIXED |
|
Query Syntax |
SENSe<ch>:MIXer:INPut:FREQuency:MODE? |
|
Return Type |
Character |
|
Fixed |
|
|
Applicable Models: All (Read-Write) Sets or returns the numerator value of the Input Fractional Multiplier. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Input numerator value. |
|
Examples |
SENS:MIX:INP:FREQ:NUM 3 |
|
Query Syntax |
SENSe<ch>:MIXer:INPut:FREQ:NUMerator? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the Input start frequency value of the mixer. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Input Start frequency |
|
Examples |
SENS:MIX:INP:FREQ:STAR 1e9 |
|
Query Syntax |
SENSe<ch>:MIXer:INPut:FREQuency:STARt? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the Input stop frequency value of the mixer. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Input stop frequency |
|
Examples |
SENS:MIX:INP:FREQ:STOP 2e9 |
|
Query Syntax |
SENSe<ch>:MIXer:INPut:FREQuency:STOP? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the value of the Input Power. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Input power in dBm. |
|
Examples |
SENS:MIX:INP:POW 9 |
|
Query Syntax |
SENSe<ch>:MIXer:INPut:POWer? |
|
Return Type |
Numeric |
|
Not Applicable |
|
Applicable Models: All
|
(Read-Write) Sets the input start power for a power sweep in a mixer channel like SMC. The value is only used when the sweep type is power sweep. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Input power value in units of dBm. |
|
Examples |
SENS:MIX:INP:POW STAR 6 |
|
Query Syntax |
SENSe<ch>:MIXer:INPut:POWer:STARt? |
|
Return Type |
Numeric |
|
Not Applicable |
|
Applicable Models: All
|
(Read-Write) Sets the input stop power for a power sweep in a mixer channel . The value is only used when the sweep type is power sweep. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Input power value in units of dBm. |
|
Examples |
SENS:MIX:INP:POW STOP 9 |
|
Query Syntax |
SENSe<ch>:MIXer:INPut:POWer:STOP? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Toggles the Use Nominal Incident Power setting ON and OFF. This setting is ONLY to be used with SMC measurements. Learn more about Nominal Incident Power. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
(boolean) - Nominal Incident Power State. Choose from: ON (1) - Turn nominal incident power ON OFF (0) - Turn nominal incident power OFF |
|
Examples |
SENS:MIX:INP:POW:USEN 1 |
|
Query Syntax |
SENSe<ch>:MIXer:INPut:POWer:USENominal? |
|
Return Type |
Boolean |
|
OFF |
|
|
Applicable Models: All (Read-Write) Sets or returns the denominator value of the LO Fractional Multiplier. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
LO stage number. Choose 1 or 2. |
|
<value> |
LO denominator. |
|
Examples |
SENS:MIX:LO:FREQ:DEN 5 |
|
Query Syntax |
SENSe<ch>:MIXer:LO<n>:FREQuency:DENominator? |
|
Return Type |
Numeric |
|
1 |
|
|
Applicable Models: All (Read-Write) Sets or returns the fixed frequency of the specified mixer LO. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
LO stage number. Choose 1 or 2 |
|
<value> |
LO frequency. |
|
Examples |
SENS:MIX:LO:FREQ:FIX 1e9 |
|
Query Syntax |
SENSe<ch>:MIXer:LO<n>:FREQuency:FIXed? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Specifies whether to use the Input frequency that is greater than the LO or less than the LO. To learn more, see the mixer setup dialog box help. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
LO stage number. Choose 1 or 2 |
|
<bool> |
ON (1) - Use the Input that is Greater than the specified LO. OFF (0) - Use the Input that is Less than the specified LO. |
|
Examples |
SENS:MIX:LO1:FREQ:ILTI 1 |
|
Query Syntax |
SENSe<ch>:MIXer:LO<n>:FREQuency:ILTI? |
|
Return Type |
Boolean |
|
OFF |
|
|
Applicable Models: All (Read-Write) Sets or returns the LO sweep mode. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
LO stage number. Choose 1 or 2 |
|
<char> |
LO sweep mode. Choose either FIXED or SWEPT |
|
Examples |
SENS:MIX:LO:FREQ:MODE FIXED |
|
Query Syntax |
SENSe<ch>:MIXer:LO<n>:FREQuency:MODE? |
|
Return Type |
Character |
|
Fixed |
|
|
Applicable Models: All (Read-Write) Sets or returns the numerator value of the LO Fractional Multiplier. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
LO stage number. Choose 1 or 2 |
|
<value> |
LO Numerator. |
|
Examples |
SENS:MIX:LO:FREQ:NUM 5 |
|
Query Syntax |
SENSe<ch>:MIXer:LO<n>:FREQuency:NUMerator? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the LO start frequency value. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
LO stage number. Choose 1 or 2 |
|
<value> |
LO Start Frequency in Hertz. |
|
Examples |
SENS:MIX:LO:FREQ:STAR 5E9 |
|
Query Syntax |
SENSe<ch>:MIXer:LO<n>:FREQuency:STARt? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the LO stop frequency value. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
LO stage number. Choose 1 or 2 |
|
<value> |
LO Stop Frequency in Hertz. |
|
Examples |
SENS:MIX:LO:FREQ:STOP 5E9 |
|
Query Syntax |
SENSe<ch>:MIXer:LO<n>:FREQuency:STOP? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the name of the VNA internal source or external source to use as the LO in a converter measurement. Important Note: This setting is immediately send to the channel configuration. First set and apply mixer frequency settings, then send this command. Otherwise, 'invalid setting' errors may occur. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
LO stage number. Choose 1 or 2. |
|
<value> |
(string) - LO Source name. Use Source:CAT? to return a list of valid source ports. An external source must be configured and selected to be valid. Learn more about external source configuration. |
|
Examples |
SENS:MIX:LO:NAME "MySource" |
|
Query Syntax |
SENSe<ch>:MIXer:LO<n>:NAME? |
|
Return Type |
String |
|
"Not Controlled" |
|
|
Applicable Models: All (Read-Write) Sets or returns the LO Power fixed value. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
LO stage. Choose 1 or 2 |
|
<value> |
LO Power in dBm |
|
Examples |
SENS:MIX:LO:POW 9 |
|
Query Syntax |
SENSe<ch>:MIXer:LO<n>:POWer? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) For an LO power sweep, sets or returns the LO power start value. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
LO stage. Choose 1 |
|
<value> |
LO start power in dBm |
|
Examples |
SENS:MIX:LO1:POW:STAR -10 |
|
Query Syntax |
SENSe<ch>:MIXer:LO1:POWer:STARt? |
|
Return Type |
Numeric |
|
- 20 dBm |
|
|
Applicable Models: All (Read-Write) For an LO power sweep, sets or returns the LO power stop value. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
LO stage. Choose 1 |
|
<value> |
LO stop power in dBm |
|
Examples |
SENS:MIX:LO1:POW:STOP 10 |
|
Query Syntax |
SENSe<ch>:MIXer:LO1:POWer:STOP? |
|
Return Type |
Numeric |
|
-10 dBm |
|
|
Applicable Models: All (Write-only) Loads a previously-configured mixer attributes file (.mxr) |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<name> |
Path and file name (including .mxr extension) to load. |
|
Examples |
SENSe:MIXer:LOAD "C:/Program Files/Keysight/Network Analyzer/Documents/Mixer/MyMixer.mxr" |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the data point for normalizing the phase measurement. Learn more. |
|
|
Parameters |
|
|
<ch> |
Channel number of the SMC measurement. If unspecified, value is set to 1. |
|
<value> |
Normalization data point. Choose a data point number between 1 and the max number of data points in the sweep that has the least amount of expected noise. |
|
Examples |
SENS:MIX:NORM:POIN 101 sense2:mixer:normalize:point 50 |
|
Query Syntax |
SENSe<ch>:MIXer:NORMalize:POINt? |
|
Return Type |
Numeric |
|
Middle point in the sweep |
|
|
Applicable Models: All (Read-Write) Sets or returns the output fixed frequency of the mixer. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Output fixed frequency in Hertz. |
|
Examples |
SENS:MIX:OUTP:FREQ:FIX 5e9 |
|
Query Syntax |
SENSe<ch>:MIXer:OUTPut:FREQuency:FIXed? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the Output sweep mode. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<char> |
Output sweep mode. Choose either FIXED or SWEPT |
|
Examples |
SENS:MIX:OUTP:FREQ:MODE FIXED |
|
Query Syntax |
SENSe<ch>:MIXer:OUTPut:FREQuency:MODE? |
|
Return Type |
Character |
|
Fixed |
|
|
Applicable Models: All (Read-Write) Specify whether to select the sum (High) or difference (Low) products.
Use SENS:MIX:IF:FREQ:SID when two LOs are used to determine the IF1 frequency. Use Sens:Mixer:Stage to set 1 or 2 LOs |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Sideband value. Choose from LOW - Low or Difference (-) HIGH - High or Sum (+) |
|
Examples |
SENS:MIX:OUTP:FREQ:SID LOW |
|
Query Syntax |
SENSe<ch>:MIXer:OUTPut:FREQuency:SIDeband? |
|
Return Type |
Character |
|
LOW |
|
|
Applicable Models: All (Read-Write) Sets or returns the Output start frequency of the mixer. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Output start frequency |
|
Examples |
SENS:MIX:OUTP:FREQ:STAR 1e9 |
|
Query Syntax |
SENSe<ch>:MIXer:OUTPut:FREQuency:STARt? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets or returns the Output stop frequency of the mixer. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<value> |
Output stop frequency |
|
Examples |
SENS:MIX:OUTP:FREQ:STOP 1e9 |
|
Query Syntax |
SENSe<ch>:MIXer:OUTPut:FREQuency:STOP? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB (Read Write) Sets and returns the state of SMC Phase measurements and calibrations. Learn more. In the User Interface, there are two "enable phase" checkboxes: in the Phase Settings dialog and in the Calibration Wizard. Checking one enables both. This single command also enables both. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<bool> |
Include Phase measurement state. Choose from ON or 1 - Include phase in SMC measurements OFF or 0 - Do NOT include phase in SMC measurements |
|
Examples |
SENS:MIX:PHAS 1 sense2:mixer:phase off |
|
Query Syntax |
SENSe<ch>:MIXer:PHASe? |
|
Return Type |
Boolean |
|
0 (OFF) |
|
|
Applicable Models: All (Write-only) Sets the VNA to DUT port map for FCA measurements. Use SENS:MIX:PMAP:INP? and SENS:MIX:PMAP:OUTP? to read these values. Learn about selectable FCA DUT ports. Changing the ports may limit your ability to use an internal second source. If a selected port is shared by one of the sources, then that source will not be available as an LO source. Learn more about Internal second sources. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<in> |
VNA port to connect to the DUT input.
|
|
<out> |
VNA port to connect to the DUT output. Choose any unused port for SMC and VMC. |
|
Examples |
SENS:MIX:PMAP 2,1 |
|
Query Syntax |
Not Applicable |
|
1,2 |
|
![]()
|
Applicable Models: All (Read-only) Returns the VNA port that is mapped to the DUT input. Use SENS:MIX:PMAP to set this value. Learn about selectable FCA DUT ports. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
Examples |
SENS:MIX:PMAP:INP? |
|
1 |
|
![]()
|
Applicable Models: All (Read-only) Returns the VNA port that is mapped to the DUT output. Use SENS:MIX:PMAP to set this value. Learn about selectable FCA DUT ports. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
Examples |
SENS:MIX:PMAP:OUTP? |
|
2 |
|
![]()
|
Applicable Models: All (Write only) Repeats the last calculation that was performed, including all ON (state) segments in segment table. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
Examples |
SENS:MIX:REC |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets whether to include SC12 sweeps during measurements. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<bool> |
(Boolean) Choose from: ON (1) - Include the SC12 (reverse) sweep. OFF (0) - Do NOT Include the SC12 (reverse) sweep. |
|
Examples |
SENS:MIX:REV 1 |
|
Query Syntax |
SENSe<ch>:MIXer:REVerse? |
|
Return Type |
Boolean |
|
ON (1) |
|
![]()
|
Applicable Models: All (Read-only) This command is replaced with SENSe:ROLE:CATalog which can be used by all channels. Returns a list of valid roles for the IMD Converter application. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
Examples |
SENS:MIX:ROLE:CAT? |
|
Not Applicable |
|
![]()
|
Applicable Models: All (Read-Write) This command is replaced with SENSe:ROLE:DEVice which can be used by all channels. Assigns a configured external source to the specified role for the converter application. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<role> |
(String) Role to which the external source is assigned. Choose from: For IMDX and IMSX, choose from: "RF2" "LO1" "LO2" For all other converter applications, choose from: "LO1" "LO2" |
|
<source> |
String) Source name from Source Configuration dialog. |
|
Examples |
SENS:MIX:ROLE:DEV "LO1","LO1Name" |
|
Query Syntax |
SENSe<ch>:MIXer:ROLE:DEVice? <source> |
|
Return Type |
String |
|
Not Applicable |
|
![]()
|
Applicable Models: All (Write-only) Saves the settings for the mixer/converter test setup to a mixer attributes file. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<name> |
Path and file name (including .mxrx extension) to save. |
|
Examples |
SENSe:MIXer:SAVE "C:/Program Files/Keysight/Network Analyzer/Documents/Mixer/MyMixer.mxrx" |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Number of IF stages (LOs) used in the mixer. See Note |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
Number of stages. Choose either 1 or 2 |
|
Examples |
SENSe1:MIXer:LO1:FREQ:NUMerator 6 |
|
Query Syntax |
SENSe<ch>:MIXer:STAGe? |
|
Return Type |
Numeric |
|
1 |
|
|
Applicable Models: All (Read-Write) Sets or returns the swept frequency range to display on the X-axis for the IMDx or NFx channel. For FCA and GCX measurements, use CALC:MEAS:MIXer:XAXis |
|
|
Parameters |
|
|
<ch> |
Channel number of the IMDx or NFx Converter measurement. If unspecified, value is set to 1. |
|
<char> |
Frequency range to display on the X-Axis. NOT case-sensitive. Choose from:
If the specified frequency range is not swept, the default swept range is used. |
|
Examples |
SENSe:MIXer:XAXis INPUT sense2:mixer:xaxis LO_1 |
|
Return Type |
Character |
|
Search is made in the following order until a swept range is found:
|
|