File  |  Instrument  |  Response  |  Stimulus  |  Utility  |  Cal  |  Apps  |  Remote ONLY


 

Save /Recall | Manage Files | Manage Folders | Print | Read Clock
Preset (User) | Security | Configure
Hdwr & Capabilities | Macros | Status | GPIB Pass-through | VISA Pass-through | Preferences

LXI | Error Messages |

Preset / User

SCPI

Preset

SYSTem:PRESet

*RST

Preset plus delete window

SYSTem:FPReset

 

Security

Frequency Blanking

SYSTem:SECurity[:LEVel]

 

Configure

Local Lockout

Local Lockout

Set and return GPIB address

None

Set VNA to GPIB system controller or talker/listener

None

Set and return SICL address

None

Control the VNA via SICL

None

Return Full computer name

None

System Impedance

SENSe:CORRection:IMPedance:INPut:MAGNitude

Load Test Set Config file and Restart VNA.

SYSTem:CONFigure

Hardware

Instrument Menu

IO Configuration

None

Modify the manufacturer name

SYSTem:PERSona:MANufacturer

Reset to original manufacturer identification

SYSTem:PERSona:MANufacturer:DEFault

Modify the product model

SYSTem:PERSona:MODel

Reset to original product model name

SYSTem:PERSona:MODel:DEFault

Set and return Source Port Control

SYSTem:ISPControl[:STATe]

 

Hardware and Capabilities

DSP Revision

SYSTem:CONFigure:REVision:DSP?

DSP FPGA

SYSTem:CONFigure:REVision:DSPFpga?

CPU Speed

SYSTem:CONFigure:REVision:CPU?

Hostname

SYSTem:COMMunicate:LAN:HOSTname?

Disk Drive Version

SYSTem:DISK:REVision?

Set and return the coupler state

SYSTem:FCORrection:CHANnel:COUPler[:STATe]

Returns the word size (32 or 64).

SYSTem:CONFigure:BIT?

Many queries regarding the capability of a specific VNA

SYSTem:CAPability

 

Macros

Execute Macro

SYSTem:SHORtcut:EXECute

Delete Macro

SYSTem:SHORtcut:DELete

Write macro path, argument, and title

SYSTem:SHORtcut:PATH

SYSTem:SHORtcut:ARGuments

SYSTem:SHORtcut:TITLe

Read macro path, argument, and title

 

Status Commands

Status Registers

GP-IB/Status Registers

*OPC;*WAI

GP-IB/Common_Commands

 

GPIB Pass Through

Open a GPIB pass-through session

SYSTem:COMMunicate:GPIB:RDEVice:OPEN

None

Write string data to the GPIB pass-through device.

SYSTem:COMMunicate:GPIB:RDEVice:WRITe

None

Write data to the GPIB pass-through device - with header.

SYSTem:COMMunicate:GPIB:RDEVice:WBLock

None

Write data to the GPIB pass-through device - without header.

SYSTem:COMMunicate:GPIB:RDEVice:WBINary

None

Reads string data from the GPIB pass-through device.

SYSTem:COMMunicate:GPIB:RDEVice:READ?

None

Closes a GPIB pass-through session

SYSTem:COMMunicate:GPIB:RDEVice:CLOSe

None

Closes ALL GPIB pass-through sessions

SYSTem:COMMunicate:GPIB:RDEVice:RESet

None

 

VISA Pass Through

Returns list of visa address strings or aliases.

SYSTem:COMMunicate:VISA:RDEVice:FIND?

Sets timeout value for VISA pass-through commands.

SYSTem:COMMunicate:VISA:RDEVice:TIMeout

 

Preferences

Reset Preference default settings

SYSTem:PREFerences:DEFault

Touchscreen ON | Off

SYSTem:TOUChscreen[:STATe]

Selected trace is wider

None

Selected trace changes width briefly

None

Cal: Auto-save User Cal Set

SENSe:CORRection:PREFerence:CSET:SAVE

Cal: For Guided Cal, set external trigger

SENSe:CORRection:PREFerence:TRIG:FREE

Cal: For Unguided Cal, set external trigger

SENSe:CORRection:PREFerence:TRIG:FREE

Cal: Simulated Cal Behavior

SENSe:CORRection:PREFerence:SIMCal

Cal: Use Primary FOM (for mmWave)

SENSe:CORRection:PREFerence:CALibration[:FOM]:RANGe

Cal: Use legacy behavior for Series-C & Shunt-L fixtures

SYSTem:PREFerences:ITEM:FIXTure:CIRCuit:DEFAults

Cal: Use Unknown thru math for SOLT methods

SYSTem:PREFerence:ITEM:USOLt

Memory: Data Math 8510 Mode

None

Power: RF power On during frequency sweep retrace

SYSTem:PREFerences:ITEM:RETRace:POWer

Power: Power Sweep Retrace

SYSTem:PREFerences:ITEM:PSRTrace

Trigger: External Trigger OUT is Global

TRIGger:PREFerences:AIGLobal

Meas: Port 1 Noise Tuner Switch state

SYSTem:PREFerences:ITEM:SWITch:DEF

Meas: Mathematical offset for receiver attenuation

SYSTem:PREFerences:ITEM:OFFSet:RCV

Meas: Mathematical offset for source attenuation

SYSTem:PREFerences:ITEM:OFFSet:SRC

Limit: Draw failed trace segments in red

SYSTem:PREFerences:ITEM:RTOF

Limit: Draw limit lines in red

SYSTem:PREFerences:ITEM:REDLimits

Marker: Programming treats Mkr 10 as Reference

SYSTem:PREFerences:ITEM:REFMarker

Marker: On Preset, Coupled Markers is ON

SYSTem:PREFerences:ITEM:MCPreset

Marker: On Preset, Coupling Method is Channel

SYSTem:PREFerences:ITEM:MCMethod

Marker: Coupling controls on|off state of markers.

SYSTem:PREFerences:ITEM:MCControl

Marker: Use single marker for marker search

SYSTem:PREFerences:ITEM:MARKer:SINGle

Marker: Sets the bandwidth search preference

SYSTem:PREFerences:ITEM:MARKer:BANDwidth:SEARch

Ext Device: de-activate on PRESET and recall.

SYSTem:PREFerences:ITEM:EDEV:DPOLicy

Avg: On PRESET set two-point group delay aperture

SYSTem:PREFerences:ITEM:GDELay:TWOPoint

Power: On PRESET always turn power ON

SYSTem:PREFerences:ITEM:PRESet:POWer

Power: Report source unleveled events as errors

SYSTem:ERRor:REPort:SUNLeveled

Power: Turn source power OFF when receiver is overloaded

SYSTem:PREFerences:ITEM:RECeivers:OVERload:POWer

Power: Report when receiver is overloaded

SYSTem:PREFerences:ITEM:RECeivers:CERRor

Preset: Confirm preset

SYSTem:PREFerences:ITEM:PRESet:CONFirm

Preset: On PRESET show Quick Start dialog

SYSTem:PREFerences:ITEM:QSTart

Controls the on/off state of the preference, "Use keyboard to navigate softkeys"

SYSTem:PREFerences:ITEM:SOFTkeys:NAVigation

Sweep: Use only ramp sweeps for Auto Sweep Mode

SYSTem:PREFerences:ITEM:ASMRamp

System: Enable Sound

SYSTem:BEEPer:STATe

System: Set limit test warning sound

SYSTem:BEEPer:WARNing:IMMediate

System: Set sound after operation completion

SYSTem:BEEPer:COMPlete:IMMediate

System: On Power-on show Keys toolbar

SYSTem:PREFerences:ITEM:Keys

System: Use parallel processing

SYSTem:PREFerences:ITEM:CORRection:PARallel:PROCess

System: Set front panel remote state when a SCPI command is received

SYSTem:PREFerences:ITEM:REMote:AUTO[:STATe]

Ext Reference: Modify Settings on Preset and Recall

SYSTem:PREFerences:ITEM:ROSCillator:RECall

More buttons

Define Data Saves

See File Menu

User Preset

See Preset

Printer Page Setup

Hardcopy

Power Limit

See Power Limits

Display and Print Colors

See Display

 

LXI

Returns Structured status of the VNA networking configuration.

None

Returns string status of the VNA networking configuration.

None

Resets the VNA LAN configuration.

None

Modifies settings of the VNA computer networking configuration.

None

Displays the LAN Status dialog with LAN Status Indicator showing IDENTIFY.

LXI:IDEN

 

Error Messages

Enable the display of Error Messages

DISPlay:ANNotation:MESSage:STATe

Timed vs Dialog messages

None