Configuring the Channel Setup View
In this view, the configuration summary table differs from the Waveform and Carrier view. The table changes from a carrier summary to a channel summary. In addition, two of the buttons above the table change from selecting predefined carriers and adding new carriers to selecting predefined channel setups and adding new channels.
Change the Channel Configuration
Only perform this procedure if you want to change to another predefined channel setup.
When you select another predefined channel setup, it replaces all of the channels showing in the configuration summary table for the current carrier. This causes the loss of any previously configured channel settings.
-
Click the predefined channel configuration button.
-
From the dialog box, select the desired predefined channel setup.
Notice that the new channel configuration appears in the channel configuration summary table..
Add a Channel
The software places the new channel just above the channel highlighted in the configuration summary table. For some of the channel selections, you are also given a selection of data rates. You can modify this data rate after the channel selection by using the
cell in the channel property pane.-
In the channel configuration summary table, select a channel.
-
Click the add new channel button.
-
From the drop-down menu, select a channel to add.
Downlink
Uplink
The new channel appears above the highlighted channel.
Delete a Channel
The software provides the convenience of deleting a single channel or multiple channels.
-
In the configuration summary table, select the channel or channels that require deletion.
To select multiple channels, use the keyboard
key operation to select channels in succession (a group) or the key to select multiple individual channels. -
Click the delete button above the configuration summary table.
Configure or Modify Channel Parameters
-
Select
> .Having the status window open provides greater visibility to errors. Error messages appear in two places: in the status bar at the bottom of the UI, and in the status window. In the status window, they appear with a large red dot, which helps to alert you to an error. The status window also lists all uncorrected errors, whereas the status bar only shows the most recent uncorrected error.
-
In the channel configuration summary table, select a channel .
-
Select a cell in the property pane.
-
Configure the channel parameter for either downlink or uplink as dictated by the carrier type (downlink or uplink).
CCDF Graph
CDP Graph