Cal Commands - Standard Measurement Class

Click here to view links to Cal commands for all Measurement Classes.

Main

Port
Extension

Cal Sets
& Cal Kits

Fixtures

Main Tab Commands
Softkey Sub-item SCPI
Basic Cal... Connector SENSe:CORRection:COLLect:CKIT:CONNector:ADD
Cal Kit SENSe:CORRection:COLLect:CKIT[:SELect]
Show all cal kits SENSe:CORRection:COLLect:CKIT:CATalog?
Cal Type SENSe:CORRection:COLLect:METHod
Other Cals Cal All...
Select the channels to be calibrated SYSTem:CALibrate:ALL:SELect
Use Smart Cal Order SYSTem:CALibrate:ALL:MCLass:PROPerty:VALue[:STATe]
Enable Extra Power Cals SYSTem:CALibrate:ALL:MCLass:PROPerty:VALue[:STATe]
Independent Calibration Channels SYSTem:CALibrate:ALL:MCLass:PROPerty:VALue[:STATe]
Include Power Calibration SYSTem:CALibrate:ALL:MCLass:PROPerty:VALue[:STATe]
Set the IFBW SYSTem:CALibrate:ALL:IFBW
Set the power level SYSTem:CALibrate:ALL:PORT:SOURce:POWer
Set the power offset SYSTem:CALibrate:ALL:PORT:SOURce:POWer:OFFSet
Set the receiver atten SYSTem:CALibrate:ALL:PORT:SOURce:POWer:ATTen
Set the User Calset Prefix SYSTem:CALibrate:ALL:CSET:PREFix
Set Path Configuration SYSTem:CALibrate:ALL:PATH:CONFigure:ELEMent
Read unique Cal properties SYSTem:CALibrate:ALL:MCLass:PROPerty:NAME:CATalog?
Read unique property values SYSTem:CALibrate:ALL:MCLass:PROPerty:VALue:CATalog?
Set property name/value SYSTem:CALibrate:ALL:MCLass:PROPerty:VALue
Read primary Cal channel SYSTem:CALibrate:ALL:GUIDed:CHANnel[:VALue]?
Returns all cal all guided calibration channels SYSTem:CALibrate:ALL:GUIDed:CHANnel:LIST?
Get Guided Cal handle None
For each channel, sets the ports to be calibrated SYSTem:CALibrate:ALL:CHANnel:PORTs
Returns a final list of ports to be calibrated SYSTem:CALibrate:ALL:GUIDed:PORTs?
Read generated Cal Sets SYSTem:CALibrate:ALL:CSET:CATalog?
Independent Power Calibration  

Return available ports

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:CATalog?

Add a power cal range

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:ADD

Reset all ranges

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:CLEar

Query how many ranges are included

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:COUNt?

Set number of points

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:POINts

Set start frequency

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:STARt

Set stop frequency

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:STOP

Smart Cal...
Initiate a Guided Cal SENSe:CORRection:COLLect:GUIDed:INITiate

Returns a text description (string) of the current calibration settings.

SENSe<ch>:CORRection:COLLect:GUIDed:CONFig:DESCription?

Loads the calibration configurations from file and commits all settings.

SENSe<ch>:CORRection:COLLect:GUIDed:CONFig:LOAD[:IMMediate] <string>

Returns a text description (string) of the calibration settings contained in the specified filename.

SENSe<ch>:CORRection:COLLect:GUIDed:CONFig:LOAD:DESCription? <string>

Save the current guided calibration settings to file.

SENSe<ch>:CORRection:COLLect:GUIDed:CONFig:SAVE <string>

List valid Connector Types for a Port SENSe:CORRection:COLLect:GUIDed:CONNector:CATalog?
List valid Cal Kits for a Connector type SENSe:CORRection:COLLect:GUIDed:CKIT:CATalog?
Select a Connector Type SENSe:CORRection:COLLect:GUIDed:CONNector:PORT
Select a Cal Kit SENSe:CORRection:COLLect:GUIDed:CKIT:PORT
Set cal method for each port pair SENSe:CORRection:COLLect:GUIDed:PATH:CMEThod
Set Thru Method for each port pair SENSe:CORRection:COLLect:GUIDed:PATH:TMEThod
Set Thru Port Pairs SENSe:CORRection:COLLect:GUIDed:THRU:PORTs
Return Number of Steps in a Cal SENSe:CORRection:COLLect:GUIDed:STEPs?
Return a Description of a Cal Step SENSe:CORRection:COLLect:GUIDed:DESCription?
Measure a Cal Standard in a Guided Cal SENSe:CORRection:COLLect:GUIDed:ACQuire
Save Cal SENSe :NOISe:EXDC:CATalog?
List of available DC Sources used to control the noise source  
E Cal...
Specify Module and Characterization SENSe:CORRection:COLLect:ACQuire
Do ECAL 1-Port SENSe:CORRection:COLLect:CKIT 99
Do ECAL 2-Port SENSe:CORRection:COLLect:CKIT 99
Get ECAL Module Info SENSe:CORRection:COLLect:CKIT:INFormation? SENSe:CORRection:CKIT:ECAL:INFormation?
Get list of ECal Modules attached to PNA SENSe:CORRection:CKIT:ECAL:LIST?
Get list of characterizations in ECal module SENSe:CORRection:CKIT:ECAL:CLISt?
Perform Module Orientation during calibration SENSe:CORRection:PREFerence:ECAL:ORIentation
Maps ECAL Module to PNA Ports SENSe:CORRection:PREFerence:ECAL:PMAP
Reads ECal orientation SENSe:CORRection:CKIT:ECAL:ORIent?
Perform ECal Isolation SENSe:CORRection:COLLect:ISOLation:ECAL
Increment Avg for ECal Isolation SENSe:CORRection:COLLect:ISOLation:AVERage:INCRement
Response Cal...
Launch Cal Wizard SYSTem:CORRection:WIZard
Set Cal Type SENSe:CORRection:COLLect:METHod
Select a Cal Kit SENSe:CORRection:COLLect:CKIT
Get a Handle to the Active Cal Kit None
Simultaneous 2-Port Calibration SENSe:CORRection:TSTandards
Acquisition Direction SENSe:CORRection:SFORward
Measure a Standard SENSe:CORRection:COLLect
Calculate Errors SENSe:CORRection:COLLect:SAVE
Do Isolation SENSe:CORRection:COLLect
Perform and apply Response (Normalization) cal SENSe:CORRection:COLLect:METHod

Source Power Cal...

Copy Source Power cal to another channel

SYSTem:MACRo:COPY:CHANnel:SOURce

GPIB Power Meter Address

SYSTem:COMMunicate:PSENsor

Set source power cal method

SOURce:POWer:CORRection:COLLect:ACQuire

Turn correction ON|OFF

SOURce:POWer:CORRection

Applies correction values after completing a source power cal acquisition sweep

Optionally do reference receiver cal

SOURce:POWer:CORRection:COLLect:SAVE

Returns the currently-selected power sensor channel (A or B) for use at a specific frequency

None

Set power level

SOURce:POWer:CORRection:LEVel

Set power offset

SOURce:POWer:CORRection:OFFSet

Set settling tolerance

SOURce:POWer:CORRection:COLLect:AVERage:NTOLerance

Set max readings for settling

SOURce:POWer:CORRection:COLLect:AVERage:COUNt

Set accuracy tolerance

SOURce:POWer:CORRection:COLLect:ITERation:NTOLerance

Set max readings for accuracy

SOURce:POWer:CORRection:COLLect:ITERation:COUNt

Turn ON|OFF display of readings

SOURce:POWer:CORRection:COLLect:DISPlay

Acquire receiver-only readings

SOURce:POWer:CORRection:COLLect:ACQuire

Initiates a source power cal acquisition

SOURce:POWer:CORRection:COLLect:ACQuire

Aborts a source power cal acquisition sweep that is currently in progress

SOURce:POWer:CORRection:COLLect:ABORt

Launches the Configure Power Sensor dialog on the PNA

None

Frequency checking (ON|OFF)

SOURce:POWer:CORRection:COLLect:FCHeck

Check test port power

None

Calibrate the source at multiple power levels

None

Cal Update...

Select Channel

SYSTem:CALibrate:CALupdate:CHANnels[:SELect]

Reference Cal Set

SYSTem:CALibrate:CALupdate:REFerence

IF Bandwidth

SYSTem:CALibrate:CALupdate:BWIDth[:RESolution]

Averaging

SYSTem:CALibrate:CALupdate:AVERage:COUNt

Power

SYSTem:CALibrate:CALupdate:SOURce:POWer

Auto

SYSTem:CALibrate:CALupdate:SETTings:AUTO

Auto-Calculate Gates

None

Select

SYSTem:CALibrate:CALupdate:PORTs[:SELect]

Gate Start

SYSTem:CALibrate:CALupdate:GATE:STARt

Gate Start Couple

SYSTem:CALibrate:CALupdate:GATE:STARt:COUPle[:STATe]

Gate Stop

SYSTem:CALibrate:CALupdate:GATE:STOP

Gate Stop Couple

SYSTem:CALibrate:CALupdate:GATE:STOP:COUPle[:STATe]

Initialize

SYSTem:CALibrate:CALupdate:INITialize

Recorrect

SYSTem:CALibrate:CALupdate:RECorrect

Advanced

 

    Enable All Cal Updates

None

    Disable All Cal Updates

None

   Delete All Cal Update Cal Sets

None

   Set Dialog to Defaults

None

Correction Channel Correction On SENSe:CORRection:STATe
Channel Correction Off SENSe:CORRection:STATe
Cal Set...
Create a Cal Set SENSe:CORRection:CSET:CREate
Delete a Cal Set CSET:DEL
List Cal Sets CSET:CATalog?
List Cal Sets in PNA None
Get Cal Set Information None
List Cal Set Error Terms SENSe:CORRection:CSET:ETERm:CATalog?
Return if a Cal Set exists CSET:EXISts?
Select a Cal Set by GUID SENSe:CORRection:CSET:ACTivate
Apply a Cal Set to a channel SENSe:CORRection:CSET:ACTivate
Copy a Cal Set SENSe:CORRection:CSET:COPY
Save a Cal Set SENSe:CORRection:CSET:SAVE
Save Cal Sets None
Automatically save to User Cal Set SENSe:CORRection:PREFerence:CSET:SAVE
Change the Description of a Cal Set SENSe:CORRection:CSET:DESCription
Change the Name of a Cal Set SENSe:CORRection:CSET:NAME
Recall a Cal File MMEMory:LOAD
Save 'in-memory' Cal Set to disk. SENSe:CORRection:CSET:FLATten
Create Cal Set with De-embeded fixture removed CSET:FIXTure:DEEMbed
Create Cal Set with Matching Network included CSET:FIXTure:EMBed
Adds stimulus data to a specific buffer None
Returns the stimulus values over which the specific error term was acquired None
Returns FOM stimulus values from a Calset SENSe:CORRection:CSET:STIMulus?
Returns the Cal Types from the calset None
Returns the properties of the calset None
Returns the numbers of the channels using the calset None
Unselect Cal Set SENSe:CORRection:CSET:DEACtivate

Factory Cal

ON/OFF

SYSTem:FCORrection:CHANnel:COUPler[:STATe]

Src Power Correct

ON/OFF

SOURce:POWer:CORRection[:STATe]

Interpolation ON/OFF SENSe:CORRection:INTerpolate[:STATe]

Correction Methods...

Power Correction Type SENSe:CORRection:WAVE[:METHod]

 

Enable Port Subset Correction SENSe:CORRection:METHods:PORT:SUBSet:[:STATe]

 

Select Ports in Subset SENSe:CORRection:METHods:PORT:SUBSet:FULL[:VALue]

 

Clear All SENSe:CORRection:METHods:PORT:SUBSet:RESet

 

(SA Class) Select Ports Will Correct Power Using Actual Waves SENSe:CORRection:METHods:SA:PORT
Correction Properties...   None
Port Extension Tab Commands
Softkey Sub-item SCPI
Select Port N SENSe:CORRection:EXTension:PORT
Port Extension ON/OFF SENSe:CORRection:EXTension
Time   SENSe:CORRection:EXTension:PORT:TIME
Distance   SENSe:CORRection:EXTension:PORT:DISTance
Velocity Factor   SENSe:CORRection:RVELocity:COAX
DC Loss   SENSe:CORRection:EXTension:PORT:LDC
Port Extensions... Extensions ON|OFF SENSe:CORRection:EXTension
Port 1 Extensions Value SENSe:CORRection:EXTension:PORT
Port 2 Extensions Value SENSe:CORRection:EXTension:PORT
Set Freq 1|2 SENSe:CORRection:EXTension:PORT:FREQuency
Set Loss 1|2 SENSe:CORRection:EXTension:PORT:LOSS
Use 1|2 SENSe:CORRection:EXTension:PORT:INCLude
Set Loss at DC SENSe:CORRection:EXTension:PORT:LDC
Relative Velocity SENSe:CORRection:RVELocity:COAX
Port Ext in distance SENSe:CORRection:EXTension:PORT:DISTance
Set distance units SENSe:CORRection:EXTension:PORT:UNIT
Set Media per port SENSe:CORRection:EXTension:PORT:MEDium
Set waveguide cutoff freq per port SENSe:CORRection:EXTension:PORT:WGCutoff
Set Velocity Factor per port SENSe:CORRection:EXTension:PORT:VELFactor
Couple to system Velocity Factor SENSe:CORRection:EXTension:PORT:SYSVelocity
Couple to system Media type SENSe:CORRection:EXTension:PORT:SYSMedia
Auto Port Extension... Measure OPEN or SHORT for Auto Port Ext SENSe:CORRection:EXTtension:AUTO:MEASure
Sets the frequencies used for Auto Port Ext. calculation SENSe:CORRection:EXTension:AUTO:CONFig
Include loss correction in Auto Port Ext SENSe:CORRection:EXTension:AUTO:LOSS
Include DC Offset in Auto Port Ext SENSe:CORRection:EXTension:AUTO:DCOFfset
Enable specified port for Auto Port Ext SENSe:CORRection:EXTension:AUTO:PORT<n>
Clears old port extension delay and loss data SENSe:CORRection:EXTension:AUTO:RESet
Set user span start frequency for Auto Port Ext SENSe:CORRection:EXTension:AUTO:STARt
Set user span stop frequency for Auto Port Ext SENSe:CORRection:EXTension:AUTO:STOP
Cal Sets & Cal Kits Tab Commands
Softkey Sub-item SCPI

Cal Set...

  CSET
Cal Set Viewer ON/OFF DISPlay:TOOL:CSET[:STATe]
Cal Kit... Set a Cal Kit Active SENSe:CORRection:COLLect:CKIT
Clear all Cal Kits from PNA SENSe:CORRection:CKIT:CLEar
Get a Handle to the Active Cal Kit None
Save All Cal Kits after Modifying None
Load collection of Kits SENSe:CORRection:CKIT:LOAD
Load (Recall) All Cal Kits None
Import a specified kit SENSe:CORRection:CKIT:IMPort
Restore Cal Kit Default SENSe:CORRection:CKIT:INITialize
Restore ALL Cal Kits Default SENSe:CORRection:CKIT:INITialize
Build a Hybrid Cal Kit None
Set the Name of a Cal Kit SENSe:CORRection:COLLect:CKIT:NAME
Set a description of a Cal Kit SENSe:CORRection:COLLect:CKIT:DESCription
Get the amount of installed kits SENSe:CORRection:CKIT:COUNt?
Set the Port Label of a Cal Kit None
Saves a Cal Kit to a file SENSe:CORRection:CKIT:EXPort

ECal...

 
Cal Pod...

Command used to send other commands as arguments

CONTrol:CALPod:COMMand

Start the CalPod software

Calpod:LAUNch

Assign Calpod serial number to a port.

Calpod:ENABle

Unassign Calpod serial number from a port.

Calpod:Disable

Initialize the selected channel

Calpod:INITialize:ACTive

Initialize ALL channels

Calpod:INITialize:ALL

Recorrect the selected channel

Calpod:Recorrect:ACTive

Recorrect ALL channels

Calpod:Recorrect:ALL

Show refresh dialog

Calpod:SHOW

Hide refresh dialog

Calpod:HIDE

Sets impedance state

Calpod:STATe

Read Calpod temperature

Calpod:TEMP?

Uncertainty Setup...

Trace Type

CALCulate:UNCertainty:DISPlay:TYPE

Coverage factor value

CALCulate:UNCertainty:DISPlay:CFACtor

Noise contribution

CALCulate:UNCertainty:MODE:NOISe

Cable/connection repeatability contribution

CALCulate:UNCertainty:MODE:CABLe:REPeat

Error term uncertainties

CALCulate:UNCertainty:MODE:ETERm

Save uncertainty data

CALCulate:UNCertainty:SAVE

Add Trace

None

Apply to all traces

None

Fixtures Tab Commands
Softkey Sub-item SCPI

Fixture Simulator Draft and Fixture Simulator Active

 

Copy draft fixture to active fixture

CALCulate:FSIMulator:DRAFt:APPLy

CALCulate:FSIMulator:APPLy

Discards changes on scratch/draft fixture

CALCulate:FSIMulator:DRAFt:DISCard

Saves SNP file corresponding to the entire scratch fixture

CALCulate:FSIMulator:DRAFt:SAVE

Saves SNP file corresponding to the entire active fixture

CALCulate:FSIMulator:SAVE

Loads an active fixture topology file

CALCulate:FSIMulator:TOPology:LOAD

Saves an active fixture topology file

CALCulate:FSIMulator:TOPology:SAVE

Sets and returns on power compensation for the active fixture

CALCulate:FSIMulator:POWer:PORT:COMPensate[:STATe]

Section State Switches

Turns port extensions ON and OFF for all ports

CALCulate:FSIMulator:DRAFt:SECTion:EXTension:ENABle

CALCulate:FSIMulator:SECTion:EXTension:ENABle?

Turns all circuits ON and OFF for all ports

CALCulate:FSIMulator:DRAFt:SECTion:CIRCuit:ENABle

CALCulate:FSIMulator:SECTion:CIRCuit:ENABle?

Turns all ZConversions ON and OFF (both SE and BAL)

CALCulate:FSIMulator:DRAFt:SECTion:ZCONversion:ENABle

CALCulate:FSIMulator:SECTion:ZCONversion:ENABle?

Circuit Section

Returns a comma-separated list of circuit numbers created in the draft circuit

CALCulate:FSIMulator:DRAFt:CIRCuit:CATalog?

CALCulate:FSIMulator:CIRCuit:CATalog?

Returns the next free circuit number than be used to create a new circuit block

CALCulate:FSIMulator:DRAFt:CIRCuit:NEXT?

Create a block of the specified block type with the specified fixture port count

CALCulate::FSIMulator:DRAFt:CIRCuit:ADD

Deletes the specified circuit

CALCulate:FSIMulator:DRAFt:CIRCuit:DELete

Sets the VNA ports for the specified circuit

CALCulate:FSIMulator:DRAFt:CIRCuit:VNA:PORTs

CALCulate:FSIMulator:CIRCuit:VNA:PORTs?

Sets the Device ports for the specified circuit

CALCulate:FSIMulator:DRAFt:CIRCuit:DEVice:PORTs

CALCulate:FSIMulator:CIRCuit:DEVice:PORTs?

Sets the resistance circuit element

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:R

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:R2

CALCulate:FSIMulator:CIRCuit:PARameter:R?

CALCulate:FSIMulator:CIRCuit:PARameter:R2?

Sets the inductance circuit element

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:L

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:L2

CALCulate:FSIMulator:CIRCuit:PARameter:L?

CALCulate:FSIMulator:CIRCuit:PARameter:L2?

Sets the capacitance circuit element

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:C

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:C2

CALCulate:FSIMulator:CIRCuit:PARameter:C?

CALCulate:FSIMulator:CIRCuit:PARameter:C2?

Sets the conductance circuit element

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:G

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:G2

CALCulate:FSIMulator:CIRCuit:PARameter:G?

CALCulate:FSIMulator:CIRCuit:PARameter:G2?

Sets the impedance (Z0) for the ideal block (scalar value).

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:Z0

CALCulate:FSIMulator:CIRCuit:PARameter:Z0?

Sets the R value at output of transformer (real only)

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:ROUT

CALCulate:FSIMulator:CIRCuit:PARameter:ROUT?

Sets the R value at input of transformer (real only)

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:RIN

CALCulate:FSIMulator:CIRCuit:PARameter:RIN?

Sets port extension delay in time

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:DELay

CALCulate:FSIMulator:CIRCuit:PARameter:DELay?

Sets the loss at DC

CALCulate:FSIMulator:DRAFt:CIRCuit:PARameter:LOSS:VALue

CALCulate:FSIMulator:CIRCuit:PARameter:LOSS:VALue?

Sets the filename

CALCulate:FSIMulator:DRAFt:CIRCuit:FILE

CALCulate:FSIMulator:CIRCuit:FILE?

Sets whether or not extrapolation is allowed

CALCulate:FSIMulator:DRAFt:CIRCuit:FILE:EXTRapolate

CALCulate:FSIMulator:CIRCuit:FILE:EXTRapolate?

Sets/gets the label on the file block.

CALCulate:FSIMulator:DRAFt:CIRCuit:FILE:LABel

CALCulate:FSIMulator:CIRCuit:FILE:LABel?

embedded or de-embedded?

CALCulate:FSIMulator:DRAFt:CIRCuit:EMBED:TYPE

CALCulate:FSIMulator:CIRCuit:EMBED:TYPE?

Turns the circuit ON and OFF

CALCulate:FSIMulator:DRAFt:CIRCuit:STATe

CALCulate:FSIMulator:CIRCuit:STATe?

Impedance Conversion

Sets the differential port impedance conversion function ON/OFF

CALCulate:FSIMulator:DRAFt:ZCONversion:DIFFerential:STATe

CALCulate:FSIMulator:ZCONversion:DIFFerential:STATe?

Sets the complex impedance value for differential port impedance

CALCulate:FSIMulator:DRAFt:ZCONversion:DIFFerential:BPORt:COMPLex

CALCulate:FSIMulator:ZCONversion:DIFFerential:BPORt:COMPLex?

CALCulate:FSIMulator:ZCONversion:DIFFerential:LPORt:COMPLex?

Sets the real impedance value for differential port impedance

CALCulate:FSIMulator:DRAFt:ZCONversion:DIFFerential:BPORt:SCALar

CALCulate:FSIMulator:DRAFt:ZCONversion:DIFFerential:LPORt:SCALar

CALCulate:FSIMulator:ZCONversion:DIFFerential:BPORt:SCALar?

CALCulate:FSIMulator:ZCONversion:DIFFerential:LPORt:SCALar?

Sets the common mode port impedance conversion function ON/OFF

CALCulate:FSIMulator:DRAFt:ZCONversion:COMMonmode:STATe

CALCulate:FSIMulator:ZCONversion:COMMonmode:STATe?

Sets the complex impedance value for common mode port impedance

CALCulate:FSIMulator:DRAFt:ZCONversion:COMMonmode:BPORt:COMPLex

CALCulate:FSIMulator:DRAFt:ZCONversion:COMMonmode:LPORt:COMPLex

CALCulate:FSIMulator:ZCONversion:COMMonmode:BPORt:COMPLex?

CALCulate:FSIMulator:ZCONversion:COMMonmode:LPORt:COMPLex?

Sets the real impedance value for common mode port impedance

CALCulate:FSIMulator:DRAFt:ZCONversion:COMMonmode:BPORt:SCALar

CALCulate:FSIMulator:DRAFt:ZCONversion:COMMonmode:LPORt:SCALar

CALCulate:FSIMulator:ZCONversion:COMMonmode:BPORt:SCALar?

CALCulate:FSIMulator:ZCONversion:COMMonmode:LPORt:SCALar?

Sets the single-ended ZCONV ON/OFF

CALCulate:FSIMulator:DRAFt:ZCONversion:SENDed:PORT:STATe

Sets the complex impedance value for SE port impedance

CALCulate:FSIMulator:DRAFt:ZCONversion:SENDed:PORT:COMPLex

CALCulate:FSIMulator:ZCONversion:SENDed:PORT:COMPLex?

Sets the real impedance value for SE port impedance

CALCulate:FSIMulator:DRAFt:ZCONversion:SENDed:PORT:SCALar

CALCulate:FSIMulator:ZCONversion:SENDed:PORT:SCALar?

Port Extension

Sets delay in time

CALCulate:FSIMulator:DRAFt:EXTension:PORT:DELay

CALCulate:FSIMulator:EXTension:PORT:DELay?

Sets delay in physical distance

CALCulate:FSIMulator:DRAFt:EXTension:PORT:DISTance:VALue

CALCulate:FSIMulator:EXTension:PORT:DISTance:VALue?

Sets unit for port extension distance

CALCulate:FSIMulator:DRAFt:EXTension:PORT:DISTance:UNIT

CALCulate:FSIMulator:EXTension:PORT:DISTance:UNIT?

Sets frequency value for "loss1" or "loss2"

CALCulate:FSIMulator:DRAFt:EXTension:PORT:LOSS:FREQuency

CALCulate:FSIMulator:EXTension:PORT:LOSS:FREQuency?

Sets loss value for "loss1" or "loss2"

CALCulate:FSIMulator:DRAFt:EXTension:PORT:LOSS:VALue

CALCulate:FSIMulator:EXTension:PORT:LOSS:VALue?

Turns "loss1" or "loss2" ON/OFF

CALCulate:FSIMulator:DRAFt:EXTension:PORT:LOSS:STATe

CALCulate:FSIMulator:EXTension:PORT:LOSS:STATe?

Sets media type

CALCulate:FSIMulator:DRAFt:EXTension:PORT:MEDium

CALCulate:FSIMulator:EXTension:PORT:MEDium?

Sets waveguide cutoff frequency

CALCulate:FSIMulator:DRAFt:EXTension:PORT:WAVEguide:FCUToff

CALCulate:FSIMulator:EXTension:PORT:WAVEguide:FCUToff?

Sets couple to system media

CALCulate:FSIMulator:DRAFt:EXTension:PORT:WAVEguide:COUPle

CALCulate:FSIMulator:EXTension:PORT:WAVEguide:COUPle?

Sets velocity factor

CALCulate:FSIMulator:DRAFt:EXTension:PORT:VELocity:FACtor

CALCulate:FSIMulator:EXTension:PORT:VELocity:FACtor?

Sets coupling to system velocity factor

CALCulate:FSIMulator:DRAFt:EXTension:PORT:VELocity:COUPle

CALCulate:FSIMulator:EXTension:PORT:VELocity:COUPle?

Sets the port loss at DC

CALCulate:FSIMulator:DRAFt:EXTension:PORT:DCLoss:VALue

CALCulate:FSIMulator:EXTension:PORT:DCLoss:VALue?

Turns port extension ON/OFF

CALCulate:FSIMulator:DRAFt:EXTension:PORT[:STATe]

CALCulate:FSIMulator:EXTension:PORT[:STATe]?

Moves the port extension block to the right-most side of the circuit sections

CALCulate:FSIMulator:DRAFt:EXTension:PORT:END

Apply Fixtures ON/OFF CALCulate:FSIMulator:STATe
Power Comp... Port N

CALCulate:FSIMulator:POWer:PORT:COMPensate:STATe

Compensate Only For De-Embeds

CALCulate:FSIMulator:POWer:COMPensate:MODE

Fixture Setup

Change order of operations

CALCulate:FSIMulator:SENDed:OORDer

2 and 4-port Extrapolate

CALCulate:FSIMulator:SNP:EXTRapolate

2-Port Fixturing

Port matching ON and OFF

CALCulate:FSIMulator:SENDed:PMCircuit:STATe

Reverse ports

CALCulate:FSIMulator:SENDed:DEEM:PORT<n>:SNP:REVerse

Sets Port Matching circuit model

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:TYPE

Sets Port Matching 'S2P' file name

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:USER:FILename

Sets Capacitance 'C' value

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:C

Sets Conductance 'G' value

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:G

Sets Inductance 'L' value

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:L

Sets Resistance 'R' value

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:R

De-embed ON and OFF

CALCulate:FSIMulator:SENDed:DEEMbed:STATe

Sets De-embedding circuit model

CALCulate:FSIMulator:SENDed:DEEMbed:PORT

Sets De-embedding 'S2P' file name

CALCulate:FSIMulator:SENDed:DEEM:PORT:USER:FILename

Port Impedance ON and OFF

CALCulate:FSIMulator:SENDed:ZCONversion:STATe

Port Z Real

CALCulate:FSIMulator:SENDed:ZCONversion:PORT:REAL

Port Z Imag

CALCulate:FSIMulator:SENDed:ZCONversion:PORT:IMAG

Port Z Real and Imag

CALCulate:FSIMulator:SENDed:ZCONversion:PORT:Z0

4-Port Network Embed/De-embed commands

Specifies the PNA / DUT topology

CALCulate:FSIMulator:EMBed:TYPE

Specifies the 4-port touchstone file

CALCulate:FSIMulator:EMBed:NETWork:FILename

Embed|De-embed?

CALCulate:FSIMulator:EMBed:NETWork:TYPE

Specify PNA port connections

CALCulate:FSIMulator:EMBed:TOPology:A:PORTs

CALCulate:FSIMulator:EMBed:TOPology:B:PORTs

CALCulate:FSIMulator:EMBed:TOPology:C:PORTs

CALCulate:FSIMulator:EMBed:TOPology:D:PORTs

4-port remap

CALCulate:FSIMulator:EMBed:NETWork<n>:PMAP

Turn ON or OFF

CALCulate:FSIMulator:EMBed:STATe

Differential Port Arbitrary Impedance

Sets the impedance value

CALCulate:FSIMulator:BAunL:DZConversion:BPORt:Z0

Sets real part of impedance

CALCulate:FSIMulator:BALun:DZConversion:BPORt:REAL

Sets imaginary part of impedance

CALCulate:FSIMulator:BALun:DZConversion:BPORt:IMAG

Turn ON or OFF

CALCulate:FSIMulator:BALun:DZConversion:STATe

Common Mode Port Arbitrary Impedance

Sets the impedance value

CALCulate:FSIMulator:BALun:CZConversion:BPORt:Z0

Sets real part of impedance

CALCulate:FSIMulator:BALun:CZConversion:BPORt:REAL

Sets imaginary part of impedance

CALCulate:FSIMulator:BALun:CZConversion:BPORt:IMAG

Turn ON or OFF

CALCulate:FSIMulator:BALun:CZConversion:STATe

Differential Port Matching

Sets type of circuit to embed

CALCulate:FSIMulator:BALun:DMCircuit:BPORt

Specifies the 2-port touchstone file

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:USER:FILename

Sets Capacitance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:C

Sets Conductance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:G

Sets Inductance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:L

Sets Resistance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:R

Turns ON/OFF

CALCulate:FSIMulator:BALun:DMCircuit:STATe

Remote ONLY

Create Cal Set with De-embeded fixture removed

CSET:FIXTure:DEEMbed

Create Cal Set with Matching network included

CSET:FIXTure:EMBed

Cal Plane Manager...   Characterize a fixture

CSET:FIXTure:CHARacterize

Creates a single S2P file from two existing files

CSET:FIXTure:CASCade

Auto Fixture Removal...

 

CSET:FIXTure:DEEMbed