Calibrate All Channels


"Cal All" allows you to calibrate multiple channels in a single calibration session.  This not only reduces the number of connections that need to be made, but also the number of cal standard measurements that must be performed.

In this topic:

Other Cal Topics

See Also

Features

Cal All offers a single, optimized calibration procedure for all channels (with some limitations, see below).  The optimizations include:

Beginning with the A.18.40 release, Cal All supports the following internal setting difference. Call All takes all required calibration data for each setting below during the Call All sequence.

M983xA

Limitations

How to perform a Cal All Channels Calibration

Using Hardkey/SoftTab/Softkey

  1. Press Cal > Other Cals > Cal All....

Programming Commands

 

Selected Channels dialog box help

  1. Check the channels to be calibrated.

  2. Check the ports to be calibrated. Click on the Apply to all channels button to apply the port selections to all channels.

  3. Click Next>

 

Measurement Class Cal Properties dialog box help

 

A warning dialog will be displayed if any of the ports being calibrated have pulse modulators enabled.

Typically, cal all will perform all calibration steps with background channels and will never enable pulse during the calibration steps.

In this case, the warning is just informative. There is nothing that needs to be changed.

 

However, cal all allows some channels to be calibrated as “Independent Channels”.

(These app types can be set as independent channels in cal all: STD, SMC, GCA, GCX, NF, NFX, IMD, IMDX).

Independent channels are calibrated using the exact stimulus of the active channel.  

For channels declared as “Independent”, the user may choose to turn off pulse during the power cal. 

When finished, all user channels will retain their original settings.

 

Confirm or change the following unique cal properties for each channel to be calibrated. Click a link to learn about these properties.

The properties with (NOT available in Cal All) are NOT available in a Cal All calibration as they are in a stand-alone calibration.

Differential IQ

 

Programming

UI Setting

Property

Value

Enable Extra Power Cals

"Enable Extra Power Cals"

"Port 1", "Port 2", "Port 3", "Port 4", "Port 1 Src2", and/or Source3

Independent Calibration Channels

"Independent Calibration Channels"

Any selected channels that support SmartCal.

Split Port Calibration Channels

"Split Port Calibration Channels" 

Any selected channels that support Split Port Cal.

Channels may optionally include a port-group list to perform an N-port split cal as a single calibration. A port that is not listed in any group is calibrated as a single-port group (a 1-port cal -- the original Split Port Cal behavior).

See the Split Port Cal section below for the full syntax.

Examples (assume each channel has 4 ports):

"1,2,3" -- channels 1, 2, 3 with every port calibrated as a single-port group (1-port cal per port; the original Split Port Cal behavior).

"1(1,2)" -- channel 1 with ports 1 and 2 grouped as a 2-port cal; ports 3 and 4 default to single-port groups (1-port cal each).

"1(1,2)(3,4)" -- channel 1 with two 2-port cals (ports 1-2 and ports 3-4).

Extra Power Cals Will Use Different Cal Plane "Extra Power Cals Will Use Different Cal Plane"

"true" (Extra Power Cals will use a different plane)

"false" (Extra Power Cals will be at the S-parameter calibration plane)

Spectrum Analyzer

 

Programming

UI Setting

Property

Value

Calibration Span

Calibration Span

"User Span" or "Instrument Span"

Calibration Points

Calibration Points

Integer indicating number of calibration points.

Enable Extra Power Cals

"Enable Extra Power Cals"

"Port 1", "Port 2", "Port 3", "Port 4", "Port 1 Src2", and/or Source3

Independent Calibration Channels

"Independent Calibration Channels"

Any selected channels that support SmartCal.

Gain Compression

 

Programming

UI Setting

Property

Value

Enable Extra Power Cals

"Enable Extra Power Cals"

"Port 1", "Port 2", "Port 3", "Port 4", "Port 1 Src2", and/or Source3

Independent Calibration Channels

"Independent Calibration Channels"

Any selected channels that support SmartCal.

GCX (Gain Compression Converters)

 

Programming

UI Setting

Property

Value

Enable Extra Power Cals

"Enable Extra Power Cals"

"Port 1", "Port 2", "Port 3", "Port 4", "Port 1 Src2", and/or Source3

Independent Calibration Channels

"Independent Calibration Channels"

Any selected channels that support SmartCal.

Split Port Calibration Channels

"Split Port Calibration Channels" 

Any selected channels that support Split Port Cal.

Channels may optionally include a port-group list to perform an N-port split cal as a single calibration. A port that is not listed in any group is calibrated as a single-port group (a 1-port cal -- the original Split Port Cal behavior).

See the Split Port Cal section below for the full syntax.

Examples (assume each channel has 4 ports):

"1,2,3" -- channels 1, 2, 3 with every port calibrated as a single-port group (1-port cal per port; the original Split Port Cal behavior).

"1(1,2)" -- channel 1 with ports 1 and 2 grouped as a 2-port cal; ports 3 and 4 default to single-port groups (1-port cal each).

"1(1,2)(3,4)" -- channel 1 with two 2-port cals (ports 1-2 and ports 3-4).

Noise Figure and NFX

Note: Calibrate All Channels for Noise Figure measurement channels is not supported on M980xA, P50xxA/B and E5080B.

 

Programming

UI Setting

Property

Value

Cal Method

"Noise Cal Method"

"Scalar"

"Vector"

Noise Tuner (used with Vector Cal Method)

"AutoOrient Tuner"

"true" - AutoOrient

"false" - Do NOT autoOrient

When "AutoOrient Tuner" = false
(Manually Orient)

"Tuner In"

"Tuner Out"

Tuner port connected to DUT input

Tuner port connected to DUT output

For example: "A" or "B"

Receiver Characterization Method

"Receiver Characterization Method"

"Use Power Meter"

"Use Noise Source"

Note: When selecting "Use Power Meter", the power cal step must be completed first when acquiring the calibration. Furthermore, the power cal port must be the same as the input port on the NF channel.

Specify the Noise Source connector - used for the 1 port cal if needed.

"Noise Source Connector"

String name of valid connector type.

To query valid connector types:

COM: ValidConnectorTypes

SCPI: SENS:CORR:COLL:GUID:CONN:CAT?

Specify the Noise Source cal kit - used for the 1 port cal if needed.

"Noise Source CalKit"

String name of valid cal kit.

To query valid cal kits names:

COM:GetCompatibleCalKits

SCPI: SENS:CORR:COLL:GUID:CKIT:CAT?

Specify ENR file

"ENR File"

String path and filename of the ENR file.

Include Power Calibration

"Include Power Calibration"

"Enable Extra Power Cals"

"Port 1 Src2 Cal Power"

"true" or "false"

"Port 1", "Port 2", "Port 3", "Port 4", and/or "Port 1 Src2"

Integer indicating valid calibration power. For example, "-20" indicates a power level of -20 dBm. Only valid if an independent port calibration on Port 1 Src2 is selected.

"Noise Tuner"

Tuner description in the form of <model> ECal <serialNumber>, as in “N4691-60004 ECal 10775”.

“Force Thru Adapter De-embed”

“true” – Always measure and de-embed the thru adapter.

“false” – Only measure and de-embed the thru adapter if no flush thru is possible.

“Force Noise Source Adapter De-embed”

“true” – Always measure and de-embed the noise source adapter.

“false” – Only measure and de-embed the adapter if no direct connection is possible.

“Cal Receiver Port Only at Low Frequencies”

Only available when doing scalar downconverter calibrations on PNAs with a max frequency of 40 GHz or higher.

“true” – only make receiver port measurements during cal at downconverted frequencies.

“false” – make receiver port measurements during cal at both input and output frequencies

“Noise Source Temperature”

The cold temperature of the noise source, in Kelvin.

USB Noise Source

"USB Noise Source"

Note: This property available when noise figure channels are included.

“usbNsSrcID” (example:  “U1831C MY12345678”)

Note: This indicates to use the specified USB Noise Source. If “ENR File” is not specified, will use the internal USB

Meas Noise Params

"Measure Noise Receiver Parameters"

“true” – Measure the noise parameters of the noise receiver

“false” – Do not measure the noise parameters of the noise receiver

Swept IMD and IMDX

 

Programming

UI Setting

Property

Value

Max Product Order

"Max Product Order"

Integer indicating desired product order.

Include 2nd Order

"Include 2nd Order"

"true" or "false"

Exclude 2nd Order

"Exclude Channels From 2nd Order"

 

Enable Extra Power Cals

"Enable Extra Power Cals"

"Port 1", "Port 2", "Port 3", "Port 4", "Port 1 Src2", and/or Source3

Independent Calibration Channels

"Independent Calibration Channels"

Any selected channels that support SmartCal.

Split Port Calibration Channels

"Split Port Calibration Channels" 

Any selected channels that support Split Port Cal.

Channels may optionally include a port-group list to perform an N-port split cal as a single calibration. A port that is not listed in any group is calibrated as a single-port group (a 1-port cal -- the original Split Port Cal behavior).

See the Split Port Cal section below for the full syntax.

Examples (assume each channel has 4 ports):

"1,2,3" -- channels 1, 2, 3 with every port calibrated as a single-port group (1-port cal per port; the original Split Port Cal behavior).

"1(1,2)" -- channel 1 with ports 1 and 2 grouped as a 2-port cal; ports 3 and 4 default to single-port groups (1-port cal each).

"1(1,2)(3,4)" -- channel 1 with two 2-port cals (ports 1-2 and ports 3-4).

Response only
(NOT available in Cal All)

 

 

Center Frequencies only
(NOT available in Cal All)

 

 

MOD (Modulation Distortion) and MODX (Modulation Distortion Converters)

 

Programming

UI Setting

Property

Value

Enable Extra Power Cals

"Enable Extra Power Cals"

"Port 1", "Port 2", "Port 3", "Port 4", "Port 1 Src2", and/or Source3

Independent Calibration Channels

"Independent Calibration Channels"

Any selected channels that support SmartCal

Calibration Span (MOD only)

"Calibration Span"

"User Span" or "Instrument Span"

Calibration Points (MOD only)

"Calibration Points"

Integer indicating number of calibration points

Enable Phase Correction (MODX only)

"Enable Phase Correction"

"true" or "false"

Phase Correction Method (MODX only)

"Phase Correction Method"

"Use Mixer Delay"

"Use Receiver Characterization Calset"

Calset (MODX only)

"Calset"

String of Cal Set Name

SMC (VMC is NOT offered)

 

Programming

UI Setting

Property

Value

Use Smart Cal Order

"Use Smart Cal Order"

true or false

Cal All optimizes the order of the calibration standards for acquisition to improve calibration results. This may result in a different order than a single channel Smart Calibration. Use “True” to have Cal All attempt to preserve the order of Smart Cal.

  depending on the client channels selected for calibration, this may not be possible due to incompatible order between channels.

Enable Phase Correction

"Enable Phase Correction"

"true" or "false"

Phase Correction Method

"Phase Correction Method"

"Use Mixer Delay"

"Use Characterized Mixer"

"Use Receiver Characterization Calset"

Mixer Delay

"Mixer Delay"

Real number indicating delay value.

Receiver Characterization Cal Set

"Calset"

String of Cal Set Name

Enable Extra Power Cals

"Enable Extra Power Cals"

"Port 1", "Port 2", "Port 3", "Port 4", "Port 1 Src2", and/or Source3

Independent Calibration Channels

"Independent Calibration Channels"

Any selected channels that support SmartCal.

Split Port Calibration Channels

"Split Port Calibration Channels"  

Any selected channels that support Split Port Cal.

Channels may optionally include a port-group list to perform an N-port split cal as a single calibration. A port that is not listed in any group is calibrated as a single-port group (a 1-port cal -- the original Split Port Cal behavior).

See the Split Port Cal section below for the full syntax.

Examples (assume each channel has 4 ports):

"1,2,3" -- channels 1, 2, 3 with every port calibrated as a single-port group (1-port cal per port; the original Split Port Cal behavior).

"1(1,2)" -- channel 1 with ports 1 and 2 grouped as a 2-port cal; ports 3 and 4 default to single-port groups (1-port cal each).

"1(1,2)(3,4)" -- channel 1 with two 2-port cals (ports 1-2 and ports 3-4).

Characterized mixer (s2p file)
(NOT available in Cal All)

 

 

Phase Import Port

"Phase Import Port"

"Autoselect", "Port 1", "Port 2", etc.

Standard Channel

 

Programming

UI Setting

Property

Value

Include Power Calibration

"Include Power Calibration"

"Enable Extra Power Cals"

"Port 1 Src2 Cal Power"

"true" or "false"

"Port 1", "Port 2", "Port 3", "Port 4", "Port 1 Src2", and/or Source3

Integer indicating valid calibration power. For example, "-20" indicates a power level of -20 dBm. Only valid if an independent port calibration on Port 1 Src2 is selected.

Independent Calibration Channels

"Independent Calibration Channels"

Any selected channels that support SmartCal.

The power cal is optional only if none of the selected channels require a power cal.

 

Setting Up an Independent Power Calibration

Independent Power Calibration

Several applications control internal and external sources in a mode that is often decoupled from the span over which the receivers are swept. This includes, for instance, Differential IQ, and Spectrum Analyzer. Cal All can add a power calibration for any port (including external sources) over an arbitrary frequency span defined by the user.

For all ports selected for an independent power calibration (except for Port 1 Src 2, see below), a power sensor calibration measurement is performed. The resulting source match correction terms are added to the calsets for ALL channels selected for the Cal All calibration. The power calibrations used in Cal All have all the same features as typical power calibrations. These include the ability to specify power offsets, the power at which the calibration is completed, and the ability to use multiple power sensors (note that using multiple power sensors is a feature only available on regular PNA ports – that is, not external sources or auxiliary ports).

Port 1 Src2 Calibration

The Port 1 Src2 calibration is a special case: In this case, a calibration is requested for situations where the Port 1 Bypass Switch is in “Combiner Path” mode and either the “Port 3 Bypass Switch” (4-port PNA-X) or the “Source 2 out 1 Bypass Switch” (2-port 2-source PNA-X) is also in “Combiner Path”. Therefore, if a user requests a calibration of this port:

  1. Port 1 will also be calibrated at the same frequencies in the combiner path (*note:  The user can still elect to add more Port 1 independent cal ranges, but this will be done in “Bypass” mode, not “Combiner mode.”

  2. The calibrations for both Port 1 and Port 1 Src2 will be done with both sources on, but offset by 10MHz (to more accurately characterize the behavior during use).

  3. These calibrations will ONLY be applied to user channels in which both the Port 1 Bypass Switch and either the Port 3 or Source 2 Out 1 Bypass Switches are set to “Combiner Path.”

Important Notes:

  • If a user selects an independent power calibration on a port also used for the typical S-parameter calibration, then the frequencies calibrated will be in addition to those frequencies used via the typical calibration (a separate measurement will be completed at the time).
  • Previously a user could select a similar calibration of “LO” ports for application channels (for instance, in a GCX measurement with Port 3 used for LO1, a user can select (via GUI or remote) to do an “LO1” calibration.  This will do a power sensor calibration of LO1 (port 3) at the frequencies specified by the channel.  This is still available, but if the user selects to do an Independent Power Calibration instead, this will override the selection by the channel.
  • If the user has a mixture of LFE (Low Frequency Extension) and non-LFE channels the calibration will be done by default in the NON-LFE configuration (this is because most applications do not support LFE and external sources and sources like Src2 Out 1 do not have LFE paths).  Instead, if it’s desired to do these calibrations in LFE mode, the user must select only LFE channels over which to do the cal all calibration.

  • If setting up the calibration remotely, it is not necessary to set the power cal state for the extra power calibrations (for example, “SENS200:CORR:COLL:GUID:PSEN2 ON”). These state commands should only be used to specify the power cal port for the main calibration.

Independent Power Calibration versus Adding "LO Ports" to Calibration:

  1. LO Ports can be added for Mixer Channels on the first Wizard Page 
            
  1. Use this when you want Cal All to determine the frequencies for the power cal as needed by that particular channel.  This works very well for mixer applications like SMC, GCX, NFX, etc.  Frequencies are determined by Cal All and depends on what was set up in the channel(s), and the power calibration is applied only to the channel(s) where the LO port was selected.
  2. Alternatively, “Independent Power Calibrations” should be used for channels where it is not obvious what frequencies or ports are used explicitly for LO inputs, or when an arbitrary tone is needed.  For example, this applies to channels like DIQ or SA, or STD channel in FOM mode.  In this case, frequencies are determined explicitly by the user and the power calibration is applied to ALL channel(s) participating in Cal All.

Important Notes:

  •  If the user is performing both LO calibrations as well as Independent Power Calibrations on the same ports, then the frequencies from the Independent Power Calibration will OVERRIDE the frequencies chosen automatically by Cal All for specific channels.  Therefore, the user should choose their frequencies carefully.  If the frequencies do not cover the range, they will get an error similar to this: 

     

     

    Independent Power Calibration for Cal All Setup

    • If the user is performing both LO calibrations as well as Independent Power Calibrations on the same ports, then the frequencies from the Independent Power Calibration will OVERRIDE the frequencies chosen automatically by Cal All for specific channels.  Therefore, the user should choose their frequencies carefully.  If the frequencies do not cover the range, they will get an error similar to this:
      1. Start the Cal All Wizard.
      2. In the Measurement Class Cal Properties dialog, enable Independent Power Calibration by selecting the port(s) to cal then clicking OK.
      1. If Port 1 Scr2 is a selected port, the Port 1 Src2 Cal Power level is displayed allowing a calibration power level to be entered.
      1. To enter the Port 1 Src2 Cal Power level, click in the field then enter a valid calibration power level.
      1. In the Power Cal Settings for  Port<n> dialog, select the port from the Power cal at dropdown.
      2. To add a new Cal range, click the New button.
      3. Specify a frequency range for each Range Name by clicking in the corresponding Settings field then clicking on the Edit button that appears.
      1. Enter the Start and Stop frequency and the number of Points then click OK.
      2. Continue the Cal All process by clicking on the Next button.

 

Split Port Cal 

Beginning with firmware revision A.18.40, there are new attributes called Split Port Cal that allow channels to perform the calibrations without a thru calibration. When a thru calibration is difficult to take, it is possible to execute 1 port calibration only for each port. This is called as "Split Port" Cal.

This feature is available in GCX, SMC, DIQ, and IMDX measurement classes only. DIQ and IMDX are available starting in A.19.10.

Note: This feature replaces "Split Cal," which was available between A.13.67 and A.17.60.

Note: Frequencies chosen for DIQ channels will be:
a. Source Frequencies, if source is Auto ON or Always ON
b. Frequencies used in parameter definitions
If frequency range for calibration is unexpected, examine parameter definitions.

 

When you click ..., the channels which support Split Port cal are displayed (DIQ, IMDX, GCX, SMC). Select the channel which you want to execute the calibration without thru.

Class  Displays the measurement class of the channel.

Split  Select the checkbox to enable the Split Cal. Those channels are enabled will be displayed in the Split Port Calibration Channels row of the Measurement Class Cal Properties  dialog.

Port Groups  Displays the list of port groups being calibrated. Parentheses indicate which ports are grouped together.

For example:

  • (1,2) (3) indicates that ports 1 and 2 are grouped together, while port 3 forms a separate group.

  • (1) (2) indicates that ports 1 and 2 are independent and are not grouped.

For channels that do not support port grouping (for example, a 2-port channel), the field still displays the port configuration as independent groups, such as (1) (2).

 

... Button  Click on this button will open the Port Groups dialog to define port groups. Button is displayed for IMDX and DIQ (if it has more than two ports). Button is not available for GCX, SMC and DIQ (if it has less than three ports). 

The active channel is displayed at the title bar. The number of groups equals to the number of ports.

 

Ports  List of ports contained in each group. Each group of ports will be calibrated together.  For example, if the user wants to perform a two port calibration between ports 1 and 2, then they must be in the same group. Selecting a row will highlight it in blue and will be displayed in the Select Ports group box below. 

 

Select Ports  This displays only choices for ports selected to be calibrated in the "Cal All" dialog. 

Rules for assigning ports: 

  • Default:  One port will be assigned to each group.  

  • User may select or unselect any ports. 

  • All ports must be assigned to a group. Removing a port from one group will automatically add it to an empty group. 

  • No port may be assigned to more than one group.  Adding a port to a group will remove that port from its previous group. 

  • A group may contain one port and a group may contain no port. 

Defaults  Sets the default state for the selected channel which will assign one port to each group.

OK   Apply the Port Groups to the currently selected channel and close the dialog.

 

On the last Cal All Wizard page, the Description column specifies whether the channel is being calibrated by Cal All or performing its own calibration: If it is being calibrated by Cal All, it displays which Cal All channel is performing the calibration.

(Scrolled to the left)


(Scrolled to the right)

Multi-Port Group Syntax (firmware revision A.xx.xx and later)

The "Split Port Calibration Channels" property accepts an optional group list following each channel number. A group is a parenthesized, comma-separated list of ports that are calibrated together as a single N-port cal. Any port that is not listed in any group is calibrated as a single-port group -- that is, a 1-port cal on that port -- which is the original Split Port Cal behavior. The legacy form "1,2,3" (channel numbers only) is therefore equivalent to "every port on those channels gets a 1-port cal", unchanged from prior releases. 

 

Format

Each entry in the comma-separated list is a channel number, optionally followed by one or more port groups in parentheses. A port group is a parenthesized, comma-separated list of port numbers. Whitespace is ignored. 

<channel>(<port>,<port>,...)(<port>,<port>,...) ..., <channel>(<port>,<port>,...)(<port>,<port>,...) ..., ... 

The parenthesized port groups are optional and may repeat. A channel with no group list defaults to single-port groups on every port.  

 

Examples (assume each channel has 4 ports)

Value 

Meaning 

"1,2,3" 

Channels 1, 2, 3. No groups listed -- every port is calibrated as a single-port group (1-port cal per port). Equivalent to the pre-existing behavior. 

"1" 

Channel 1. No groups listed -- every port is calibrated as a single-port group (1-port cal per port). 

"1(1,2)" 

Channel 1: ports 1 and 2 are grouped and calibrated together as a 2-port cal. Ports 3 and 4 default to single-port groups (1-port cal each). 

"1(1,2)(3,4)" 

Channel 1: two 2-port cals (ports 1-2 and ports 3-4). 

"1(1,2),2,3" 

Channel 1: ports 1 and 2 grouped as a 2-port cal; ports 3 and 4 default to single-port groups. Channels 2 and 3: every port is a single-port group. 

"1(1)(2)(3)(4)" 

Equivalent to "1" -- explicit single-port groups are accepted but functionally identical to omitting the group list. 

 

Rules

  • A channel number may appear at most once. 

  • A port may appear in at most one group within the same channel. 

  • Ports not listed in any group are treated as default single-port groups (the legacy behavior is preserved). 

  • The following are rejected and leave the property unchanged. The set command returns SCPI error +1073, "Unexpected error; String is invalid. <reason>" (the set is not partially applied). The <reason> text identifies which condition triggered the reject: 

    • Syntax errors (mismatched parentheses, non-integer tokens). 

      • <reason> = Syntax error. 

    • Empty port group, e.g. "1()". 

      • <reason> = Channel <n> has an empty port group. 

    • Duplicate channel entries, e.g. "1(1,2),1(3,4)". 

      • <reason> = Channel <n> is used more than once. 

    • A port appears more than once within the same channel, whether across groups (e.g. "1(1,2)(2,3)") or within the same group (e.g. "1(1,1)"). 

      • <reason> = Port <p> on channel <n> appears more than once. 

    • Zero or negative channel or port numbers. 

      • <reason> = Channel or port number must be positive. 

  • When the input contains more than one of the conditions above, only the first one encountered during parsing is reported; the remaining conditions are not surfaced in <reason>. Fix the reported issue, resend the command, and inspect the next error if any. 

  • The following are silently filtered (the rest of the value is accepted): 

    • Channel numbers that do not exist. 

    • Channels whose measurement class does not support Split Port Cal. 

  • Ports listed in a group that are not selected by SYST:CAL:ALL:CHAN<n>:PORT:SEL are excluded at calibration time. The property value itself is not modified. 

Query

The query returns the value with single-port groups omitted -- a port not listed in any group has the same meaning as an explicit single-port group, so the parenthesized form is normalized away. 

 

Set 

Query returns

"1" 

"1" 

"1,2,3" 

"1,2,3" 

"1(1)(2)(3)(4)" 

"1" 

"1(1,2)(3)(4)" 

"1(1,2)" 

"1(1,2)(3,4)" 

"1(1,2)(3,4)" 

"1(1,2),2,3" 

"1(1,2),2,3" 

 

Backward Compatibility

The legacy channel-only form (e.g., "1,2,3") remains valid. Stored state files, Cal Sets, and existing SCPI scripts continue to work without modification. 

 

 

 Independent Calibration Channels

Beginning with firmware revision A.13.67,there are new attributes called Independent Calibration Channels that allow channels to perform the calibrations as a independent calibration a SmartCal. This is an advanced feature. For example, it can make the calibration better by avoiding additional calculations associated with path difference betweem channels on the PNA.

Any selected channels will perform their own SmartCal instead of importing the calibration from the SmartCal performed on the special Cal All channel (typically Channel 200).

 

Note: Channels that do not support their own SmartCal cannot be Independent Calibration Channels. They will be filtered out if selected as Independent Calibration Channels.

Example of Cal All Process

The following is an example showing the typical Cal All process using three standard channels:

Ch 1: 1-2 GHz, 101 points

Ch 2: 2-3 GHz, 101 points

Ch 3: 3-4 GHz, 101 points

 

Cal All process without Independent Calibration Channel selections:

  1. Creates a Cal All channel (typically Channel 200), which goes from 1-4 GHz, 303 points. 

  2. Cal All tells the  Cal All channel to perform a SmartCal.

  3. When the calibration is done, the SmartCal on the Cal All channel computes the error terms, and passes them to Ch1, Ch2, and Ch3.

Cal All process with channel 3 selected as an Independent Calibration Channel:

  1. Creates a Cal All channel (typically Channel 200), which goes from 1-3 GHz, 202 points. 

  2. Cal All tells the Cal All channel to perform a SmartCal.

  3. Cal All tells Ch 3 to perform its own SmartCal.

  4. When the calibration is done:

    1. Channel 200 SmartCal computes error terms, and passes them to Ch1 and Ch2.

    2. Ch 3 computes its own error terms (since it performed its own SmartCal).

For any channels that are 1) Split Port Cal (SMC/GCX/MODX), 2) Cal Receiver Port Only at Low Frequency (banded noise only), or 3) Independent Calibration Channels, note the following:

  • These channels will be performing their own SmartCal calibrations and will NOT inherit a calest from the Cal All calibration.

  • Connection lists will be organized such that even if several channels are performing the same connection as part of their calibration the user will be prompted only once. For example, if channels 2, 3, and 200 (CalAll channel) will be needing a power sensor on port one, then the user will be prompted once for this connection, and channels 2,3, and 200 will take power sweeps consecutively.

  • Settings made from the GUI apply to all active calibrations. If a user wants to set different calibration settings, use the remote UI (with the appropriate channel number). The only exception is that the user may choose specific calibration powers (if allowed) for each channel performing its own Calibration. This is accomplished using the SENSe:CORRection:COLLect:GUIDed:PSENsor:POWer:LEVel SCPI command and the PowerCalibrationPowerLevel COM command.  From the GUI, this is accomplished in the following Power Cal Page:


Note: Some channels do not support setting the cal power level. If this is the case, then the field will be disabled.

On the last Cal All Wizard page, the Description column specifies whether the channel is being calibrated by Cal All or performing its own calibration: If it is being calibrated by Cal All, it displays which Cal All channel is performing the calibration.

(Scrolled to the left)


(Scrolled to the right)

Note: If a user chooses to Enable Extra Power Cals, then the only client channels that are participating in Cal All as normal will inherit the corresponding power calibration terms (this is most often used with SA, which cannot be an Independent Calibration Channel).

  

Extra Power Cals at Different Cal Plane

DiffIQ Cal All property, "Extra Power Cals Will Use Different Cal Plane", which enables source power calibration at a different cal plane within a single Cal All session. This feature applies to DiffIQ only. 

  Property value: True or False. This property is available only when all selected channels in the Cal All session are DiffIQ. When set to True, the extra source power cal at a different cal plane is performed for the ports configured by the existing "Enable Extra Power Cals" property. 

  When this property is set to True, Cal All performs the following for the ports specified by "Enable Extra Power Cals": 

  1. Places the extra power cals as the last step in Cal All. 

  1. Writes only the SourcePowerCorrection array and Response Tracking(a*) array to the calset for the extra cal — does not combine with the results from the regular S-Parameter + Power Guided Cal. 

 

Calibration Attenuator Settings dialog box help

This dialog shows the Power, Attenuator, and IFBW settings for the Cal All calibration. The default values for the Cal All session are the preset values of a standard S-parameter channel. These values are not necessarily the same as those of the channels that are selected for calibration. When there are differences in measurement path (switch) settings between the Cal All channel and the selected channels, these differences are detected by Cal All and additional measurements are made for each path condition. These additional measurements allow Cal All to produce error terms appropriate for each of the selected channels. In general, the Cal All session should be performed at a power level that is high enough to prevent noise in the error terms. However, an increase in power could cause compression or damage to the analyzer receivers. The following settings allow you to increase the power level ONLY during the Cal All session.

Note: The following settings do not apply to Independent Calibration Channels. Those calibrations are performed using the power and attenuation settings as configured in the channel.

Power Limit (Disable)

Cal All shows you when power limits are enabled.  This setting provides you a convenient way to TEMPORARILY disable these limits in order to take advantage of the power settings available in Cal All.  If power limits are on, your DUT is probably a high-gain device and the attenuator settings in your channels are high resulting in lower power at the cal reference plane.  This lower signal can result in noisier measurements during the acquisition of cal. This situation is precisely what Cal All is intended to improve.  Cal All allows you to configure the calibration conditions for better signal-to-noise performance during the cal while leaving your DUT conditions alone. You can elect to clear the “Disable Power Limits during cal” checkbox when you prefer to calibrate at a higher power level than is allowed by your limit. The limit is restored after the Cal All session.

Source / Receiver Attenuator

By default, the Cal All calibration is performed with Source and Receiver attenuators set to 0. Change the Source or Receiver attenuator settings when external hardware (such as a booster amplifier) would cause the analyzer receivers to be compressed or damaged.

You may also want to change the attenuator or path configuration settings to force the cal channel to match settings of the selected channels. If all of the selected channels are set to identical hardware settings, it may be better to apply these settings to the cal channel. For example, if your channels all use a 5 or 10 dB attenuator step at port 1, you might elect to change the Cal All channels to use the same low attenuator settings.  This will result in the cal measurements being made under the same path conditions as the channel and it will eliminate the need to mathematically compensate for the difference.  However, if large attenuator values are used, the default Cal All settings will likely improve your results.

S-Parameter Cal Port Power

Set the power level at which the S-Parameter cal is performed.

Power Offsets

Power Offsets are channel-scoped. Consequently, offsets that you already set are NOT automatically copied to the Cal All session.  This setting allows you to also apply a Power Offset during the Cal All session. Learn about Power Offsets.

Noise Reduction

This button accesses the following dialog for settings that help reduce trace noise and the noise floor which can lead to better dynamic range and more accurate measurements. Learn more.

IF Bandwidth

Set the IFBW used to perform the Cal All calibration. The default IFBW setting of 1 kHz is a good nominal setting for most measurements. Lowering the IFBW removes noise from the calibration measurement, but also causes slower sweeps.

Always ON

Check to enable averaging.

Average Factor

Specifies the number of measurements that are averaged. Range of 1 to 65536 (2^16).

Average Type

Sweep  Each data point is based on the average of the same data point measured over consecutive sweeps.

(Sweep) Restart   Begins a new set of measurements that are used for the average. Applies only to Sweep averaging - NOT Point.

Point   Each data point is measured the number of times specified by the Average Factor, and then averaged, before going to the next data point.

Reduce IF BW at Low Frequencies

When this box is checked, the VNA uses a smaller IF Bandwidth than the selected value. Learn more.

Note: [M983xA] Turning ON makes the sweep slower.  Turn OFF and select the proper IF BW manually could save the sweep time.

 

Select DUT Connectors and Cal Kits dialog box help

For each DUT port:

  • Select the connector at the calibration reference plane (where the cal standards will be connected).

  • Select the cal kit to be used.

Check Modify Cal to change the Thru method. An Unknown Thru cal is performed by default. Learn about THRU methods.

Learn more about this dialog.

 

Power Cal Settings dialog box help

A guided power cal is performed on the source ports for the Cal All calibration.

This dialog is displayed for each source port to receive a power cal.

To perform an LO power cal for a mixer channel, set the LO port to a VNA or external source in the Mixer Setup dialog. Then select that port in the Selected Channels dialog.

 

  • To use the same power sensor for all power cals, select One Power Sensor under Cal using pulldown list. 

  • To use different power sensors, select Multiple Sensors under Cal using pulldown list. The sensor must be configured as a PMAR device. Learn how.

  • To import the power calibration error terms from an existing calset that contains power calibration, select Import Power Cal under Cal using pulldown list. 

  • Select Source PMax Table under Cal using pull down list, this primarily used to calibrate the source of the millimeter head when no sensor is available.

Learn about this dialog box.

 

Cal All Summary  dialog box help

This page is a summary of the Cal All settings. Confirm the settings, then click Next > or < Back to change settings.

 

Cal Steps  dialog box help

Follow the prompts to connect each standard. Then click Measure.

Click Re-measure if necessary.

Then click Next >

 

 

Finish Cal  dialog box help

Click Finish to save the Cal All session results to Cal Registers.

Or click Save As User CalSet, then enter a prefix title. The Meas Class and channel number are appended to this prefix to save to a User Cal Set for each calibrated channel.

Learn more about this dialog.