Last updated: February 12, 2011
RB Test Mode
connection between the UE and test set (see
How Do I Set Up a Call and Make a Connection?
).
Adjacent Channel Leakage Ratio
.
ACLR
Setup
(
F1
):
Trigger Arm
is set to
Single
, you must press the
START SINGLE
key to begin the measurement.
Change View
(
F2
) key to display the measurement results in either graphical or numeric format.
Graph Limits
(
F5
) to enter the pass/fail measurement limit for each of the four frequency offsets (shown in the graphical measurements example below as the thin lines above each measurement).A typical result is shown below.
This section is applicable to the lab application or feature-licensed test application only.
Operating Mode
(
F1
) to
Cell Off
.
34.121 Preset Call Configurations
(
F11
on
Call Parms 1 of 3
) and select
5.2B, 5.9B, 5.10B, and 5.13.2B:HSPA:QPSK
, then select the desired sub-test. You may then skip any steps marked with
[34.121 Call Config]
in this procedure.
Channel (UARFCN) Parms
(
F12
on
Call Parms 1 of 3
). Set
DL Channel
(
F7
) to the appropriate "low range" frequency for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band II set
DL Channel
=
9663
).
Uplink Parameters
(
F4
on
Call Control 2 of 6
).
Uplink DPCH Bc/Bd Control
to
Manual
.
Manual Uplink DPCH Bc
to
11
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Manual Uplink DPCH Bd
to
15
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Maximum Uplink Transmit Power Level
to
21 dBm
.
Operating Mode
to
Active Cell
(pressing the
CALL SETUP
key quickly brings you back to the top level
Call Control
menu).
Cell Power
(
F7
on
Call Parms 1 of 3
) to
-86 dBm/3.84 MHz
.
Channel Type
(
F8
) to
12.2k RMC + HSPA
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Generator Info
(
F3
on
Call Control 2 of 6
), select
Downlink Channel Levels
(
F3
), select
Connected DL Channel Levels
(
F3
), then select
HSPA Conn DL Channel Levels
(
F4
).
HSPA Cell 1 Connected CPICH Level
to
-10 dB
(this is the default value).
HSPA Cell 1 Connected P-CCPCH/SCH Level
to
-12 dB
(this is the default value).
HSPA Cell 1 Connected PICH Level
to
-15 dB
(this is the default value).
HSPA Cell 1 Connected (F-)DPCH Level
to
-10 dB
(this is the default value).
HSPA Cell 1 Connected E-AGCH Level
to
-20 dB
(this is the default value).
HSPA Cell 1 Connected E-HICH Level
to
-20 dB
(this is the default value).
HSPA Cell 1 Connected E-RGCH Level
to
Off
(this is the default value).
HSPA Cell 1 Connected HS-PDSCHs Level (Sum)
to
-3 dB
(this is the default value).
HSPA Cell 1 Connected HS-SCCH 1 Level
to
-8 dB
.
HSUPA Parameters
(
HSPA Parameters
(
F10
),
F9
).
HSUPA RB Test Mode Setup
(
F8
).
Common HSUPA Parameters
(
F9
).
E-DPCCH/DPCCH Power Offset (DeltaE-DPCCH)
to
6
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1). Note, 34.121-1 Table C.11.1.3 provides Beta
ec
(209/225 for sub-test 1). To determine what value of DeltaE-DPCCH corresponds to this, use 3GPP TS 25.213 Table 1B and the value of Beta
c
from 34.121-1 Table C.11.1.3 (11/15 for sub-test 1). For sub-test 1, A
ec
= Beta
ec
/Beta
c
= (209/225)/(11/15) = 19/15; therefore DeltaE-DPCCH = 6.
Reference E-TFCI Power Offsets
to
Definition 34.121-01
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Serving Grant
(
F10
).
RB Setup AG
to
26: (119/15)^2
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1). Note, 34.121-1 Table C.11.1.3 AG Index corresponds to 3GPP TS 25.212 s4.10.1A.1 Table 16B, which maps the Absolute Grants sent on the E-AGCH. To send the equivalent Absolute Grant in the RB Setup message, you must use the AG Index in 3GPP TS 25.321 s9.2.5.2.1 Table 9.2.5.2.1.1.
HSDPA Parameters
(
HSPA Parameters
(
F10
),
F10
).
Cell Parameters
(
F2
).
Cell Info
(
F2
), then
Cell Parameters
(
F2
).
Call Control 2 of 6
menu)
PS Domain Information
to
Present
(this is the default value in the lab application).
Cell Info
,
Reselection Parameters
(
F3
).
RB Test Mode Setup
(
F6
on
Call Control 3 of 6
) and set
UE Loopback Type
to
Type 1
(this is the default value).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Algorithm
to
Two
(this is the default value) (for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
PS Domain Information
parameter must be set to
Present
when the UE registers (attaches) with the test set.
Originate Call
(
F3
on
Call Control 1 of 6
).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Mode
to
Active bits
(this is the default value).
UE Target Power
(
F7
on
Call Parms 3 of 3
) to
2 dBm
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1, power class 3 UE). This value is determined as follows: Maximum power for a power class 3 UE is +24 dBm, but
UE Target Power
only sets the DPCCH+DPDCH power level of the UE. In order to achieve a total output power of +16.5 dBm (24 dBm - 7.5 dB), you must set
UE Target Power
to at most 16.5 dBm -
Power change due to HS-DPCCH, E-DPCCH and E-DPDCH
.
UE Target Power
to 2 dBm for sub-test 1.
UE Target Power
values for sub-tests 2-5 are as follows: sub-test 2: 11 dBm, sub-test 3: 3 dBm, sub-test 4: 14 dBm, sub-test 5: 6 dBm.
Channel Power
.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
Alternating bits
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Additional Screens
(
F1
from
Call Control 2 of 6
), select
HSPA Information
(
F2
) and observe the
Last Received E-TFCI
(it should be 75 for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1, 67 for sub-test 2, 92 for sub-test 3, 71 for sub-test 4 and 67 for sub-test 5).
E-TFCI Recording Information
(
F3
) (for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
HSPA Parameters
(
F10
),
HSUPA Parameters
(
F9
),
E-TFCI Recording
(
F11
),
E-TFCI Recording Parameters
(
F7
) (for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1):
E-TFCI Recording Count
(
F7
) to
15
(this is the default value).
Send Step Up TPC Bit Pattern
(
F10
) and then
Start Recording E-TFCI Values
(
F8
).
Send Step Down TPC Bit Pattern
(
F11
) and then
Start Recording E-TFCI Values
(
F8
).
Adjacent Channel Leakage Ratio
.
Handovers
(
F5
)) to change the following settings:| Setting | Sub-test 2 | Sub-test 3 | Sub-test 4 | Sub-test 5 |
|---|---|---|---|---|
| TCR DPCH Bc/Bd Control | Manual | Manual | Manual | Manual |
| TCR Manual Uplink DPCH Bc | 6 | 15 | 2 | 15 |
| TCR Manual Uplink DPCH Bd | 15 | 9 | 15 | 0 |
| TCR DeltaACK, DeltaNACK, DeltaCQI | 8 | 8 | 8 | 0 |
| TCR Ack-Nack Repetition Factor | 3 | 3 | 3 | 3 |
| TCR CQI Feedback Cycle (k) | 4 ms | 4 ms | 4 ms | 4 ms |
| TCR CQI Repetition Factor | 2 | 2 | 2 | 2 |
| TCR E-DPCCH/DPCCH Power Offset | 8 | 8 | 5 | 0 |
| TCR Reference E-TFCI Power Offsets | 34121-01 | 34121-02 | 34121-01 | 34121-03 |
| TCR Absolute Grant | 18: (47/15)^2 | 21: (67/15)^2 | 23: (84/15)^2 | 18: (47/15)^2 |
Channel Type
(
F8
) to
HSPA
.
HSUPA RB Test Mode Setup
(
F8
) and set
RB E-DPDCH Max Channel Codes (HSPA)
to
SF4
.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Algorithm
to
One
.
Originate Call
(
F3
on
Call Control 1 of 6
).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Mode
to
Active bits
.
UE Target Power
(
F7
on
Call Parms 3 of 3
) to
6 dBm
(for power class 3 UE).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
All Up bits
. Adjacent Channel Leakage Ratio (ACLR) Measurement Description