Last updated: January 16, 2009
Trigger Source
is set to
Immediate
or
External
.
Trigger Source
can only be set to HS-DPCCH when
Channel Type
=
12.2k RMC + HSDPA
or
12.2k RMC + HSPA
.This measurement uses auto-ranging to automatically set the expected level into the test set.
If
Over Range
(5) is returned, the measured signal exceeds the expected input level or exceeds the maximum allowed input power for the test set.
If
Under Range
(6) is returned, the measured signal is below the expected input level.
If
Uncalibrated Due to Temperature
(19) is returned, the temperature in the test set has changed by ± 10° C or more since the last calibration and should be calibrated again. See
Calibrating the Test Set
.
See Integrity Indicator .