Last updated: February 10, 2011
Before performing these procedures, ensure that you have specified the proper Amplitude Offset for your test setup, and that the test set has been properly calibrated (see Calibrating the Test Set ).
This section is applicable to the lab application or feature-licensed test application only.
3GPP TS 34.121 5.2A measures the UE's maximum output power when the HS-DPCCH is present. For ease of measurement, the test requires you to configure the UE such that the HS-DPCCH is always transmitted, and at a constant level. This is accomplished by setting
DeltaACK
,
DeltaNACK
and
DeltaCQI
to
8
, by setting
CQI Feedback Cycle (k)
to
4 ms
and
CQI Repetition Factor
to
2
, and by setting
Ack-Nack Repetition Factor
to
3
(required because the test is performed using H-Set 1, which has an X00X00 data transmission pattern).
Operating Mode
(
F1
) to
Cell Off
.
Channel (UARFCN) Parms
(
F12
on
Call Parms 1 of 3
). Set
DL Channel
(
F7
) and
Uplink Channel
(
F8
) to the appropriate "low range" frequencies for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band II, set
DL Channel
=
9663
and
Uplink Channel
=
9263
).
Uplink Parameters
(
F4
on
Call Control 2 of 5
).
Uplink DPCH Bc/Bd Control
to
Manual
.
Manual Uplink DPCH Bc
to the value corresponding to the first 34.121 v7.0.0 Table C.10.1.4 sub-test you wish to test (for example, for sub-test 3, set
Manual Uplink DPCH Bc
to
15
).
Manual Uplink DPCH Bd
to the value corresponding to the first 34.121 v7.0.0 Table C.10.1.4 sub-test you wish to test (for example, for sub-test 3, set
Manual Uplink DPCH Bd
to
8
).
Maximum Uplink Transmit Power Level
to
+21 dBm
.
Operating Mode
to
Active Cell
(pressing the
CALL SETUP
key quickly brings you back to the top level
Call Control
menu).
Channel Type
(
F8
) to
12.2k RMC + HSDPA
.
HSDPA Parameters
(
HSPA Parameters
(
F10
),
F10
).
HSDPA RB Test Mode Setup
(
F8
).
HS-DSCH Configuration Type
to
FRC
(this is the default value).
FRC Type
to
H-Set 1 QPSK
(this is the default value).
CN Domain
as needed (by default it is set to
PS Domain
). Note, before you can establish a connection in the PS domain, the UE must attach to the test set. To enable this, the
PS Domain Information
parameter (under
Cell Parameters
,
F12
on
Call Control 2 of 5
) must be set to
Present
when the UE registers (attaches) with the test set.
HSDPA Uplink Parameters
(
F11
).
Cell Parameters
(
F2
).
Cell Info
(
F2
), then
Cell Parameters
(
F2
).
Call Control 2 of 5
menu)
Generator Info
(
F3
on
Call Control 2 of 5
), select
Connected DL Channel Levels
(
F4
), then select
HSDPA Conn DL Channel Levels
(
F4
).
Cell 1 Connected HSDPA CPICH Level
to
-10 dB
(this is the default value).
Cell 1 Connected HSDPA P-CCPCH/SCH Level
to
-12 dB
(this is the default value).
Cell 1 Connected HSDPA PICH Level
to
-15 dB
(this is the default value).
Cell 1 Connected HSDPA DPCH Level
to
-9 dB
.
Cell 1 Sum of Active Conn HS-PDSCH Levels
to
-3 dB
(this is the default value).
Cell 1 Connected HS-SCCH 1 Level
to
-8 dB
.
Originate Call
(
F3
on
Call Control 1 of 5
).
Cell Power
(
F7
on
Call Parms 1 of 3
) to
-86 dBm/3.84 MHz
.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
).
UE Target Power
(
F7
on
Call Parms 3 of 3
) to a high value, such as
24 dBm
. The test set drives the UE to the specified level (or simply continues to send all up bits if the UE does not reach that level), while also appropriately ranging the test set's measurement receiver.
UL CL Power Ctrl Parameters
(
F8
). Set
UL CL Power Ctrl Mode
to
All Up bits
.
Channel Power
.
Trigger Arm
to
Single
, press the
START SINGLE
key to begin the measurement.
TCR Manual Uplink DPCH Bc
and
TCR Manual Uplink DPCH Bd
settings), then repeat steps 14-16.
TCR Timing Indication (CFN Handling)
to
Maintain
and
TCR Relative DPCH Frame Offset
to
0 chips
or set
TCR Default DPCH Offset (DOFF)
to
3 x 512 chips
. You must also set
TCR DeltaACK
,
TCR DeltaNACK
and
TCR DeltaCQI
to
8
, set
TCR Ack-Nack Repetition Factor
to
3
, set
TCR CQI Feedback Cycle (k)
to
4ms
, and set
TCR CQI Repetition Factor
to
2
.This section is applicable to the lab application or feature-licensed test application only.
Operating Mode
(
F1
) to
Cell Off
.
34.121 Preset Call Configurations
(
F11
on
Call Parms 1 of 3
) and select
5.2B, 5.9B, 5.10B, and 5.13.2B:HSPA:QPSK
and then
Sub-test 1
. You may then skip any steps marked with
[34.121 Call Config]
in this procedure.
Channel (UARFCN) Parms
(
F12
on
Call Parms 1 of 3
). Set
DL Channel
(
F7
) to the appropriate "low range" frequency for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band II set
DL Channel
=
9663
).
Uplink Parameters
(
F4
on
Call Control 2 of 6
).
Uplink DPCH Bc/Bd Control
to
Manual
.
Manual Uplink DPCH Bc
to
11
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Manual Uplink DPCH Bd
to
15
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Maximum Uplink Transmit Power Level
to
21 dBm
.
Operating Mode
to
Active Cell
(pressing the
CALL SETUP
key quickly brings you back to the top level
Call Control
menu).
Cell Power
(
F7
on
Call Parms 1 of 3
) to
-86 dBm/3.84 MHz
.
Channel Type
(
F8
) to
12.2k RMC + HSPA
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Generator Info
(
F3
on
Call Control 2 of 6
), select
Downlink Channel Levels (
F3
), and then
Connected DL Channel Levels
(
F3
). Select
HSPA Conn DL Channel Levels
(
F4
).
HSPA Cell 1 Connected CPICH Level
to
-10 dB
(this is the default value).
HSPA Cell 1 Connected P-CCPCH/SCH Level
to
-12 dB
(this is the default value).
HSPA Cell 1 Connected PICH Level
to
-15 dB
(this is the default value).
HSPA Cell 1 Connected (F-)DPCH Level
to
-10 dB
(this is the default value).
HSPA Cell 1 Connected E-AGCH Level
to
-20 dB
(this is the default value).
HSPA Cell 1 Connected E-HICH Level
to
-20 dB
(this is the default value).
HSPA Cell 1 Connected E-RGCH Level
to
Off
(this is the default value).
HSPA Cell 1 Connected HS-PDSCHs Level (Sum)
to
-3 dB
(this is the default value).
HSPA Cell 1 Connected HS-SCCH 1 Level
to
-8 dB
.
HSUPA Parameters
(
HSPA Parameters
(
F10
),
F9
).
HSUPA RB Test Mode Setup
(
F8
).
Common HSUPA Parameters
(
F9
).
E-DPCCH/DPCCH Power Offset (DeltaE-DPCCH)
to
6
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1). Note, 34.121-1 Table C.11.1.3 provides Beta
ec
(209/225 for sub-test 1). To determine what value of DeltaE-DPCCH corresponds to this, use 3GPP TS 25.213 Table 1B and the value of Beta
c
from 34.121-1 Table C.11.1.3 (11/15 for sub-test 1). For sub-test 1, A
ec
= Beta
ec
/Beta
c
= (209/225)/(11/15) = 19/15; therefore DeltaE-DPCCH = 6.
Reference E-TFCI Power Offsets
to
Definition 34.121-01
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Serving Grant
(
F10
).
RB Setup AG
to
Index 26: (119/15)^2
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1). Note, 34.121-1 Table C.11.1.3 AG Index corresponds to 3GPP TS 25.212 s4.10.1A.1 Table 16B, which maps the Absolute Grants sent on the E-AGCH. To send the equivalent Absolute Grant in the RB Setup message, you must use the AG Index in 3GPP TS 25.321 s9.2.5.2.1 Table 9.2.5.2.1.1.
HSDPA Parameters
(
HSPA Parameters
(
F10
),
F10
).
Cell Parameters
(
F2
).
Cell Info
(
F2
), then
Cell Parameters
(
F2
).
Call Control 2 of 6
menu)
PS Domain Information
to
Present
(this is the default value in the lab application).
Cell Info
,
Reselection Parameters
(
F3
).
RB Test Mode Setup
(
F6
on
Call Control 3 of 6
) and set
UE Loopback Type
to
Type 1
(this is the default value).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Algorithm
to
Two
(this is the default value).
PS Domain Information
parameter must be set to
Present
when the UE registers (attaches) with the test set.
Originate Call
(
F3
on
Call Control 1 of 6
).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Mode
to
Active bits
(this is the default value) .
UE Target Power
(
F7
on
Call Parms 3 of 3
) to
2 dBm
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1, power class 3 UE). This value is determined as follows: Maximum power for a power class 3 UE is +24 dBm, but
UE Target Power
only sets the DPCCH+DPDCH power level of the UE. In order to achieve a total output power of +16.5 dBm (24 dBm - 7.5 dB), you must set
UE Target Power
to at most 16.5 dBm -
Power change due to HS-DPCCH, E-DPCCH and E-DPDCH
.
UE Target Power
to 2 dBm for sub-test 1.
UE Target Power
values for sub-tests 2-5 are as follows: sub-test 2: 11 dBm, sub-test 3: 3 dBm, sub-test 4: 14 dBm, sub-test 5: 6 dBm.
Channel Power
.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
Alternating bits
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Additional Screens
(
F1
from
Call Control 2 of 6
), select
HSPA Information
(
F2
) and observe the
Last Received E-TFCI
(it should be 75 for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1, 67 for sub-test 2, 92 for sub-test 3, 71 for sub-test 4 and 67 for sub-test 5).
E-TFCI Recording Information
(
F3
) (for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
HSPA Parameters
(
F10
),
HSUPA Parameters
(
F9
),
E-TFCI Recording
(
F11
),
E-TFCI Recording Parameters
(
F7
) (for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1):
E-TFCI Recording Count
to
15
(this is the default value).
Send Step Up TPC Bit Pattern
(
F10
) and then
Start Recording E-TFCI Values
(
F8
).
Send Step Down TPC Bit Pattern
(
F11
) and then
Start Recording E-TFCI Values
(
F8
).
Handovers
(
F5
)) to change the following settings:| Setting | Sub-test 2 | Sub-test 3 | Sub-test 4 | Sub-test 5 |
|---|---|---|---|---|
| TCR DPCH Bc/Bd Control | Manual | Manual | Manual | Manual |
| TCR Manual Uplink DPCH Bc | 6 | 15 | 2 | 15 |
| TCR Manual Uplink DPCH Bd | 15 | 9 | 15 | 0 |
| TCR DeltaACK, DeltaNACK, DeltaCQI | 8 | 8 | 8 | 0 |
| TCR Ack-Nack Repetition Factor | 3 | 3 | 3 | 3 |
| TCR CQI Feedback Cycle (k) | 4 ms | 4 ms | 4 ms | 4 ms |
| TCR CQI Repetition Factor | 2 | 2 | 2 | 2 |
| TCR E-DPCCH/DPCCH Power Offset | 8 | 8 | 5 | 0 |
| TCR Reference E-TFCI Power Offsets | 34121-01 | 34121-02 | 34121-01 | 34121-03 |
| TCR Absolute Grant | 18: (47/15)^2 | 21: (67/15)^2 | 23: (84/15)^2 | 18: (47/15)^2 |
Channel Type
(
F8
) to
HSPA
.
HSUPA RB Test Mode Setup
(
F8
).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Algorithm
to
One
.
Originate Call
(
F3
on
Call Control 1 of 6
).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Mode
to
Active bits
.
UE Target Power
(
F7
on
Call Parms 3 of 3
) to
6 dBm
(for power class 3 UE).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
All Up bits
.
Operating Mode
(
F1
) to
Cell Off
.
DL Channel
(
F10
) and
Uplink Channel
(
F11
) to the appropriate "low range" frequencies for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band I,
DL Channel
=
10563
and
Uplink Channel
=
9613
).
Operating Mode
to
Active Cell
.
RB Test Mode
connection between the UE and test set (see
How Do I Set Up a Call and Make a Connection?
).
Connected DL Channel Levels
are set to their default values, as required by 3GPP TS 34.121 Table E.3.1 (select
Generator Info
,
F3
on
Call Control 2 of 5
).
Cell Power
(
F7
) to
-93 dBm
.
Call Drop Timer
(
F11
on
Call Parms 2 of 3
) to
Off
.
UE Target Power
:
UL CL Power Ctrl Mode
is set to its default value of
Active Bits
(select
UL CL Power Ctrl Parameters
,
F8
on the
Call Parms 3 of 3
menu).
UE Target Power
(
F7
) to -55 dBm.The test set then drives the UE to the specified level, while also appropriately ranging its measurement receiver.
UL CL Power Ctrl Parameters
menu (
F8
) and set
UL CL Power Ctrl Mode
to
All Down bits
and ensure that
UL CL Power Ctrl Algorithm
is set to
Two
. The test set then drives the UE to transmit at the lowest level possible.
Channel Power
.