Last updated: January 16, 2009
 Trigger Source 
is set to
 Immediate
 or
 RF Rise
.
Trigger Source 
can only be set to HS-DPCCH when 
Channel Type
 =
 12.2k RMC + HSDPA 
or
 12.2k RMC + HSPA
.
 Auto Range 
is on, the UE's output power must be stable in order for the autoranging algorithm to operate properly.
 
If 
Over Range
 (5) is returned, the measured signal exceeds the expected input level or exceeds the maximum allowed input power for the test set. See 
Auto Range
 and 
Manual Power Range Offset
.
 
If 
Under Range
 (6) is returned, the measured signal is below the expected input level. 
 
If 
Uncalibrated Due to Temperature
 (19) is returned, the temperature in the test set has changed by ± 10° C or more since the last calibration and should be calibrated again. See 
Calibrating the Test Set
.
See Integrity Indicator .