Last updated: January 15, 2009
This section is only applicable to the lab application.
 Operating Mode 
(
F1
) to
 Cell Off
.
 DL Channel 
(
F10
) and
 Uplink Channel 
(
F11
) to the appropriate "mid range" frequencies for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band I,
 DL Channel 
=
 10700 
and
 Uplink Channel 
=
 9750
).
 Operating Mode 
to
 Active Cell
.
 Uplink Dummy DCCH Data 
is set to its default value of
 Off
 (select
 RB Test Mode Setup
,
 F6 
on
 Call Control 3 of 5
).
 Uplink DPCH Bc/Bd Control 
is set to its default value of
 Auto 
(select
 Uplink Parameters
,
 F4 
on
 Call Control 2 of 5
).
 UL CL Power Ctrl Algorithm 
is set to its default value of
 Two
 (select
 UL CL Power Ctrl Parameters
,
 F8 
on
 Call Parms 3 of 3
).
 12.2k RMC RB Test Mode 
connection between the UE and test set (see 
How Do I Set Up a Call and Make a Connection?
).
 Connected DL Channel Levels 
are set to their default values, as required by 3GPP TS 34.121 Table E.3.1 (select
 Generator Info
, 
F3 
on
 Call Control 2 of 5
).
 Cell Power 
(
F7
) to
 -93 dBm
.
 UE Target Power 
(
F7
 on
 Call Parms 3 of 3
) to
 0 dBm
. Ensure that
 UL CL Power Ctrl Mode
 is set to its default value of
 Active Bits
 (select
 UL CL Power Ctrl Parameters
,
 F8 
on
 Call Parms 3 of 3
). The test set then drives the UE to 0 dBm, while also appropriately ranging its measurement receiver.
 Alternating bits
 to hold the UE's power at 0 dBm.
Change Of TFC
. 
 Change Of TFC Setup 
(
F1
).
Change of TFC (Transport Format Combination) Measurement Description
Change of TFC (Transport Format Combination) Troubleshooting
Programming a Change of TFC (Transport Format Combination) Measurement