Last updated: January 16, 2009
This section is only applicable to the lab application.
This section provides an example of how to make change of TFC measurements via GPIB.
The basic procedure to perform change of TFC measurements is as follows:
10 ! Change of TFC Measurement Programming Example 20 ! This programming example assumes that Uplink Dummy DCCH Data is 30 ! set to Off, Uplink DPCH Bc/Bd Control is set to Auto, UL CL Power 40 ! Ctrl Algorithm is set to Two, and that there is an RB Test Mode 50 ! connection between the test set and UE. 60 ! 70 Testset=714 80 ! 90 ! *** Set Up Test Parameters *** 100 ! 110 OUTPUT Testset;"CALL:MS:POWer:TARGet 0" 120 ! Set MS Target Power to 0 dBm. 130 OUTPUT Testset;"CALL:CLPControl:UPLink:MODE UDOWn" 140 ! Set UL CL Power Ctrl Mode to Alternating. 150 ! 160 ! *** Set Up Measurement Parameters *** 170 ! 180 OUTPUT Testset;"SETup:WCTFormat:COUNt 5" 190 ! Set Multi-Measurement Count to 5. 200 ! 210 ! *** INITiate and FETCh Measurements *** 220 ! 230 OUTPUT Testset;"INITiate:WCTFormat" 240 ! Initiate a Change of TFC measurement. 250 OUTPUT Testset;"FETCh:WCTFormat?" 260 ! Fetch Change of TFC measurement results. 270 ENTER Testset;Int,Down_pwr,Down_err,Down_pf,Up_pwr,Up_err,Up_pf 280 ! Retrieve the results. 290 ! 300 ! *** Print Measurement Results *** 310 ! 320 CLEAR SCREEN 330 PRINT "Change of TFC Measurement Results:" 340 PRINT 350 PRINT "Integrity Indicator = ",Int 360 PRINT "Step Down Relative Power (in dB) = ",Down_pwr 370 PRINT "Step Down Error (in dB) = ",Down_err 380 PRINT "Step Down Pass/Fail (0 = pass, 1 = fail) = ",Down_pf 390 PRINT "Step Up Relative Power (in dB) = ",Up_pwr 400 PRINT "Step Up Error (in dB) = ",Up_err 410 PRINT "Step Up Pass/Fail (0 = pass, 1 = fail) = ",Up_pf 420 ! 430 END