Last updated: January 15, 2009
The dynamic power analysis measurement is a flexible tool that allows you to measure the output power of your UE versus time. This section provides examples for two main uses of the measurement, UE power calibration and HS-DPCCH power versus time measurement.
This procedure assumes that the test set is in
Active Cell Operating Mode
. However, this measurement is also available in
and
FDD Test Operating Mode
CW Operating Mode
.
Dynamic Power Analysis
measurement.
Dynamic Power Setup
(
F1
) and set the measurement parameters as needed. For example, to analyze the power sequence shown below, set the parameters as follows:
Steps
to
23
.
Step Length
to
666.7 us
.
RF Rise Trigger Threshold
to
-10 dBm
.
Trigger Qualification State
to
On
.
Trigger Qualification Type
to
RF Rise and Fall
.
Trigger Qualification Rise Threshold
to
10 dB
.
Trigger Qualification Fall Threshold
to
10 dB
.
Trigger Arm
to
Single
.
Trigger Source
to
RF Rise
.
Close Menu
(
F6
).
Trigger Arm
is set to
Single
, you must press the
START SINGLE
key to begin the measurement.
Axis Control
(
F2
). Set the axis control parameters as needed. Select
Return
(
F6
).
Marker
(
F3
) to turn on the marker on the graphical display.A typical result is shown below:
This section is only applicable to the lab application or a test application with the required feature license.
3GPP TS 34.121 s5.7A defines a specific UE output power waveform:
It then specifies the required relative power changes for the test points numbered above. The test is performed with the UE's DPCCH+DPDCH power equal to 0 dBm and also at maximum output power (the resulting power pattern and test points are altered somewhat at maximum power, but the ACK/CQI sequence is unchanged).
Operating Mode
(
F1
) to
Cell Off
.
34.121 Preset Call Configurations
(
F11
on
Call Parms 1 of 3
) and select
5.2C, 5.7A, 5.13.1A, 5.13.1AA, 5.13.2A with QPSK
. You may then skip any steps marked with
[34.121 Call Config]
in this procedure.
Channel (UARFCN) Parms
(
F12
on
Call Parms 1 of 3
). Set
DL Channel
(
F7
) and
Uplink Channel
(
F8
) to the appropriate "mid range" frequencies for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band II, set
DL Channel
=
9800
).
Uplink Parameters
(
F4
on
Call Control 2 of 5
).
Uplink DPCH Bc/Bd Control
to
Manual
.
Manual Uplink DPCH Bc
to
15
(for 34.121 v7.5.0 Table C.10.1.4 sub-test 3).
Manual Uplink DPCH Bd
to
8
(for 34.121 v7.5.0 Table C.10.1.4 sub-test 3).
Maximum Uplink Transmit Power Level
to
+21 dBm
.
Operating Mode
to
Active Cell
(pressing the
CALL SETUP
key quickly brings you back to the top level
Call Control
menu).
Channel Type
(
F8
) to
12.2k RMC + HSDPA
.
HSDPA Parameters
(
HSPA Parameters
(
F10
),
F10
).
HSDPA RB Test Mode Setup
(
F8
).
HS-DSCH Configuration Type
to
FRC
(this is the default value).
FRC Type
to
H-Set 1 QPSK
(this is the default value).
CN Domain
as needed (by default it is set to
PS Domain
). Note, before you can establish a connection in the PS domain, the UE must attach to the test set. To enable this, the
PS Domain Information
parameter (under
Cell Parameters
,
F12
on
Call Control 2 of 5
) must be set to
Present
when the UE registers (attaches) with the test set.
HSDPA Uplink Parameters
(
F11
).
DeltaACK
and
DeltaNACK
to
8
.
DeltaCQI
to
7
.
Ack-Nack Repetition Factor
to
1
(this is the default value).
CQI Feedback Cycle (k)
to
4 ms
.
CQI Repetition Factor
to
1
(this is the default value).
Cell Parameters
(
F2
).
Cell Info
(
F2
), then
Cell Parameters
(
F2
).
Call Control 2 of 5
menu)
Default DPCH Offset (DOFF)
to
3 x 512 chips
.
PS Domain Information
to
Present
(this is the default value in the lab application) if you plan to establish the HSDPA connection in the PS domain (i.e. if you've set
CN Domain
to
PS Domain
or
CS/PS Domain
in step 3 above).
Cell Info
,
Reselection Parameters
(
F3
).
Generator Info
(
F3
on
Call Control 2 of 5
), select
Connected DL Channel Levels
(
F4
), then select
HSDPA Conn DL Channel Levels
(
F4
).
Cell 1 Connected HSDPA CPICH Level
to
-10 dB
(this is the default value).
Cell 1 Connected HSDPA P-CCPCH/SCH Level
to
-12 dB
(this is the default value).
Cell 1 Connected HSDPA PICH Level
to
-15 dB
(this is the default value).
Cell 1 Connected HSDPA DPCH Level
to
-9 dB
.
Cell 1 Sum of Active Conn HS-PDSCH Levels
to
-3 dB
(this is the default value).
Cell 1 Connected HS-SCCH 1 Level
to
-8 dB
.
RB Test Mode Setup
(
F6
on
Call Control 3 of 5
) and set
UE Loopback Type
to
Type 1
(this is the default value).
Originate Call
(
F3
on
Call Control 1 of 5
).
Cell Power
(
F7
on
Call Parms 1 of 3
) to
-86 dBm/3.84 MHz
.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
).
UE Target Power
(
F7
on
Call Parms 3 of 3
) to
0 dBm
. The test set drives the UE's power to the specified value, while also appropriately ranging the test set's measurement receiver.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
Alternating bits
.
Dynamic Power Analysis
.
Dynamic Power Setup
(
F1
).
34.121 5.7A Measurement Configuration
, then select
Yes
. You may then skip any steps marked with
[34.121 Meas Config]
.
Steps
to
37
.
Step Length
to
333.3 us
.
Measurement Interval
to
283.3 us
(to exclude the transient periods).
RRC Filter
to
Off
(to measure "mean power").
Trigger Arm
to
Single
, if desired.
Trigger Source
to
HS-DPCCH
.
Trigger Delay
to
-308.3 us.
(To trigger the measurement on the half slot just prior to subframe 0, a trigger delay of -333.3 us is required. To exclude the transient period after the slot boundary, a trigger delay of -333.3 us + 25 us = -308.3 us is required.)
HS-DPCCH Trigger Subframe Alignment
to
subframe 0
(this is the default value).
Close Menu
(
F6
).
Trigger Arm
to
Single
, press the
START SINGLE
key to begin the measurement.
Adjust the
Axis Control
(
F2
) as needed and use the
Marker
(
F3
) to measure the power changes for each of the specified steps.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
Active bits
.
UE Target Power
(
F7
on
Call Parms 3 of 3
) to a high value, such as
24 dBm
. The test set drives the UE to the specified level (or simply continues to send all up bits if the UE does not reach that level), while also appropriately ranging the test set's measurement receiver.
UL CL Power Ctrl Parameters
(
F8
). Set
UL CL Power Ctrl Mode
to
All Up bits
.Dynamic Power Analysis Measurement Description