Last updated: January 16, 2009
The dynamic power analysis measurement is a flexible tool that allows you to measure the output power of your UE versus time. This section describes two main uses of the measurement:
The dynamic power analysis measurement is not performed with a call established between the test set and UE. Rather, you must place your UE into a test mode which forces it to continuously transmit the power sequence you desire to test, and then analyze the resulting UE output power using the test set.
 
The dynamic power analysis measurement can measure UE output power sequences that step up and/or down with varying or fixed power step sizes. The power step length, which must be fixed for the sequence, can be between 10 us and 12 ms (the measurement is specified for step lengths of 67 us to 12 ms). A total of 58.26 ms of power sequence can be analyzed (for example, up to 87 steps can be measured when
 Step Length 
is set to one timeslot (666.7 us)). 
 Off 
or 40 dB when
 RRC Filter 
=
 On
. To measure a power range greater than 40 dB, you must break the power range up into individual power sequences that do not exceed 40 dB, and perform the measurement for each power sequence.To use the measurement, you must first set Measurement Frequency to the expected UE transmitter frequency and set Manual Power to the maximum expected power for the sequence. You can perform the dynamic power analysis measurement in Active Cell Operating Mode or FDD Test Operating Mode . However, since this measurement does not utilize any overhead signalling to control the UE's power or frequency, you must manually set the test set's Expected Power and Measurement Frequency in either operating mode.
You must specify the length and number of steps in the sequence (including trigger pulses), configure the RF rise trigger, initiate the measurement, then order the UE to send its sequence continuously .
The measurement executes most efficiently if the UE transmits its power sequence continuously, until the measurement has completed. The measurement can be triggered externally or by an RF rise in the power sequence. Once triggered, the measurement captures the first power sequence, auto-ranges to the maximum power of the sequence, then triggers on and measures the next available power sequence. The time for the auto-ranging to complete varies depending upon the power sequence.
 
You can vary the
 Measurement Interval 
and its placement within each step (using the
 Trigger Delay 
setting), and insert or remove the
 RRC Filter
. The measurement can analyze CW signals and uplink DPCH signals (when measuring CW signals, you must adjust the
 RF Rise Trigger Threshold 
setting accordingly and use the
 Frequency Offset 
setting to set the proper offset from the 
Measurement Frequency
 setting.)
 
You can trigger the dynamic power analysis measurement using an RF rise within the power sequence by setting
 Trigger Source 
to
 RF Rise 
and specifying the appropriate
 RF Rise Trigger Threshold
. If your power sequence starts with an abrupt rise in power, no separate trigger pulse is needed. However, for the most robust triggering, it is recommended that you include a trigger pulse in every power sequence. The trigger pulse should rise in power by at least 20 dB, reach the maximum power of the sequence, then fall in power by at least 20 dB. Before initiating the measurement, you must set 
Power Control
 to
 Manual 
and set 
Manual Power
 to the highest power expected in the sequence. It is then recommended that
 RF Rise Trigger Threshold 
be set to approximately 10 dB below the expected maximum power.
 
It is recommended that you also use trigger qualification, which allows you to further define the measurement trigger. Instead of the measurement triggering when the UE's signal simply rises above the
 RF Rise Trigger Threshold 
value, you can specify that the signal must meet some additional criteria before the measurement is triggered. To use trigger qualification, set
 Trigger Qualification State 
to
 On 
and set
 Trigger Qualification Type 
to
 RF Rise
,
 RF Fall 
or
 RF Rise and Fall 
as appropriate for your power sequence. You must then set
 Trigger Qualification Rise Threshold 
and/or
 Trigger Qualification Fall Threshold 
accordingly. It is recommended that these rise/fall criteria be at least 10 dB.
 
To ensure successful auto-ranging, you must set the
 Steps 
setting equal or greater than the number of steps in the power sequence (including trigger pulses). When the measurement is triggered, the test set captures data for the time period specified by the
 Steps 
and
 Step Length 
setting to determine the power range of the sequence. It then ranges its receivers to accommodate the highest power in the sequence. The time for this auto-ranging to complete varies depending upon the number of steps in the sequence; a typical duration is approximately 500 ms (note that this is much greater than the duration of one power sequence). Once it has completed this auto-ranging, the test set re-arms and then is triggered by the next available power sequence. It then analyzes and reports the power of each step in that power sequence.
 
The measurement is most accurate over a 40 dB range (when 
RRC Filter
 =
 On
). If the UE's power sequence spans more than 40 dB, the test set will measure and report the power of the entire sequence, but accuracy is degraded for steps that are more than 40 dB below the highest power in the sequence. To measure a power range greater than 40 dB, you must break the power range up into individual power sequences that do not exceed 40 dB.
To ensure that the measurement executes as quickly as possible, the UE should transmit its power sequence continuously until the measurement completes. This ensures that as soon as the measurement is done auto-ranging, another power sequence is immediately available for measurement.
To help ensure your measurement routine executes as fast as possible, consider the following:
 
To perform power versus time measurements on an HSDPA or HSPA uplink signal, you must be on a 
Radio Bearer Test Mode
 connection with a 
Channel Type
 of
 12.2k RMC + HSDPA 
or 12.2k RMC + HSPA. 
The dynamic power analysis measurement can capture up to 58.26 ms of power signal. Thus, the product of Steps and Step Length must not exceed 58.26 ms.
You must specify the total number of steps to be measured.
 
The time duration of each step is determined by 
Step Length
. If
 Step Length 
is set to 666.666... us, then the number of
 Steps 
to measure is equivalent to the number of timeslots to measure.
 
For UE power calibration: the number of steps to measure must include any trigger pulses or separation steps included in the UE's power sequence. It is important that you set
 Steps 
equal or greater than the number of steps in your UE's power sequence so that the entire power sequence is evaluated during auto-ranging of the measurement (see 
Auto-ranging in the Dynamic Power Analysis Measurement for UE Power Calibration
).
For UE power calibration: this setting specifies the time duration of one step in the UE's power sequence (in seconds). Each step in the power sequence must be identical in length.
For HSDPA/HSPA power versus time ( lab application or feature-licensed test application only ): this setting specifies the time duration of one step, which determines how often a power measurement is made.
 
Step Length 
must be greater than or equal to 
Measurement Interval
.
 
When measuring the average power of each step, you can specify how long a period of time over which to average the power for each step using the
 Measurement Interval 
setting. This setting is applied to the measurement of every step.
 
Measurement Interval 
must be less than or equal to 
Step Length
.
 
When measuring the average power of each step, you can specify how long a period of time over which to average the power for each step using the 
Measurement Interval
setting, and then place the measurement interval at the desired position within the step's duration in time using the
 Trigger Delay 
setting. In other words, the
 Trigger Delay 
setting specifies how long after the start of the step the power measurement should begin. This setting is applied to the measurement of every step.
 
For example, for UE power calibration, the default settings of
 Step Length 
=
 666.7 us
,
 Measurement Interval 
=
 300 us 
and
 Trigger Delay 
=
 183.3 us 
causes the test set to measure power for 300 us centered in the middle of the step:
 
For example, for HSDPA power versus time (
lab application or feature-licensed test application only
), setting
 Step Length 
=
 666.7 us
,
 Measurement Interval 
=
 616.7 us 
and
 Trigger Delay 
=
 25 us 
causes the test set to measure power over the entire timeslot excluding the 25 us transient periods on either side of the slot boundaries:
You may choose to measure the average power of each step with or without the RRC (Root Raised Cosine) filter in place. The RRC filter has an alpha of 0.22 and a bandwidth equal to the chip rate of 3.84 MHz.
 
For UE power calibration: the UE's signal may or may not be modulated with an uplink DPCH signal. If the signal is not modulated with an uplink DPCH signal and is offset in frequency from the expected measurement frequency, you must set the
 Frequency Offset 
setting accordingly, to allow for the most accurate power measurements possible.
 
You may set
 Trigger Source 
to
 RF Rise
,
 External 
or
 HS-DPCCH 
(
lab application or feature-licensed test application only
). For more information on these trigger types, see 
Trigger Source Description
.
 
For UE power calibration,
 Trigger Source 
must be set to
 RF Rise 
or
 External
. If
 Trigger Source 
is set to
 RF Rise
, you must characterize the trigger using the 
RF Rise Trigger Threshold
. For the most robust triggering, it is also recommended that you further qualify the trigger using the 
Trigger Qualification State
 setting.
 
For HSDPA or HSPA power versus time, it is recommended that you use a
 Trigger Source 
of
 HS-DPCCH
. When
 Trigger Source 
is set to
 HS-DPCCH
, you can specify on which uplink subframe the measurement triggers using the 
HS-DPCCH Trigger Subframe Alignment
 setting. You can also measure HSDPA/HSPA power versus time using a
 Trigger Source 
of
 External
, but you must ensure that your external trigger is properly aligned to the portion of the HSDPA/HSPA signal that you wish to measure.
This setting is only applicable to the lab application or a feature-licensed test application.
 
When 
Trigger Source
is set to
 HS-DPCCH
, you can specify on which uplink subframe the measurement triggers. You can then use the 
Trigger Delay
 setting to move the 
Measurement Interval
 relative to that subframe boundary.
 
This setting is only applicable when 
Trigger Source
is set to
 RF Rise
. When
 Trigger Source 
is set to
 RF Rise
, you must set the
 RF Rise Trigger Threshold 
to the power level (in dBm) at which you want the measurement to trigger. When the power of the UE's signal rises above the
 RF Rise Trigger Threshold 
level, the measurement is triggered.
 
The test set assumes a crest factor of 3.1 dB for the signal (as is typical for an uplink DPCH signal relative to a CW signal) and thus actually triggers when the input signal reaches the
 RF Rise Trigger Threshold 
level plus 3.1 dB. If the UE's signal has a crest factor other than 3.1 dB, you must set the
 RF Rise Trigger Threshold 
level accordingly.
 
RF Rise Trigger Threshold 
must be set to within 0 dB to -25 dB of the 
Expected Power
.
 
This setting is only available when 
Trigger Source
 is set to
 RF Rise
.
 
This setting is only applicable when 
Trigger Source
is set to
 RF Rise
.
 
For complex UE power sequences, you may choose to further define the measurement trigger using trigger qualification. Instead of the measurement triggering when the UE's signal simply rises above the
 RF Rise Trigger Threshold 
value, you can specify that the UE's signal must meet some additional criteria as well before the measurement is triggered, using the 
Trigger Qualification Type
 setting.
 
This setting is only applicable when 
Trigger Source
is set to
 RF Rise
.
RF Rise
: If you choose a
 Trigger Qualification Type 
of
 RF Rise
, then the measurement will not trigger unless the UE's signal rises above the
 RF Rise Trigger Threshold 
value AND crosses this level with a positive change in power equal to or greater than the 
Trigger Qualification Rise Threshold
. For example, if
 RF Rise Trigger Threshold 
is set to
 0 dBm 
and
 Trigger Qualification Rise Threshold 
is set to
 10 dB
, then the measurement will not trigger until the UE's signal rises above 0 dBm AND increases in power by at least 10 dB within the qualification interval. The qualification interval is one 
Step Length
 before the transition across the
 RF Rise Trigger Threshold 
and one
 Step Length 
after the transition. (The power measurements performed in the qualification interval are performed according to the 
Measurement Interval
, 
Trigger Delay
, and 
RRC Filter
 settings, see 
Specifying the Measurement Characteristics for Each Step
).
RF Fall
: If you choose a
 Trigger Qualification Type 
of
 RF Fall
, then the measurement will not trigger unless the UE's signal rises above the
 RF Rise Trigger Threshold 
value AND then exhibits a negative change in power equal to or greater than the 
Trigger Qualification Fall Threshold
 during the qualification interval. The qualification interval is the two
 Step Lengths 
immediately after the transition across the
 RF Rise Trigger Threshold
.
RF Rise and Fall
: If you choose a
 Trigger Qualification Type 
of
 RF Rise and Fall
, then the measurement will not trigger unless the UE's signal rises above the
 RF Rise Trigger Threshold 
value AND crosses this level with a positive change in power equal to or greater than the 
Trigger Qualification Rise Threshold
 AND then exhibits a negative change in power equal to or greater than the 
Trigger Qualification Fall Threshold
. In other words, both requirements of a
 Trigger Qualification Type 
of
 RF Rise 
and
 RF Fall 
as explained above must be met
 
No matter which type is chosen for the
 Trigger Qualification Type
, if the requirements are met, then the measurement will trigger at the point at which the
 RF Rise Trigger Threshold 
was crossed.
 
This setting is only available when 
Trigger Qualification State
 is set to
 On
.
 
This setting is only applicable when 
Trigger Source
is set to
 RF Rise
.
 
This setting specifies the positive change in power that must occur for the measurement to trigger when the
 RF Rise Trigger Threshold 
is crossed, when 
Trigger Qualification Type
 is set to
 RF Rise 
or
 RF Rise and Fall
.
 
This setting is only applicable when 
Trigger Source
is set to
 RF Rise
.
 
This setting specifies the negative change in power that must occur for the measurement to trigger when the
 RF Rise Trigger Threshold 
is crossed, when 
Trigger Qualification Type
 is set to
 RF Fall 
or
 RF Rise and Fall
.
 
This setting should be used in conjunction with the 
34.121 Preset Call Configurations
. The
 34.121 5.7A Measurement Configuration 
setting sets the following:
 Trigger Arm 
=
 Single
,
 Steps 
=
 37
,
 Step Length 
=
 333.3 us
, 
Measurement Interval 
=
 283.3 us
,
 Trigger Source 
=
 HS-DPCCH
,
 HS-DPCCH Trigger Subframe Alignment 
=
 subframe 0
,
 Trigger Delay 
=
 -308.3 us
, and
 RRC Filter 
=
 Off
. You can then use the marker to measure the power step changes and ensure that your UE conforms to 5.7A (see 
Measuring 3GPP TS 34.121 v7.5.0 s5.7A HS-DPCCH
).
You can query the number of steps measured using the FETCh:WDPAnalysis commands. The number of steps measured is also displayed on the front panel graphical display (see How Do I Make a Dynamic Power Analysis Measurement? ).
The number of steps measured is determined by the Steps setting.
Once the dynamic power analysis measurement has autoranged and triggered on the UE's power sequence, the test set then measures the average power for each step in the sequence as specified by the Measurement Interval , Trigger Delay , and RRC Filter settings. (See Specifying the Measurement Characteristics for Each Step .)
You can retrieve the average power measured for each step using the FETCh:WDPAnalysis commands or from the front panel (see How Do I Make a Dynamic Power Analysis Measurement? ).
A typical UE power calibration measurement result is shown below:
The dynamic power analysis measurement can measure power between -61 dBm and +28 dBm.
 
The dynamic range for any one measurement is 40 dB when 
RRC Filter
 =
 On 
(the UE's power may not vary by more than 40 dB in a single power sequence).
 
You must calibrate the dynamic power analysis measurement using the
 Calibrate Measurements 
procedure (see 
Calibrating the Test Set
).
Manual Operation: How Do I Make a Dynamic Power Analysis Measurement?
Programming the Dynamic Power Analysis Measurement
Dynamic Power Analysis Troubleshooting
What 3GPP W-CDMA/HSPA Conformance Tests Are Supported?
Product Note: W-CDMA Dynamic Power Analysis Using the Keysight 8960 Wireless Communications Test Set