Sets/queries the Cell Info List setting. This parameter
can only be set when call status is |
|
| PRES | |
| Requirements | |
OUTPUT 714;"CALL:BCCHannel:CELLlist PRESent" ! Selects BCCH Cell Info List to preset on the BCCH. |
|
Sets/queries the Frequency Band Indicator State setting. This setting cannot be changed in active cell operating mode. |
|
| 1|0 | |
| 1 (on) | |
| Requirements | |
OUTPUT 714;"CALL:BCCHannel:FBINdicator:STATe OFF" ! Turns Frequency Band Indicator State off. |
|
Sets/queries the BCCH SIB 11 Inter-frequency FDD measurement indicator: |
|
| 1|0 | |
| 1 | |
| Lab Application Revision: F.00.19 and above | |
OUTPUT 714;"CALL:BCCHannel:FMOCcasion:FDDIndicator 1" |
|
Sets/queries the band for each of the 8 GSM neighbor cells (see GSM Cells ). This parameter
can only be set when call status is |
|
Range:
DCS1800|PCS1900,DCS1800|PCS1900,DCS1800|PCS1900, The command must be issued with a comma-separated list of 8 values. Each value in the list defines the band for the corresponding neighbor cell (cell 1 through cell 8). Whether each cell is actually present in the cell list transmitted by the test set is controlled by the CALL[:CELL]:BCCHannel:GSMSystem:STATe setting. |
|
| DCS1800,DCS1800,DCS1800,DCS1800,DCS1800,DCS1800,DCS1800,DCS1800, | |
OUTPUT 714;"CALL:BCCHannel:GSMSystem:BAND PCS1900,PCS1900,PCS1900,PCS1900,PCS1900, PCS1900,PCS1900,PCS1900" ! Sets the band for each of the 8 GSM neighbor cells to PCS1900. |
|
Sets/queries the BCC for each of the 8 GSM neighbor cells (see GSM Cells ). This parameter
can only be set when call status is |
|
|
The command must be issued with a comma-separated list of 8 values. Each value in the list defines the BCC for the corresponding neighbor cell (cell 1 through cell 8). Whether each cell is actually present in the cell list transmitted by the test set is controlled by the CALL[:CELL]:BCCHannel:GSMSystem:STATe setting. |
|
| 5,0,1,2,3,4,6,7 | |
OUTPUT 714;"CALL:BCCHannel:GSMSystem:BCC 4,1,3,6,0,7,2,5" ! Sets the BCC for the first GSM neighbor cell to 4, ! sets the BCC for the second GSm neighbor cell to 1, etc. |
|
Sets/queries the BCH ARFCN for each of the 8 GSM neighbor cells (see GSM Cells ). This parameter
can only be set when call status is |
|
|
The command must be issued with a comma-separated list of 8 values. Each value in the list defines the BCH ARFCN for the corresponding neighbor cell (cell 1 through cell 8). Whether each cell is actually present in the cell list transmitted by the test set is controlled by the CALL[:CELL]:BCCHannel:GSMSystem:STATe setting. |
|
| 20,30,40,50,60,70,80,90 | |
OUTPUT 714;"CALL:BCCHannel:GSMSystem:BCHannel 22,32,42,52,62,72,82,92" ! Sets the BCH ARFCN for the first GSM neighbor cell to 22, ! sets the BCC for the second GSm neighbor cell to 32, etc. |
|
Sets/queries the NCC for each of the 8 GSM neighbor cells (see GSM Cells ). This parameter
can only be set when call status is |
|
|
The command must be issued with a comma-separated list of 8 values. Each value in the list defines the NCC for the corresponding neighbor cell (cell 1 through cell 8). Whether each cell is actually present in the cell list transmitted by the test set is controlled by the CALL[:CELL]:BCCHannel:GSMSystem:STATe setting. |
|
| 1, 0, 2, 3, 4, 5, 6, 7 | |
OUTPUT 714;"CALL:BCCHannel:GSMSystem:NCC 7,1,6,3,0,4,5,2" ! Sets the NCC for the first GSM neighbor cell to 7, ! sets the NCC for the second GSm neighbor cell to 1, etc. |
|
Sets/queries GSM <num> Cell Cell Reselection Min Rx Level for each of the 8 GSM neighbor cells. This parameter
can only be set when call status is |
|
|
The command
must be issued with a comma-separated
list of 8 values. Each value in the
list defines the |
|
| -104,-104,-104,-104,-104,-104,-104,-104 (dBm) | |
OUTPUT 714;"CALL:BCCHannel:GSMSystem:CRESelection:RLMinimum -100,-100,-100,-100,-100,-100,-100,-100" ! Sets Cell Reselection Min Rx Level for the first GSM neighbor cell to -100 dBm, ! sets Cell Reselection Min Rx Level for the second GSM neighbor cell to -100 dBm, etc. |
|
Sets/queries whether each of the 8 GSM neighbor cells is included in the cell info list transmitted by the test set (see GSM Cells ). This parameter
can only be set when call status is |
|
|
The command must be issued with a comma-separated list of 8 valid settings. |
|
| 1,0,0,0,0,0,0,0 | |
OUTPUT 714;"CALL:BCCHannel:GSMSystem:STATe 1,1,1,1,1,1,1,1" ! Includes all 8 GSM neighbor cells in the cell info list. |
|
THIS COMMAND IS OBSOLETE. Please use the CALL[:CELL]:BCCHannel:ITRFrequency:DOWNlink:CHANnel command. Sets/queries the downlink channel number (DL UARFCN) of the Inter-frequency cell info list which is included in the System Information Block (SIB) 11 on the BCCH. The Inter-frequency cell info list contains only one cell. This setting is available only when the BCCH SIB 11 Cell Info List is set to "Present" (see CALL[:CELL]:BCCHannel:CELLlist ). If this setting is changed while the Operating Mode is "Active Cell.", the test set will perform the BCCH Update procedure. |
|
| Requirements | |
OUTPUT 714;"CALL:BCCHannel:INTERFREQ:DOWNlink:CHANnel 10735" ! Sets the BCCH Inter-frequency Cell DL UARFCN to 10735. |
|
THIS COMMAND IS OBSOLETE. Please use the CALL[:CELL]:BCCHannel:ITRFrequency:SCODe command. Sets/queries the primary scrambling code of the Inter-frequency cell info list which is included in the System Information Block (SIB) 11 on the BCCH. The Inter-frequency cell info list contains only one cell. This setting is available only when the BCCH SIB 11 Cell Info List is set to "Present" (see CALL[:CELL]:BCCHannel:CELLlist ). If this setting is changed while the Operating Mode is "Active Cell.", the test set will perform the BCCH Update procedure. |
|
OUTPUT 714;"CALL:BCCHannel:INTERFREQ:SCODe 63" ! Sets the BCCH Inter-frequency Cell Scrambling Code to 63. |
|
THIS COMMAND IS OBSOLETE. Please use the CALL[:CELL]:BCCHannel:ITAFrequency:SCODe command. Sets/queries the primary scrambling code of the 2nd cell in the Intra-frequency cell info list which is included in the System Information Block (SIB) 11 on the BCCH. This setting is available only when the BCCH SIB 11 Cell Info List is set to "Present" (see CALL[:CELL]:BCCHannel:CELLlist ). The Intra-frequency cell info list contains three cells. As required by the W-CDMA specifications, Cell 1 in this list is always the serving cell so the cell information is automatically set to match the test set's cell. If this setting is changed while the Operating Mode is "Active Cell.", the test set will perform the BCCH Update procedure. |
|
OUTPUT 714;"CALL:BCCHannel:INTRAFREQ:CELL2:SCODe 130" ! Sets the BCCH Intra-frequency Cell 2 Scrambling Code to 130. |
|
THIS COMMAND IS OBSOLETE. Please use the CALL[:CELL]:BCCHannel:ITAFrequency:SCODe command. Sets/queries the primary scrambling code of the 3rd cell in the Intra-frequency cell info list which is included in the System Information Block (SIB) 11 on the BCCH. This setting is available only when the BCCH SIB 11 Cell Info List is set to "Present" (see CALL[:CELL]:BCCHannel:CELLlist ). The Intra-frequency cell info list contains three cells. As required by the W-CDMA specifications, Cell 1 in this list is always the serving cell so the cell information is automatically set to match the test set's cell. If this setting is changed while the Operating Mode is "Active Cell.", the test set will perform the BCCH Update procedure. |
|
OUTPUT 714;"CALL:BCCHannel:INTRAFREQ:CELL3:SCODe 500" ! Sets the BCCH Intra-frequency Cell 3 Scrambling Code to 500. |
|
Sets/queries Intra-freq <num> Cell Cell Reselection Offset1 for each of the 8 intra-frequency neighbor cells. This parameter
can only be set when call status is |
|
|
The command
must be issued with a comma-separated
list of 8 values. Each value in the
list defines the |
|
| 0,0,0,0,0,0,0,0 (dB) | |
OUTPUT 714;"CALL:BCCHannel:ITAFrequency:CRESelection:OFFSet -20,-20,-20,-20,-20,-20,-20,-20" ! Sets Cell Reselection Offset1 for the first intra-frequency neighbor cell to -20 dB, ! sets Cell Reselection Offset1 for the second intra-frequency neighbor cell to -20 dB, etc. |
|
Sets/queries Intra-freq <num> Cell Cell Reselection Offset2 for each of the 8 intra-frequency neighbor cells. This parameter
can only be set when call status is |
|
|
The command
must be issued with a comma-separated
list of 8 values. Each value in the
list defines the |
|
| 0,0,0,0,0,0,0,0 (dB) | |
OUTPUT 714;"CALL:BCCHannel:ITAFrequency:CRESelection:OFFSet2 -20,-20,-20,-20,-20,-20,-20,-20" ! Sets Cell Reselection Offset2 for the first intra-frequency neighbor cell to -20 dB, ! sets Cell Reselection Offset2 for the second intra-frequency neighbor cell to -20 dB, etc. |
|
Sets/queries the primary scrambling code for each of the 8 intra frequency neighbor cells (see Intra-frequency Cells ). This parameter
can only be set when call status is |
|
|
The command must be issued with a comma-separated list of 8 values. Each value in the list defines the primary scrambling code for the corresponding neighbor cell (cell 1 through cell 8). Whether each cell is actually present in the cell info list transmitted by the test set is controlled by the CALL[:CELL]:BCCHannel:ITAFrequency:STATe setting. |
|
| 0,127,191,255,319,383,447,511 | |
OUTPUT 714;"CALL:BCCHannel:ITAFrequency:SCODe 0,127,192,255,320,384,448,511" ! Sets the scrambling code for the first intra frequency neighbor ! cell to 0, sets the scrambling code for the second intra ! frequency neighbor cell to 127, etc. |
|
Sets/queries whether each of the 8 intra frequency neighbor cells is included in the cell info list transmitted by the test set (see Intra-frequency Cells ). Changing
this setting results in the execution of the Broadcast
Channel (BCCH) Update Procedure (SIB Contents) if BCCH Update Page is set to |
|
|
The command must be issued with a comma-separated list of 8 valid settings. |
|
| 1,1,0,0,0,0,0,0 | |
OUTPUT 714;"CALL:BCCHannel:ITAFrequency:STATe 1,1,1,1,1,1,1,1" ! Includes all 8 intra frequency neighbor cells in the ! cell info list. |
|
Sets/queries Inter-freq <num> Cell Cell Reselection Offset1 for each of the 8 intra-frequency neighbor cells. This parameter
can only be set when call status is |
|
|
The command
must be issued with a comma-separated
list of 8 values. Each value in the
list defines the |
|
| 0,0,0,0,0,0,0,0 (dB) | |
OUTPUT 714;"CALL:BCCHannel:ITRFrequency:CRESelection:OFFSet -20,-20,-20,-20,-20,-20,-20,-20" ! Sets Cell Reselection Offset1 for the first inter-frequency neighbor cell to -20 dB, ! sets Cell Reselection Offset1 for the second inter-frequency neighbor cell to -20 dB, etc. |
|
Sets/queries Inter-freq <num> Cell Cell Reselection Offset2 for each of the 8 intra-frequency neighbor cells. This parameter
can only be set when call status is |
|
|
The command
must be issued with a comma-separated
list of 8 values. Each value in the
list defines the |
|
| 0,0,0,0,0,0,0,0 (dB) | |
OUTPUT 714;"CALL:BCCHannel:ITRFrequency:CRESelection:OFFSet2 -20,-20,-20,-20,-20,-20,-20,-20" ! Sets Cell Reselection Offset2 for the first inter-frequency neighbor cell to -20 dB, ! sets Cell Reselection Offset2 for the second inter-frequency neighbor cell to -20 dB, etc. |
|
Sets/queries the UARFCN for each of the 8 inter frequency neighbor cells (see Inter-frequency Cells ). This parameter
can only be set when call status is |
|
The command must be issued with a comma-separated list of 8 values. Each value in the list defines the UARFCN for the corresponding neighbor cell (cell 1 through cell 8). Whether each cell is actually present in the cell info list transmitted by the test set is controlled by the CALL[:CELL]:BCCHannel:ITRFrequency:STATe setting. |
|
| 10730,10730,10730,10730,10730,10730,10730,10730 | |
Test Application Revision: A.05 and above. Lab Application Revision: B.01 and above Test Application Revision: A.05.28 and above, added 1037 - 1062. Lab Application Revision: B.01 and above Lab Application Revision: B.01.29 and above, added 1037 - 1062. Test Application Revision A.09 and Lab Application Revision C.04 and D.00, changed channel ranges to match 3GPP TS 25.101 v7.2.0 (previously, channels supported were: 412-687, 1037-1062, 4320-4495, 4600-4825, 9000-9425, 9625-9975, and 10,525-10,875, resolution = 1). Test Application Revision A.11 and Lab Application Revisions D.02 and E.00, added 3112 to 3388, 3412, 3437, 3462, 3487, 3512, 3537, 3562, 3587, 3612, 3637, 3662, 3687 Test Application Revision A.14 and Lab Application Revision F.00, added 3837 - 3903, 3927, 3932, 3957, 3962, 3987, 3992, 4017 - 4043, 4067, 4092, 4117 - 4143, 4167, 4192 |
|
OUTPUT 714;"CALL:BCCHannel:ITRFrequency:DOWNlink:CHANnel 10730,10730,10730,10730, 10730,10730,10730,10730" ! Sets the UARFCN for each of the 8 inter frequency neighbor ! cells to 10730. |
|
Sets/queries the primary scrambling code for each of the 8 inter frequency neighbor cells (see Inter-frequency Cells ). This parameter
can only be set when call status is |
|
|
The command must be issued with a comma-separated list of 8 values. Each value in the list defines the primary scrambling code for the corresponding neighbor cell (cell 1 through cell 8). Whether each cell is actually present in the cell info list transmitted by the test set is controlled by the CALL[:CELL]:BCCHannel:ITRFrequency:STATe setting. |
|
| 0,127,191,255,319,383,447,511 | |
OUTPUT 714;"CALL:BCCHannel:ITRFrequency:SCODe 0,127,192,255,320,384,448,511" ! Sets the scrambling code for the first inter frequency neighbor ! cell to 0, sets the scrambling code for the second inter ! frequency neighbor cell to 127, etc. |
|
Sets/queries whether each of the 8 inter frequency neighbor cells is included in the cell info list transmitted by the test set (see Inter-frequency Cells ). This parameter
can only be set when call status is |
|
|
The command must be issued with a comma-separated list of 8 valid settings. |
|
| 1,0,0,0,0,0,0,0 | |
OUTPUT 714;"CALL:BCCHannel:ITRFrequency:STATe 1,1,1,1,1,1,1,1" ! Includes all 8 inter frequency neighbor cells in the ! cell info list. |
|
Sets/queries the N300 RRC Conn Req Max Retransmits . This setting
can only be changed when call status is |
|
| Same as setting | |
| 0 | |
OUTPUT 714;"CALL:BCCHannel:N300 0" ! Sets the N300 Constant to 0. |
|
Sets/queries the N312 Link Establishment In-Sync Count (Idle) . This setting
can only be changed when call status is |
|
| Same as setting | |
| 50 | |
OUTPUT 714;"CALL:BCCHannel:N312 50" ! Sets the N312 Constant to 50. |
|
Sets/queries the T313 Out-Of-Sync Reception Timer . This setting
can only be changed when call status is |
|
| Same as setting | |
| S2 | |
OUTPUT 714;"CALL:BCCHannel:N313 S200" ! Sets the N313 UE Out-Of-Sync Counter to S200 |
|
Sets/queries the N315 Successive In-Sync Reception Counter . This setting
can only be changed when call status is |
|
| Same as setting | |
| S50 | |
OUTPUT 714;"CALL:BCCHannel:N315 S1" ! Sets N315 UE In-Sync Counter to S1. |
|
The setting
form of this command performs two functions: (1) sets the
Sintersearch
value (see CALL[:CELL]:BCCHannel:SERSearch:VALue
) and (2) sets the The query
form of this command returns the This setting
can only be changed when call status is |
|
|
Sintersearch can be set to any even number value between -32 dB and +20 dB, but any negative value will be interpreted by the UE as 0 dB. |
|
| Same as setting | |
OUTPUT 714;"CALL:BCCHannel:SERSearch 4" ! Sets Sintersearch state to on and sets Sintersearch value to 4 dB. |
|
Sets/queries
the Sintersearch
state. The This parameter
can only be set when call status is |
|
| 1|0 | |
| 1 (on) | |
OUTPUT 714;"CALL:BCCHannel:SERSearch:STATe OFF" ! Turns Sintersearch state off. |
|
Sets/queries
the Sintersearch
value. The This parameter
can only be set when call status is |
|
|
Sintersearch can be set to any even number value between -32 dB and +20 dB, but any negative value will be interpreted by the UE as 0 dB. |
|
| Same as setting | |
| 0 dB | |
OUTPUT 714;"CALL:BCCHannel:SERSearch:VALue 4 DB" ! Sets the Sintersearch value to 4 dB. |
|
Sets/queries Transmit SIB5bis . This setting
can only be changed when call status is |
|
| Same as setting | |
| SBAN | |
Test Application Revision: A.01.01 and above Lab Application Revision: D.00.04 and above Test Application Revision A.11, Lab Application Revisions D.02 and E.00, added BAND10 and SBANds, changed default from BAND49 to SBANds. |
|
OUTPUT 714;"CALL:BCCHannel:SIB5:BIS SBANds" ! Sets Transmit SIB5bis to Standard Bands. |
|
Sets/queries
the This setting controls whether or not SIB19 shall be transmitted via the BCCH. |
|
| Range: PRES|ABS | |
| ABSent | |
OUTPUT 714;"CALL:BCCHannel:SIB19:INFormation PRESent" ! Sets the SIB19 information to Off. |
|
The setting
form of this command performs two functions: (1) sets the
Sintrasearch
value (see CALL[:CELL]:BCCHannel:SRASearch:VALue
) and (2) sets the The query
form of this command returns the This setting
can only be changed when call status is |
|
|
Sintrasearch can be set to any even number value between -32 dB and +20 dB, but any negative value will be interpreted by the UE as 0 dB. |
|
| Same as setting | |
OUTPUT 714;"CALL:BCCHannel:SRASearch 4" ! Sets Sintrasearch state to on and sets Sintrasearch value to 4 dB. |
|
Sets/queries
the Sintrasearch
state. The This parameter
can only be set when call status is |
|
| 1|0 | |
| 1 (on) | |
OUTPUT 714;"CALL:BCCHannel:SRASearch:STATe OFF" ! Turns Sintrasearch state off. |
|
Sets/queries
the Sintrasearch
value. The This parameter
can only be set when call status is |
|
|
Sintrasearch can be set to any even number value between -32 dB and +20 dB, but any negative value will be interpreted by the UE as 0 dB. |
|
| Same as setting | |
| 0 dB | |
OUTPUT 714;"CALL:BCCHannel:SRASearch:VALue 4 DB" ! Sets the Sintrasearch value to 4 dB. |
|
Sets/queries the T300 RRC Conn Req Retransmit Timer . This setting
can only be changed when call status is |
|
Range: MS100 | MS200 | MS400 | MS600 | MS800 | MS1000 | MS1200 | MS1400 | MS1600 | MS1800 | MS2000 | MS3000 | MS4000 | MS6000 | MS8000 |
|
| Same as setting | |
| MS400 | |
OUTPUT 714;"CALL:BCCHannel:T300 MS400" ! Sets the T300 Timer to 400 ms. |
|
Sets/queries the T305 Periodic Cell Update Timer . |
|
Range: MINS5 | MINS10 | MINS30 | MINS60 | MINS120 | MINS360 | MINS720 | INF |
|
| Same as setting | |
| INF | |
OUTPUT 714;"CALL:BCCHannel:T305 INF" ! Sets the T305 Timer to Infinity. |
|
Sets/queries the T308 RRC Conn Release Comp Retransmit Timer . |
|
| Same as setting | |
| MS40 | |
OUTPUT 714;"CALL:BCCHannel:T308 MS40" ! Sets the T308 Timer to 40 ms. |
|
Sets/queries the T309 CCO From UTRAN to 2G Connect Timer . This setting
can only be changed when call status is |
|
| Same as setting | |
| 8 seconds | |
OUTPUT 714;"CALL:BCCHannel:T309 8" ! Sets the T309 Timer to 8 seconds. |
|
Sets/queries the T312 Link Establishment Timer (Idle) . This setting
can only be changed when call status is |
|
| Same as setting | |
| 5 | |
OUTPUT 714;"CALL:BCCHannel:T312 5" ! Sets the T308 Timer to 40 ms. |
|
Sets/queries the T313 Out-Of-Sync Reception Timer . This setting
can only be changed when call status is |
|
| Same as setting | |
| 3 seconds | |
OUTPUT 714;"CALL:BCCHannel:T313 15" ! Sets the T313 UE Link Reestablishment Timer to 15 seconds. |
|
Sets/queries the T314 CS Domain Re-Establishment Timer . |
|
| Same as setting | |
| S0 | |
OUTPUT 714;"CALL:BCCHannel:T314 S8" ! Sets the T314 CS Domain Reestablishment Timer to 8 seconds. |
|
Sets/queries the T315 PS Domain Re-Establishment Timer . |
|
| Same as setting | |
| S0 | |
OUTPUT 714;"CALL:BCCHannel:T315 S10" ! Sets the T315 PS Domain Reestablishment Timer to 10 seconds. |
|
Function |
Sets/queries the T323 Fast Dormancy Timer . |
Setting |
Range: S0|S5|S10|S20|S30|S60|S90|S120 Unit: second |
Query |
Same as setting |
*RST Setting |
S0 |
Requirements |
Lab Application Revision: F.00.00 and above |
Programming Example OUTPUT 714;"CALL:BCCHannel:T323 S5" |
|
Sets/queries the T312 Link Establishment Timer (Idle) . This parameter
can only be set when call status is |
|
| Same as setting | |
| 0 | |
OUTPUT 714;"CALL:BCCHannel:T3212 10" ! Sets T3212 Periodic Location Update Timer to 10 decihours (1 hour). |
|
Sets/queries the T3312 Periodic RA Update Timer . To set the units for this timer, see CALL[:CELL]:BCCHannel:T3312:UNITs . |
|
| Same as setting | |
| 10 | |
OUTPUT 714;"CALL:BCCHannel:T3312 10" ! Sets T3312 Timer to 10. |
|
Sets/queries the T3312 Periodic RA Update Units . To set the value for this timer, see CALL[:CELL]:BCCHannel:T3312[:VALue] . |
|
| Range: SEC2 | MIN | DHO | DEAC | |
| DEAC | |
OUTPUT 714;"CALL:BCCHannel:T3312:UNITs DEAC" ! Sets T3312 timer's units to DEACtivated. |
|
Sets/queries the BCCH Update Page state (see BCCH Update Page and Broadcast Channel (BCCH) Update Procedure (SIB Contents) ). |
|
| INH | |
OUTPUT 714;"CALL:BCCHannel:UPDAtepage AUTO" ! Instructs the test set to send a Paging Type 1 message ! to the UE when a BCCH Update has occurred. |
|