|
|
|
Last updated: October 30, 2013
CALL:FDDTest:MACEHS:DTBLocks:SDTX:RBEHavior
CALL:FDDTest:MACEHS:PTBLock:RVSequence
CALL:FDDTest:MACEHS:STBLock:RVSequence
CALL:FDDTest:OCNSource:CONFig:STATe:HSDPa
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -13 dB (on) | |
OUTPUT 714;"CALL:FDDTest:ANTenna2:CPIChannel:SLEVel:HSDPa -13" ! Sets the FDD Test P-CPICH power offset Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -13 dB (on) | |
OUTPUT 714;"CALL:FDDTest:ANTenna2:CPIChannel:SLEVel:HSPA -13" ! Sets the FDD Test P-CPICH power offset Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -13 dB (on) | |
OUTPUT 714;"CALL:FDDTest:ANTenna2:CPIChannel:SECondary:SLEVel:HSDPa -13" ! Sets the FDD Test S-CPICH power offset Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -13 dB (on) | |
OUTPUT 714;"CALL:FDDTest:ANTenna2:CPIChannel:SECondary:SLEVel:HSPA -13" ! Sets the FDD Test S-CPICH power offset Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the See FDD Test Operating Mode . |
|
| Same as setting | |
| -5.35 dB (on) | |
OUTPUT 714;"CALL:FDDTest:CCPChannel:PRIMary -13" ! Sets the FDD Test P-CCPCH/SCH Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -12 dB (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CCPChannel:PRIMary:HSDPa -13" ! Sets the HSDPA FDD Test P-CCPCH/SCH Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -12 dB (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CCPChannel:PRIMary:HSPA -13" ! Sets the HSPA FDD Test P-CCPCH/SCH Level to -13 dB and turns its state on. |
|
|
Sets/queries the The |
|
| Same as setting | |
| -5.35 dB | |
OUTPUT 714;"CALL:FDDTest:CCPChannel:PRIMary:LEVel -7" |
|
|
Sets/queries the The |
|
| Same as setting. | |
| -12 dB | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CCPChannel:PRIMary:LEVel:HSDPa -7" |
|
|
Sets/queries the The |
|
| Same as setting. | |
| -12 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CCPChannel:PRIMary:LEVel:HSPA -7" |
|
|
Sets/queries the The |
|
| 1 (on) | |
OUTPUT 714;"CALL:FDDTest:CCPChannel:PRIMary:STATe ON" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CCPChannel:PRIMary:STATe:HSDPa ON" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CCPChannel:PRIMary:STATe:HSPA ON" |
|
|
Sets/queries the FDD Test UL CL Power Ctrl Algorithm . |
|
| Same as setting | |
| ALG2 | |
OUTPUT 714;"CALL:FDDTest:CLPControl:UPLink:ALGorithm ALG1" ! Sets FDD Test UL CL Power Ctrl Algorithm to One. |
|
|
Sets/queries the FDD Test UL CL Power Ctrl Mode . |
|
| UDOW | |
|
Test or Lab Application Revision: A.01 and above |
|
OUTPUT 714;"CALL:FDDTest:CLPCONTROL:UPLink:MODE UDOWN" !Sets the closed loop power control mode to alternating up, down bits. |
|
|
Sets/queries the FDD Test UL CL Power Ctrl Stepsize when FDD Test UL CL Power Ctrl Algorithm is set to |
|
| Same as setting | |
| 1 dB | |
OUTPUT 714;"CALL:FDDTest:CLPControl:UPLink:STEPsize 2 dB" ! Sets FDD Test UL CL Power Ctrl Stepsize to 2 dB. |
|
|
Sets/queries Deactivation Type . |
|
| Same as setting. | |
| IMM | |
OUTPUT 714;"CALL:FDDTest:COMPressed:DACTivation:TYPe CFN" ! Sets deactivation type to CFN. |
|
|
Sets/queries Ending CFN . |
|
| Same as setting. | |
| 0 | |
OUTPUT 714;"CALL:FDDTest:COMPressed:ECFNumber 16" |
|
|
This command is obsolete. Please use CALL:FDDTest:COMPressed:TGPSequence:ALL:SCFNumber or CALL:FDDTest:COMPressed:TGPSequence([1]|2|3|4):SCFNumber . |
|
| Same as setting. | |
| 0 | |
OUTPUT 714;"CALL:FDDTest:COMPressed:SCFNumber 4" |
|
|
Sets/queries <num> TG Starting CFN for the first through fourth TGPSs (the first num value sets |
|
| Same as setting. | |
| 0,2,6,14 | |
| Lab Application Revision: D.00.04 and above. | |
OUTPUT 714;"CALL:FDDTest:COMPressed:TGPSequence:ALL:SCFNumber 0,4,12,28" ! Sets First TG Starting CFN to 0, Second TG Starting CFN to 4, ! Third TG Starting CFN to 12, and Fourth TG Starting CFN to 28. |
|
|
Sets/queries <num> TG Starting CFN for the first, second, third or fourth TGPS (sending :TGPSequence or :TGPSequence1 sets |
|
| Same as setting. | |
| Lab Application Revision: D.00.04 and above. | |
OUTPUT 714;"CALL:FDDTest:COMPressed:TGPSequence3:SCFNumber 12" ! Sets Third TG Starting CFN to 12. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the See FDD Test Operating Mode . |
|
| Same as setting | |
| -3.3 dB (on) | |
OUTPUT 714;"CALL:FDDTest:CPIChannel -13" ! Sets the FDD Test CPICH Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CPIChannel:HSDPa -13" ! Sets the HSDPA FDD Test CPICH Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CPIChannel:HSPA -13" ! Sets the HSPA FDD Test CPICH Level to -13 dB and turns its state on. |
|
|
Sets/queries the The |
|
| Same as setting | |
| -3.3 dB | |
OUTPUT 714;"CALL:FDDTest:CPIChannel:LEVel -7" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -10 dB | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CPIChannel:LEVel:HSDPa -7" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -10 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CPIChannel:LEVel:HSPA -7" |
|
|
Sets/queries the The |
|
| 1 (on) | |
OUTPUT 714;"CALL:FDDTest:CPIChannel:STATe ON" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CPIChannel:STATe:HSDPa ON" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:CPIChannel:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the See FDD Test Operating Mode . |
|
| Same as setting | |
| -10.3 dB (on) | |
OUTPUT 714;"CALL:FDDTest:DPCHannel -13" ! Sets the FDD Test DPCH Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:DPCHannel:HSDPa -13" ! Sets the HSDPA FDD Test DPCH Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:DPCHannel:HSPA -13" ! Sets the HSPA FDD Test DPCH Level to -13 dB and turns its state on. |
|
| Sets/queries DPCH Frame Offset . | |
| Same as setting | |
| 0 (0 x 256 chips) | |
|
Test Application Revision: A.09 and above |
|
OUTPUT 714;"CALL:FDDTest:DPCHannel:FOFFset 6" ! Sets DPCH Frame Offset to 6 x 256 chips. |
|
|
Sets/queries the The |
|
| Same as setting | |
| -10.3 dB | |
OUTPUT 714;"CALL:FDDTest:DPCHannel:LEVel -7" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -10 dB | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:DPCHannel:LEVel:HSDPa -7" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -10 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:DPCHannel:LEVel:HSPA -7" |
|
|
Sets/queries the The |
|
| 1 (on) | |
OUTPUT 714;"CALL:FDDTest:DPCHannel:STATe ON" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:DPCHannel:STATe:HSDPa ON" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:DPCHannel:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -20 dB (on) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:EAGChannel -20"
! Sets the |
|
|
Sets/queries the The |
|
| Same as setting | |
| -20 dB | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:EAGChannel:LEVel -20" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:EAGChannel:STATe ON" |
|
|
Sets/queries FDD Test E-DPDCH Max Channel Codes . |
|
| TSF4 | |
|
Test Application Revision A.12 and above, with the required feature license. Lab Application Revision: E.00.16 and above. |
|
OUTPUT 714;"CALL:FDDTest:EDPDchannel:CCODes:MAX TSF4" ! Sets FDD Test E-DPDCH Max Channel Codes to 2SF4. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -20 dB (on) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:EHIChannel -20"
! Sets the |
|
|
Sets/queries the The |
|
| Same as setting | |
| -20 dB | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:EHIChannel:LEVel -20" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:EHIChannel:STATe ON" |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -20 dB (off) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:ERGChannel -20"
! Sets the |
|
|
Sets/queries the The |
|
| Same as setting | |
| -20 dB | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:ERGChannel:LEVel -20" |
|
|
Sets/queries the The |
|
| 0 (off) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:ERGChannel:STATe OFF" |
|
| Sets/queries FDD Test Mode F-DPCH Slot Format. | |
| Same as setting | |
| 0 | |
OUTPUT 714;"CALL:FDDTest:FDPChannel:SLOT:FORMat 0" ! Sets FDD Test Mode F-DPCH Slot Format to 0. |
|
|
Sets/queries the FDD Test F-DPCH State . |
|
| 0 (off) | |
OUTPUT 714;"CALL:FDDTest:FDPChannel:STATe OFF" |
|
|
Sets/queries the FDD Test Primary Precoding Weight . |
|
| Same as setting | |
| DEF3412101 | |
|
Test Application Revision: A.20.00 and above, with the required feature license Lab Application Revision: I.00.00 and above. |
|
OUTPUT 714;"CALL:FDDTest:FRC:MIMO:PPWeight:CONFig DEF3412101" ! Sets the downlink primary precoding weight to be determined as per the specification in the TS34.121-1 section 9.2.4. |
|
|
Sets/queries the FDD Test "FRC Type" . |
|
|
QAM1|QAM2|QAM3|QAM3A |QAM6|QAM6A|QAM64H8|QAM64H8A|QAM16H10| QAM16H10A|QPSK1|QPSK2 |QPSK3||QPSK3A|QPSK4|QPSK5|QPSK6|QPSK6A| |
|
| Same as setting | |
| QPSK1 | |
|
Test Application Revision A.08 and above, with the required feature license. Lab Application Revision: C.03 and above. Test Application Revision A.10.01 and Lab Application Revision D.01.01 added QAM6 and QPSK6. Lab Application Revision F.00 added QAM64H8, QAM16H10, QPSKH10. Test Application Revision: A.19.00 and above with the required feature license and Lab Application Revision: H.01.00 and above, added QPSK3A, QAM16H3A, QPSK6A, QAM16H6A, QAM64H8A, QPSK10A, QAM16H10A, QPSK12. |
|
OUTPUT 714;"CALL:FDDTest:FRC:TYPE QPSK2" ! Sets FRC Type to H-Set 2 QPSK. |
|
|
Sets/queries |
|
|
(The return string is always 4 characters from the set 0123456789ABCDEF, enclosed by double quotes.) |
|
| "AAAA" | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HRNTi 'EEEE'" ! Sets FDD Test Primary H-RNTI (Hex) to EEEE. |
|
|
Sets/queries |
|
|
(The return string is always 4 characters from the set 0123456789ABCDEF, enclosed by double quotes.) |
|
| "5555" | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HRNTi:ALTernate '2222'" ! Sets FDD Test Alternate H-RNTI (Hex) to 2222. |
|
|
Sets/queries FDD Test "HS-SCCH1 Alternate H-RNTI (Hex)" . |
|
|
(The return string is always 4 characters from the set 0123456789ABCDEF, enclosed by double quotes.) |
|
| "5555" | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HRNTi:ALTernate '2222'" ! Sets FDD Test HS-SCCH 1 Alternate H-RNTI (Hex) to 2222. |
|
|
Sets/queries FDD Test "HS-SCCH2 Alternate H-RNTI (Hex)" . |
|
|
(The return string is always 4 characters from the set 0123456789ABCDEF, enclosed by double quotes.) |
|
| "5555" | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HRNTi:ALTernate '2222'" ! Sets FDD Test HS-SCCH 2 Alternate H-RNTI (Hex) to 2222. |
|
|
Sets/queries FDD Test "HS-SCCH2 Alternate H-RNTI (Hex)" . |
|
|
(The return string is always 4 characters from the set 0123456789ABCDEF, enclosed by double quotes.) |
|
| "5555" | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HRNTi:ALTernate '2222'" ! Sets FDD Test HS-SCCH 3 Alternate H-RNTI (Hex) to 2222. |
|
|
Sets/queries FDD Test "HS-SCCH4 Alternate H-RNTI (Hex)" . |
|
|
(The return string is always 4 characters from the set 0123456789ABCDEF, enclosed by double quotes.) |
|
| "5555" | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HRNTi:ALTernate '2222'" ! Sets FDD Test HS-SCCH 4 Alternate H-RNTI (Hex) to 2222. |
|
|
Sets/queries the FDD Test Dual Carrier Band Configuration . This parameter can only be set when |
|
| Same as setting | |
| SBANd | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDPa:MCARrier:BAND:CONFig:TYPE SBANd" ! Sets the FDD Test primary and secondary serving cell DL UARFCN use UARFCNs that are in the single band. |
|
| Sets/queries FDD Test "RB Test HS-DSCH Configuration Type" . | |
| Same as setting | |
| FRC | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:CONFig UDEFined" ! Sets FDD Test HS-DSCH Configuration Type to User Defined. |
|
|
Sets/queries FDD Test "HS-DSCH Data Pattern" . |
|
| PRBS15 | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:DATA ONES" ! Sets FDD Test HS-DSCH Data Pattern to All Ones. |
|
|
Sets/queries FDD Test "N_cqi_typeA/M_cqi Ratio" . |
|
|
Range: R1To2| R2To3|R3To4| |R4To5|R5To6|R6To7|R7To8|R8To9|R9To10|R1To1 |
|
| Same as setting | |
| R1To1 | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:MIMO:NMRatio R1To1" ! Sets the N_cqi_typeA/M_cqi ratio on the HS-DPCCH to 1/1 when operating in FDD Test Mode. |
|
|
Sets/queries FDD Test Static Primary Precoding Weight . |
|
| Same as setting | |
| 0 | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:MIMO:PPWeight:STATic 2" ! Sets the primary precoding weight applied in the FDD Test Mode to 2. |
|
|
Sets/queries FDD Test Mode "Number of Transport Blocks" . |
|
| Same as setting | |
| 1 | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:MIMO:TBLock:COUNt 2" ! Sets the number of transport blocks scheduled on the HS-DSCH to 2 when operating in FDD Test Mode. |
|
|
Sets/queries FDD Test UE HS-DSCH Category . This command is only applicable when CALL:FDDTest:HSDSchannel:UDEFined:MS:IREDundancy:BUFFer:ALLocation is set to |
|
| Same as setting | |
| 1 | |
|
Test Application Revision: A.09 and above, with the required feature license Lab Application Revision: C.04 and above Lab Application Revision: D.00 and above Test Application Revision A.10 and Lab Application Revision D.01 added UE categories 7 and 8 Test Application Revision: A.19.00 and above with the required feature license, added 21-24. |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:MS:CATegory 12" ! Sets FDD Test UE HS-DSCH Category to 12. |
|
| Sets/queries FDD Test "User Defined Number of HARQ Processes" . | |
| Same as setting | |
| 2 | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:HARQ:PROCess:COUNt 1" ! Sets FDD Test User Defined Number of HARQ Processes to 1. |
|
| Sets/queries FDDT "User Defined Number of Active HS-PDSCHs" . | |
| Same as setting | |
| 5 | |
|
Test Application Revision: A.09 and above, with the required feature license Lab Application Revision: C.04 and above Lab Application Revision: D.00 and above Test Application Revision A.10 and Lab Application Revision D.01 expanded range from "1 to 5" to "1 to 10" Test Application Revision A.15 and Lab Application Revision F.01 expanded range from "1 to 10" to "1 to 15" |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:HSPDschannel:COUNt 3" ! Sets FDDT User Defined Number of Active HS-PDSCHs to 3. |
|
| Sets/queries FDD Test "User Defined Inter-TTI Interval" . | |
| Same as setting | |
| 3 | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:ITTI 1" ! Sets FDD Test User Defined Inter-TTI Interval to 1. |
|
| Sets/queries FDD Test "User Defined HS-DSCH MAC Entity" . | |
| Range: HSPeed | EHSPeed | |
| HSPeed | |
|
Lab Application Revision: F.00 and above Test Application Revision: A.14 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:MAC HSPeed" ! Sets the FDD Test Mode HS-DSCH MAC entity to MAC-hs. |
|
| Sets/queries FDD Test "User Defined MAC-ehs HS-DSCH TB Size Table" . | |
| Range: BIT | OCTet | |
| OCTet | |
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:MACEHS:TBSTable:ALIGnment OCTet" ! Sets the FDD Test Mode MAC-ehs HS-DSCH TB size table to octet-aligned. |
|
|
Sets/queries FDD Test HSDPA MIMO State This application requires the installation of 8.0 hardware or later. This setting can not be configured when |
|
| Range: 1|0 | |
| 0 (OFF) | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:MIMO:STATe ON" ! Sets the MIMO be configured in the serving cell when operating in FDD Test Mode. |
|
|
Sets/queries FDD Test Number of HARQ Processes for MIMO |
|
| Same as setting | |
| 12 | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:MIMO:HARQ:PROCess:COUNt 14" ! Sets the number of HARQ processes that are active in the MAC-ehs layer to 14 when |
|
|
Sets/queries FDD Test "User Defined Modulation Type" . The setting is for the primary transport block when MIMO is configured. Setting the modulation type with the value lower than FDD Test "Secondary TB Modulation Type" will post the error message: "FDD call operation rejected; primary transport modulation type must not be lower than secondary transport block modulation type". |
|
| Same as setting | |
| QPSK | |
|
Test Application Revision: A.09 and above, with the required feature license Lab Application Revision: C.04 and above Lab Application Revision: D.00 and above Lab Application Revision: F.00 and Test Application Revision: A.14, added QAM64 |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:MODulation QAM16" ! Sets FDD Test User Defined Modulation Type to 16QAM. |
|
|
Sets/queries FDD Test User Defined UE IR Buffer Allocation . When this command is set to When this command is set to |
|
| Same as setting | |
| IMPLicit | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:MS:IREDundancy:BUFFer:ALLocation EXPLicit" ! Sets FDD Test User Defined UE IR Buffer Allocation to Explicit. |
|
|
Sets/queries FDDT "User Defined Explicit UE IR Buffer Size" . This command is only applicable when CALL:FDDTest:HSDSchannel:UDEFined:MS:IREDundancy:BUFFer:ALLocation is set to |
|
|
Range: 800, 1600, 2400, 3200, 4000, 4800, 5600, 6400, 7200, 8000, 8800, 9600, 10400, 11200, 12000, 12800, 13600, 14400, 15200, 16000, 17600, 19200, 20800, 22400, 24000, 25600, 27200, 28800, 30400, 32000, 36000, 40000, 44000, 48000, 52000, 56000, 60000, 64000, 68000, 72000, 76000, 80000, 88000, 96000, 104000, 112000, 120000, 128000, 136000, 144000, 152000, 160000, 176000, 192000, 208000, 224000, 240000, 256000, 272000, 288000, 304000 |
|
| Same as setting | |
| 19200 | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:MS:IREDundancy:BUFFer:SIZE 9600" ! Sets FDDT User Defined Explicit UE IR Buffer Size to 9600. |
|
|
Sets/queries FDD Test "Secondary TB Modulation Type" and determines the actual transport block size described in Test Mode User Def TBS(Secondary Data Stream) . Setting the modulation type to 64 QAM when FDD Test "User Defined 64QAM State" is Setting the modulation type with the value higher than FDD Test "User Defined Modulation Type" will post the error message: "FDD call operation rejected; primary transport modulation type must not be lower than secondary transport block modulation type". |
|
| Same as setting | |
| QPSK | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:STBLock:MODulation:TYPE QPSK" ! Sets the secondary transport block modulation type to QPSK when |
|
|
Sets/queries FDD Test "Secondary TB Size Index" . |
|
| Same as setting | |
| 62 | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:STBSize:INDex 48" ! Sets the secondary transport block size index to 48 when |
|
|
Sets/queries FDDT "User Defined Transport Block Size Index" . You can query the transport block size using the CALL:STATus:HSDSchannel:TBSize? query. |
|
| Same as setting | |
| 62 | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:TBSize:INDex 48" ! Sets FDDT User Defined Transport Block Size Index to 48. |
|
|
Sets/queries FDD Test "User Defined 64QAM State" . This parameter is used when CALL:FDDTest:HSDSchannel:UDEFined:MAC is set to |
|
| 0 (OFF) | |
OUTPUT 714;"CALL:FDDTest:HSDSchannel:UDEFined:QAM64:STATe OFF" |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -3 dB (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSPDschannel -4"
! Sets the |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -3 dB (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSPDschannel:HSPA -4"
! Sets the |
|
|
THIS COMMAND IS OBSOLETE. Please use CALL:FDDTest:HSPDschannel:CCODe:CODE . Sets/queries FDD Test First HS-PDSCH Channelization Code . |
|
|
Range: CODE5|CODE6|CODE7|CODE8|CODE9|CODE10|CODE11|CODE12|CODE13|CODE14 |
|
| Same as setting | |
| CODE7 | |
|
Test Application Revision A.08 and above, with the required feature license. Lab Application Revision: C.03 and above. Test Application Revision A.10.01 and Lab Application Revision D.01.01 added CODE5 and CODE6. |
|
OUTPUT 714;"CALL:FDDTest:HSPDschannel:CCODe CODE8" ! Sets FDD Test First HS-PDSCH Channelization Code to 8. |
|
|
Sets/queries FDD Test First HS-PDSCH Channelization Code . |
|
| Same as setting | |
| 7 | |
OUTPUT 714;"CALL:FDDTest:HSPDschannel:CCODe:CODE 7" ! Sets FDD Test First HS-PDSCH Channelization Code to 7. |
|
|
Sets/queries the The |
|
| Same as setting | |
| -3 dB | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSPDschannel:LEVel -4" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -3 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSPDschannel:LEVel:HSPA -4" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSPDschannel:STATe ON" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSPDschannel:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel -11"
! Sets the |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel:HSPA -11"
! Sets the |
|
|
Sets/queries the FDD Test Mode HSDPA/HSPA HS-SCCH 1 Channel Configuration State. |
|
| 1 (on) | |
OUTPUT 714;"CALL:FDDTest:HSSCchannel:CONFig:STATe ON" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -10 dB | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel:LEVel -11" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -10 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel:LEVel:HSPA -11" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel:STATe ON" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel2 -11"
! Sets the |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel2:HSPA -11"
! Sets the |
|
|
Sets/queries the FDD Test Mode HSDPA/HSPA HS-SCCH 2 Channel Configuration State. |
|
| 1 (on) | |
OUTPUT 714;"CALL:FDDTest:HSSCchannel2:CONFig:STATe ON" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel2:LEVel -11" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel2:LEVel:HSPA -11" |
|
|
Sets/queries the The |
|
| 0 (off) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel2:STATe ON" |
|
|
Sets/queries the The |
|
| 0 (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel2:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel3 -11"
! Sets the |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel3:HSPA -11"
! Sets the |
|
|
Sets/queries the FDD Test Mode HSDPA/HSPA HS-SCCH 3 Channel Configuration State. |
|
| 1 (on) | |
OUTPUT 714;"CALL:FDDTest:HSSCchannel3:CONFig:STATe ON" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel3:LEVel -11" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel3:LEVel:HSPA -11" |
|
|
Sets/queries the The |
|
| 0 (off) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel3:STATe ON" |
|
|
Sets/queries the The |
|
| 0 (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel3:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel4 -11"
! Sets the |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel4:HSPA -11"
! Sets the |
|
|
Sets/queries the FDD Test Mode HSDPA/HSPA HS-SCCH 4 Channel Configuration State. |
|
| 1 (on) | |
OUTPUT 714;"CALL:FDDTest:HSSCchannel4:CONFig:STATe ON" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel4:LEVel -11" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel4:LEVel:HSPA -11" |
|
|
Sets/queries the The |
|
| 0 (off) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel4:STATe ON" |
|
|
Sets/queries the The |
|
| 0 (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:HSSCchannel4:STATe:HSPA ON" |
|
|
Sets/queries the MAC-hs Header . |
|
| PRES | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:MACHs:HEADer DATA" ! Sets the MAC-hs Header to Used for Data. |
|
|
Sets/queries the |
|
| Same as setting | |
| 4 | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:MACHs:NTRans 2" ! Sets the FDD Test Number of Transmissions to 2. |
|
|
Sets/queries the Note: The number of RV parameters in the sequence that are used is determined by the |
|
|
Range: Comma separated list of 1 to 8 characters from the set 01234567. |
|
|
Range: Comma separated list of 8 characters from the set 01234567, enclosed by double quotes (if you enter fewer than 8 characters, the query result will fill the remaining characters with zeros). |
|
| 0,2,5,6,0,0,0,0 | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:MACHs:RVSequence '0,2,7,4,3,1'" ! Sets the FDD Test RV Sequence to 0,2,7,4,3,1,0,0. |
|
|
Sets/queries the |
|
| Same as setting | |
| SDTX | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:MACHs:SDTX:RBEHavior ACK" ! Sets the FDD Test statDTX Reception Behavior to Handle as ACK. |
|
|
Sets/queries the MAC-hs Transmit Window Size . This setting is only applicable if CALL:FDDTest:MACHs:HEADer is set to |
|
| Same as setting | |
| PDU16 | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:MACHs:WSIZe:TRANsmit PDU12" ! Sets the MAC-hs Transmit Window Size to 12. |
|
|
Sets/queries the FDD Test "statDTX Reception Behavior" . |
|
| Same as setting | |
| PSSSdtx | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:MACEHS:DTBLocks:SDTX:RBEHavior PSSSdtx" ! Sets the test set respond to a statDTX from the UE when two transport blocks were scheduled as statDTX/statDTX when operating in FDD Test Mode. |
|
|
Sets/queries the FDD Test "RV Sequence for MIMO Primary Transport Block" . |
|
|
Range: Comma separated list of 1 to 8 characters from the set 01234567, each entry being an integer of 0 to 3. |
|
| Range: Comma separated list of 8 characters from the set 01234567, enclosed by double quotes (if you enter fewer than 8 characters, the query result will fill the remaining characters with zeros). | |
| 0,3,2,1,0,0,0,0 | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:MACEHS:PTBLock:RVSequence 0,3,2,1,0,0,0,0" ! Sets the Redundancy Version Sequence used for each transmission of a particlular primary transport block to 0,3,2,1,0,0,0,0 when operating in FDD Test Mode. |
|
|
Sets/queries the FDD Test "RV Sequence for MIMO Secondary Transport Block" . |
|
|
Range: Comma separated list of 1 to 8 characters from the set 01234567, each entry being an integer of 0 to 3. |
|
| Range: Comma separated list of 8 characters from the set 01234567, enclosed by double quotes (if you enter fewer than 8 characters, the query result will fill the remaining characters with zeros) | |
| 0,3,2,1,0,0,0,0 | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:MACEHS:STBLock:RVSequence 0,3,2,1,0,0,0,0" ! Sets the Redundancy Version Sequence used for each transmission of a particlular secondary transport block to 0,3,2,1,0,0,0,0 when operating in FDD Test Mode. |
|
|
Sets/queries the FDD Test HSDPA/HSPA orthogonal channel noise simulator (OCNS) 1 to 6 Power Offsets (raletive levels). |
|
| 0 dB | |
OUTPUT 714;"CALL:FDDTest:OCNSource:POFFset:HSDPa 0, 0, 0, 0, 0, 0" |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the See FDD Test Operating Mode . |
|
| Same as setting | |
| -8.33 dB (on) | |
OUTPUT 714;"CALL:FDDTest:PICHannel -13" ! Sets the FDD Test PICH Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -15 dB (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:PICHannel:HSDPa -13" ! Sets the HSDPA FDD Test PICH Level to -13 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the The query form of this command returns the |
|
| Same as setting | |
| -15 dB (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:PICHannel:HSPA -13" ! Sets the HSPA FDD Test PICH Level to -13 dB and turns its state on. |
|
|
Sets/queries the DL PICH Data . The pattern can be set to either all ones or all zeros. |
|
| All Zeros | |
OUTPUT 714;"CALL:FDDTest:PICHannel:DATA ALLONE" ! Sets the paging indicator channel data to all ones. |
|
|
Sets/queries the The |
|
| Same as setting | |
| -8.33 dB | |
OUTPUT 714;"CALL:FDDTest:PICH:LEVel -7" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:PICH:LEVel:HSDPa -7" |
|
|
Sets/queries the The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:PICH:LEVel:HSPA -7" |
|
|
Sets/queries the The |
|
| 1 (on) | |
OUTPUT 714;"CALL:FDDTest:PICHannel:STATe ON" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.08 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:PICHannel:STATe:HSDPa ON" |
|
|
Sets/queries the The |
|
| 1 (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:FDDTest:PICHannel:STATe:HSPA ON" |
|
|
Sets/queries FDD Test Secondary Cell DL Channel Config . This setting is only allowed to be changed when the |
|
| Range: ADJacent| MANual | |
| ADJacent | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:SSCell:CHANnel:CONFig:TYPE MANual" |
|
|
Sets/queries the FDD Test Secondary Cell DL Manual UARFCN . |
|
|
|
| Same as setting | |
| 3012 | |
| Requirements |
Test Application Revision: A.20.00 and above, with the required feature license |
OUTPUT 714;"CALL:FDDTest:SSCell:CHANnel:MANual:UARFcn 3012" |
|
|
Sets/queries the FDD Test Secondary Cell Manual Band Arbitrator . |
|
| BAND6 | |
|
Test Application Revision: A.20.00 and above, with the required feature license |
|
OUTPUT 714;"CALL:FDDTest:SSCell:CHANnel:MANual:BARBitrator BAND6" |
|
|
Sets/queries the DL TFCI Pattern . |
|
|
(0 to 3 characters from the set 0123456789aAbBcCdDeEfF, up to 3FF) |
|
|
(The return string is always 3 characters from the set 0123456789ABCDEF, up to 3FF) |
|
| "000" | |
OUTPUT 714;"CALL:FDDTEST:TFCINDICATOR '2DE'" |
|
|
Sets/queries Uplink TFCI Control . |
|
| 0 (manual) | |
OUTPUT 714;"CALL:FDDTEST:UPLink:TFCIndicator:CONTrol:AUTO 1" ! Sets Uplink TFCI Control to Auto. |
|
|
Sets/queries Manual Uplink TFCI . This setting is only applicable when CALL:FDDTest:UPLink:TFCIndicator:CONTrol:AUTO is set to |
|
| DTDC | |
OUTPUT 714;"CALL:FDDTEST:UPLink:TFCIndicator:MANual DTCH" ! Sets Manual Uplink TFCI to DTCH Only. |
|
|
|
|