Home > E-UTRAN / WCDMA Interworking
This section is only applicable to the lab application.
E-UTRAN/WCDMA interworking relates to the test set working together with the Keysight E6621A PXT (See note below) to perform inter-Radio Access Technologies operations. This allows you to test the multi-mode wireless devices for LTE-WCDMA inter-RAT performance while using the test set as the WCDMA network simulator. In particular, the test set supports the following test scenarios:
For the hardware connection for these tests, see E-UTRAN / WCDMA Interworking Physical Connection .
For the inter-RAT frequency and priority information, see SIB19 Information .
For detailed guidance on how to use the E6621A PXT, please refer to the E6621A user's guide at
http://cp.literature.keysight.com/litweb/pdf/E6621-90002.pdf
Before any LTE-WCDMA inter-RAT test, you must first set up a connection between the two simulators, for signaling and packet data transferring. Namely, you must set up the E-UTRAN / WCDMA Interworking Parameters and connect to the external LTE simulator successfully before performing any inter-RAT operations.
Manual Operation: You can access the following menu from the
CALL SETUP
hardkey, go to the left side
Call Control 6 of 6
, then press the
E-UTRAN/WCDMA Interworking Info
(
F2
).
Ext EPC IP Addr
Specifies the external EPC's IPv4 address, i.e. the IPv4 address of the LTE simulator for the test set to set up a connection via LAN.
This setting is non-volatile (it persists across partial and full presets and power-cycling the test set).
GPIB Command: SYSTem:COMMunicate:LAN:EPCore:ADDRess
Connect To External EPC
This action establishes a connection between the test set and the LTE simulator specified by
Ext EPC IP Addr
. When a connection is successfully set up, check the
External EPC Conn Status
for
Connected
and check the
Connected EPC IP Address
for the IPv4 address of the connected LTE simulator.
GPIB Command: SYSTem:COMMunicate:LAN:EPCore:CONNect
Disconnect From External EPC
When a connection is established between the test set and the LTE simulator, this action disconnects the test set from the LTE simulator specified by
Ext EPC IP Addr
. The
External EPC Conn Status
shows
Not Connected
if there is no connection present.
GPIB Command: SYSTem:COMMunicate:LAN:EPCore:DCONnect
External EPC Conn Status
Indicates the external EPC connection status, whether there is a connection present between the test set and the LTE simulator.
GPIB Command: SYSTem:STATus:COMMunicate:LAN:EPCore:CONNected[:STATe]?
Connected EPC IP Address
Indicates the IP address of the connected LTE simulator.
GPIB Command: SYSTem:STATus:COMMunicate:LAN:EPCore:CONNected:ADDRess?
The figure below shows a typical Physical connection for E-UTRAN /WCDMA interworking.
Note that there are two LAN Ports on the rear panel of the test set (See Rear Panel Connectors ). For E-UTRAN /WCDMA interworking, LAN 2 PORT is required to exchange signaling message or packet data. LAN 1 PORT is optional, but it is still useful for other LAN operations such as protocol logging, firmware downloads or screen captures.
Control 1 of 2
,
LAN IP Address 2 (Data+)
setting is at the bottom of
Instrument Setup
(F1) menu.
Ext EPC IP Addr
must not be identical to the
LAN IP Address
setting. When the connection is successfully set up,
Ext EPC IP Addr
can not be changed.