Last updated: January 16, 2009
This section is only applicable to the lab application.
 PRACH Preambles 
and
 PRACH Ramping Cycles (MMAX) 
settings
 
The measurement requires a minimum of 3 PRACH preambles, so 
PRACH Preambles
 must be no less than 3. It is also recommended that you set
 PRACH Preambles 
to no greater than 3 and set 
PRACH Ramping Cycles (MMAX)
 to
 1 
to allow the UE's PRACH sequence to end as soon as possible. This helps avoid the following issue: 
Test set may lock up if operations are attempted before the UE completes its PRACH sequence
.
 Call Limit State 
to
 Off 
before Initiating a PRACH Measurement
 
It is recommended that you set 
Call Limit State
 to
 Off 
before initiating this measurement. Then, when the measurement completes, if the UE is still sending PRACH preambles to the test set, the test set will acknowledge the UE. Note, when the test set acknowledges the UE, the call is not completed because the UE is attempting to establish a test set-originated call, whereas the test set acknowledges the UE expecting a UE-originated call. Acknowledging the UE helps prevent the UE from placing the test set into its cell barred list (see 
Test Set in Cell Barred List
). When the test set acknowledges the UE, you will see the call status move from
 Paging 
to 
Idle
, to
 Setup
, to
 Releasing 
and then back to
 Idle
. Do not attempt to stop or re-initiate the measurement, or to start any new measurements until the test set has reached
 Idle 
state (see 
Test set may lock up if operations are attempted before the UE completes its PRACH sequence
).
Setting call limit mode to off before initiating the measurement also avoids another issue: When the measurement completes, if you try to send signalling to the UE while it is still sending PRACH preambles to the test set, the UE will ignore the incoming messages and the signalling will fail. If call limit mode is set to off, the test set will acknowledge the UE and cause it to stop sending PRACH preambles, and then send the signalling you have requested to the UE.
When the measurement completes, you must wait until the UE has finished its PRACH sequence before turning off or re-initiating the measurement, or before starting any new measurements. Otherwise, the test set may lock up. If you are controlling the test set via remote program, you must include a wait period after the measurement completes.
 
If you set
 Call Limit Mode 
to
 Off 
before initiating the measurement, you will know that the UE's PRACH sequence is complete when you see the call status move from
 Paging 
to 
Idle
, to
 Setup
, to
 Releasing 
and then back to
 Idle 
(see 
Importance of Setting Call Limit State to Off before Initiating a PRACH Measurement
). Do not attempt any of the above listed operations until the test set has reached
 Idle 
state.
 
To allow the UE to complete its PRACH sequence as quickly as possible, it is recommended that you set
 PRACH Preambles 
to
 4 
and
 PRACH Ramping Cycles (MMAX) 
to
 1 
(see 
Recommended PRACH Preambles and PRACH Ramping Cycles (MMAX) settings
).
 Trigger Source 
is set to
 RF Rise 
or
 External
.
 RF Rise
.
 
If 
Over Range
 (5) is returned, the measured signal exceeds the expected input level or exceeds the maximum allowed input power for the test set. 
 
If 
Under Range
 (6) is returned, the measured signal is below the expected input level. 
 
If 
Uncalibrated Due to Temperature
 (19) is returned, the temperature in the test set has changed by ± 10° C or more since the last calibration and should be calibrated again. 
Calibrating the Test Set
See Integrity Indicator .